BC_TypeDef Struct ReferenceBSP > API for DK's
Board Controller Register definiton
Definition at line 53
of file bsp_dk_bcreg_3201.h
.
#include <
bsp_dk_bcreg_3201.h
>
Field Documentation
__IO uint16_t BC_TypeDef::ADC_READ |
0x24 - AEM ADC SPI interface
Definition at line 73
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::ADC_STATUS |
0x22 - AEM ADC SPI interface
Definition at line 72
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::ADC_WRITE |
0x20 - AEM ADC SPI interface
Definition at line 71
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::ARB_CTRL |
0x16 - Arbiter control, board control or EFM32GG access to display
Definition at line 66
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::BC_MBOX_TXCTRL |
0x80 - BC <-> EFM32 communication channel
Definition at line 103
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::BC_MBOX_TXDATA |
0x82
Definition at line 104
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::BC_MBOX_TXSTATUS0 |
0x84
Definition at line 105
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::BC_MBOX_TXSTATUS1 |
0x86
Definition at line 106
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::BUF_CTRL |
0xc0 - Buffer Controller Control
Definition at line 117
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::CLKRST |
0x26 - Clock and reset control
Definition at line 75
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::DISPLAY_CTRL |
0x12 - SSD2119 TFT display control
Definition at line 64
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::EBI_CTRL |
0x14 - Extended Address Mode control
Definition at line 65
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::EM |
0x02 - Energy Mode indicator
Definition at line 55
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::FW_BUILDNO |
0x2A - Firmware build number
Definition at line 78
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::FW_VERSION |
0x2C - Firmware version
Definition at line 79
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::HW_VERSION |
0x28 - Hardware version
Definition at line 77
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTCLEAR |
0x44 - Interrupt clear
Definition at line 95
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTEN |
0x42 - Interrupt Enable flags
Definition at line 94
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTFLAG |
0x40 - Interrupt Status flags
Definition at line 93
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTPCTRL |
0x48 - Interrupt pulse control
Definition at line 97
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTPHIGH |
0x4C - Interrupt puls high period
Definition at line 99
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTPLOW |
0x4A - Interrupt puls low period
Definition at line 98
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::INTSET |
0x46 - Interrupt set
Definition at line 96
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::MAGIC |
0x04 - Should always read 0xEF32
Definition at line 56
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::MBOX_TXCTRL |
0xa2 - BC <-> EFM32 communication channel
Definition at line 110
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::MBOX_TXDATA |
0xa4
Definition at line 111
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::MBOX_TXSTATUS0 |
0xa6
Definition at line 112
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::MBOX_TXSTATUS1 |
0xa8
Definition at line 113
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::PERICON |
0x18 - Peripheral Control, on board switches
Definition at line 67
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::RESERVED4[0x0d] |
0xa0 - Reserved
Definition at line 108
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::RESERVED5[0x0b] |
0xaa - Reserved
Definition at line 115
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::RESERVERD0 |
0x00 - Reserved
Definition at line 54
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::RESERVERD1[0x02] |
0x1C - Reserved
Definition at line 69
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::RESERVERD3[0x19] |
0x50 - Reserved
Definition at line 101
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_BC0 |
0x38 - Board Control registers
Definition at line 88
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_BC1 |
0x3A
Definition at line 89
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_BC2 |
0x3C
Definition at line 90
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_BC3 |
0x3E
Definition at line 91
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_COMMON |
0x2E - Shared register between board controller and EFM32
Definition at line 81
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_EFM0 |
0x30 - EFM32 accessible registers
Definition at line 83
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_EFM1 |
0x32
Definition at line 84
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_EFM2 |
0x34
Definition at line 85
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SCRATCH_EFM3 |
0x36
Definition at line 86
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::SPI_DEMUX |
0x1A - SPI DEMUX
Definition at line 68
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::UIF_AEM |
0x0E - AEM button
Definition at line 62
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::UIF_CTRL |
0x10 - CPLD control register
Definition at line 63
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::UIF_DIP |
0x0A - DIP switch status
Definition at line 60
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::UIF_JOYSTICK |
0x0C - Joystick presses
Definition at line 61
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::UIF_LEDS |
0x06 - On board LEDs
Definition at line 58
of file bsp_dk_bcreg_3201.h
.
__IO uint16_t BC_TypeDef::UIF_PB |
0x08 - Push button PB0-PB4 status
Definition at line 59
of file bsp_dk_bcreg_3201.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/bsp/
bsp_dk_bcreg_3201.h