LESENSE_ST_TypeDef Struct ReferenceDevices

LESENSE_ST EFM32TG LESENSE ST.

Definition at line 46 of file efm32tg_lesense_st.h.

#include <efm32tg_lesense_st.h>

Data Fields

__IOM uint32_t TCONFA
 
__IOM uint32_t TCONFB
 

Field Documentation

__IOM uint32_t LESENSE_ST_TypeDef::TCONFA

State transition configuration A

Definition at line 47 of file efm32tg_lesense_st.h.

__IOM uint32_t LESENSE_ST_TypeDef::TCONFB

State transition configuration B

Definition at line 48 of file efm32tg_lesense_st.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/efm32tg_lesense_st.h