USART_InitSync_TypeDef Struct ReferenceEMLIB > USART
Synchronous mode initialization structure.
Definition at line 463
of file em_usart.h
.
#include <
em_usart.h
>
Data Fields | |
bool | autoCsEnable |
bool | autoTx |
uint32_t | baudrate |
USART_ClockMode_TypeDef | clockMode |
USART_Databits_TypeDef | databits |
USART_Enable_TypeDef | enable |
bool | master |
bool | msbf |
USART_PrsRxCh_TypeDef | prsRxCh |
bool | prsRxEnable |
uint32_t | refFreq |
Field Documentation
bool USART_InitSync_TypeDef::autoCsEnable |
bool USART_InitSync_TypeDef::autoTx |
Enable AUTOTX mode. Transmits as long as RX is not full. Generates underflows if TX is empty.
Definition at line 497
of file em_usart.h
.
Referenced by MIC_init(), and USART_InitSync().
uint32_t USART_InitSync_TypeDef::baudrate |
Desired baud rate.
Definition at line 474
of file em_usart.h
.
Referenced by MIC_init(), MICROSD_Init(), SPIDRV_Init(), and USART_InitSync().
USART_ClockMode_TypeDef USART_InitSync_TypeDef::clockMode |
Clock polarity/phase mode.
Definition at line 486
of file em_usart.h
.
Referenced by SPIDRV_Init(), and USART_InitSync().
USART_Databits_TypeDef USART_InitSync_TypeDef::databits |
Number of data bits in frame.
Definition at line 477
of file em_usart.h
.
Referenced by USART_InitSync().
USART_Enable_TypeDef USART_InitSync_TypeDef::enable |
Specifies whether TX and/or RX shall be enabled when initialization is completed.
Definition at line 465
of file em_usart.h
.
Referenced by MIC_init(), USART_InitI2s(), and USART_InitSync().
bool USART_InitSync_TypeDef::master |
Select if to operate in master or slave mode.
Definition at line 480
of file em_usart.h
.
Referenced by SPIDRV_Init(), and USART_InitSync().
bool USART_InitSync_TypeDef::msbf |
Select if to send most or least significant bit first.
Definition at line 483
of file em_usart.h
.
Referenced by MICROSD_Init(), SPIDRV_Init(), and USART_InitSync().
USART_PrsRxCh_TypeDef USART_InitSync_TypeDef::prsRxCh |
Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).
Definition at line 493
of file em_usart.h
.
Referenced by USART_InitSync().
bool USART_InitSync_TypeDef::prsRxEnable |
uint32_t USART_InitSync_TypeDef::refFreq |
USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.
Definition at line 471
of file em_usart.h
.
Referenced by USART_InitSync().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_usart.h