BAP - Barometric Pressure SensorBSP > Thunderboard Sense BSP
Detailed Description
Driver for the Bosch Sensortec BMP280 pressure sensor.
| Data Structures | |
| struct | __BAP_Config | 
| Structure to configure the BMP280 device. | |
| Typedefs | |
| typedef struct __BAP_Config | BAP_Config | 
| Structure to configure the BMP280 device. | |
| Functions | |
| uint32_t | BAP_config ( BAP_Config *cfg) | 
| Configure the barometric pressure sensor. | |
| void | BAP_deInit (void) | 
| De-initializes the barometric pressure module. | |
| uint32_t | BAP_getPressure (float *pressure) | 
| Initiates pressure measurement on the barometric pressure sensor and reads pressure from it. | |
| uint32_t | BAP_getTemperature (float *temperature) | 
| Initiates temperature measurement on the barometric pressure sensor and reads pressure from it. | |
| uint32_t | BAP_init (uint8_t *deviceId) | 
| Initializes the barometric pressure sensor chip. | |
| Error Codes | |
| #define | BAP_OK 0x0000 | 
| #define | BAP_ERROR_DRIVER_NOT_INITIALIZED 0x0001 | 
| #define | BAP_ERROR_I2C_TRANSACTION_FAILED 0x0002 | 
| #define | BAP_ERROR_DEVICE_ID_MISMATCH 0x0003 | 
Macro Definition Documentation
| #define BAP_ERROR_DEVICE_ID_MISMATCH 0x0003 | 
The device ID does not match the expected value
        Definition at line
        
         33
        
        of file
        
         bap.h
        
        .
       
Referenced by BAP_init() .
| #define BAP_ERROR_DRIVER_NOT_INITIALIZED 0x0001 | 
The driver is not initialized
        Definition at line
        
         31
        
        of file
        
         bap.h
        
        .
       
| #define BAP_ERROR_I2C_TRANSACTION_FAILED 0x0002 | 
I2C transaction failed
        Definition at line
        
         32
        
        of file
        
         bap.h
        
        .
       
| #define BAP_OK 0x0000 | 
No errors
        Definition at line
        
         30
        
        of file
        
         bap.h
        
        .
       
Referenced by BAP_getPressure() , BAP_getTemperature() , and BAP_init() .
Function Documentation
| uint32_t BAP_config | ( | BAP_Config * | 
            cfg
            | ) | 
Configure the barometric pressure sensor.
- Parameters
- 
         [in] cfgStructure, which holds the configuration parameters 
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         143
        
        of file
        
         bap.c
        
        .
       
References bmp280_set_power_mode() , bmp280_set_standby_durn() , bmp280_set_work_mode() , __BAP_Config::oversampling , __BAP_Config::powerMode , and __BAP_Config::standbyTime .
| void BAP_deInit | ( | void | 
            | ) | 
De-initializes the barometric pressure module.
- Returns
- None
        Definition at line
        
         123
        
        of file
        
         bap.c
        
        .
       
References bmp280_set_power_mode() , and BOARD_bapEnable() .
| uint32_t BAP_getPressure | ( | float * | 
            pressure
            | ) | 
Initiates pressure measurement on the barometric pressure sensor and reads pressure from it.
- Parameters
- 
         [out] pressureThe measured pressure in millibars 
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         203
        
        of file
        
         bap.c
        
        .
       
References BAP_OK , bmp280_compensate_pressure_int64() , bmp280_compensate_temperature_int32() , bmp280_get_forced_uncomp_pressure_temperature() , bmp280_read_uncomp_pressure() , and bmp280_read_uncomp_temperature() .
| uint32_t BAP_getTemperature | ( | float * | 
            temperature
            | ) | 
Initiates temperature measurement on the barometric pressure sensor and reads pressure from it.
- Parameters
- 
         [out] temperatureThe measured temperature in degrees Celsius 
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         168
        
        of file
        
         bap.c
        
        .
       
References BAP_OK , bmp280_compensate_temperature_int32() , bmp280_get_forced_uncomp_pressure_temperature() , and bmp280_read_uncomp_temperature() .
| uint32_t BAP_init | ( | uint8_t * | 
            deviceId
            | ) | 
Initializes the barometric pressure sensor chip.
- Parameters
- 
         [out] deviceIdThe device ID of the connected chip 
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         69
        
        of file
        
         bap.c
        
        .
       
References BAP_ERROR_DEVICE_ID_MISMATCH , BAP_OK , bmp280_init() , bmp280_set_power_mode() , bmp280_set_work_mode() , BOARD_bapEnable() , bmp280_t::delay_msec , bmp280_t::dev_addr , and UTIL_delay() .