PRS_TypeDef Struct ReferenceDevices > PRS
PRS Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32mg1p_prs.h
       
       .
      
      
       #include <
       
     
        efr32mg1p_prs.h
       
       >
      
| Data Fields | |
| PRS_CH_TypeDef | CH [12] | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DMAREQ0 | 
| __IOM uint32_t | DMAREQ1 | 
| __IM uint32_t | PEEK | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [1] | 
| uint32_t | RESERVED2 [1] | 
| uint32_t | RESERVED3 [3] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IOM uint32_t | ROUTELOC1 | 
| __IOM uint32_t | ROUTELOC2 | 
| __IOM uint32_t | ROUTEPEN | 
| __IOM uint32_t | SWLEVEL | 
| __IOM uint32_t | SWPULSE | 
Field Documentation
| PRS_CH_TypeDef PRS_TypeDef::CH[12] | 
Channel registers
        Definition at line
        
         66
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::CTRL | 
Control Register
        Definition at line
        
         59
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::DMAREQ0 | 
DMA Request 0 Register
        Definition at line
        
         60
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::DMAREQ1 | 
DMA Request 1 Register
        Definition at line
        
         61
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IM uint32_t PRS_TypeDef::PEEK | 
PRS Channel Values
        Definition at line
        
         63
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| uint32_t PRS_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         53
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| uint32_t PRS_TypeDef::RESERVED1[1] | 
Reserved for future use
        Definition at line
        
         58
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| uint32_t PRS_TypeDef::RESERVED2[1] | 
Reserved for future use
        Definition at line
        
         62
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| uint32_t PRS_TypeDef::RESERVED3[3] | 
Reserved registers
        Definition at line
        
         65
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         54
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::ROUTELOC1 | 
I/O Routing Location Register
        Definition at line
        
         55
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::ROUTELOC2 | 
I/O Routing Location Register
        Definition at line
        
         56
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::ROUTEPEN | 
I/O Routing Pin Enable Register
        Definition at line
        
         52
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::SWLEVEL | 
Software Level Register
        Definition at line
        
         51
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
| __IOM uint32_t PRS_TypeDef::SWPULSE | 
Software Pulse Register
        Definition at line
        
         50
        
        of file
        
         efr32mg1p_prs.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG1P/Include/
       efr32mg1p_prs.h