HIDKBD_KeyReport_t Struct ReferenceKit Drivers > HidKeyboard
HID keyboard input report definition.
       Definition at line
       
        38
       
       of file
       
        hidkbd.h
       
       .
      
      
       #include <
       
     
        hidkbd.h
       
       >
      
| Data Fields | |
| uint8_t | key [6] | 
| uint8_t | modifier | 
| uint8_t | reserved | 
Field Documentation
| uint8_t HIDKBD_KeyReport_t::key[6] | 
Array of 6 key array indices, key index codes are defined in the "Keyboard page" section of "USB HID Usage Tables document", also refer to usbkbdscancodes.c .
        Definition at line
        
         41
        
        of file
        
         hidkbd.h
        
        .
       
| uint8_t HIDKBD_KeyReport_t::modifier | 
Key modifier byte as defined in HID spec. section "8.3 Report Format for Array Items".
        Definition at line
        
         39
        
        of file
        
         hidkbd.h
        
        .
       
| uint8_t HIDKBD_KeyReport_t::reserved | 
Reserved, should be set to zero.
        Definition at line
        
         40
        
        of file
        
         hidkbd.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       hidkbd.h