CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU

HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.

Definition at line 1447 of file em_cmu.h .

#include < em_cmu.h >

Data Fields

bool autoSelEm01
bool autoStartEm01
bool autoStartSelOnRacWakeup
uint16_t ctuneStartup
uint16_t ctuneSteadyState
bool lowPowerMode
CMU_OscMode_TypeDef mode
uint8_t regIshSteadyState
uint8_t thresholdPeakDetect
uint8_t timeoutPeakDetect
uint8_t timeoutShuntOptimization
uint8_t timeoutStartup
uint8_t timeoutSteady
uint8_t xoCoreBiasTrimStartup
uint8_t xoCoreBiasTrimSteadyState

Field Documentation

bool CMU_HFXOInit_TypeDef::autoSelEm01
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 1459 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::autoStartEm01
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 1458 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 1460 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint16_t CMU_HFXOInit_TypeDef::ctuneStartup

Startup phase CTUNE (load capacitance) value

Definition at line 1461 of file em_cmu.h .

Referenced by BSP_initClocks() , and CMU_HFXOInit() .

uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState

Steady-state phase CTUNE (load capacitance) value

Definition at line 1462 of file em_cmu.h .

Referenced by BSP_initClocks() , and CMU_HFXOInit() .

bool CMU_HFXOInit_TypeDef::lowPowerMode

Enable low-power mode

Definition at line 1457 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode

Oscillator mode

Definition at line 1476 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState

Shunt steady-state current

Definition at line 1463 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect

Peak detection threshold

Definition at line 1466 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect

Timeout - peak detection

Definition at line 1468 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization

Timeout - shunt optimization

Definition at line 1467 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutStartup

Timeout - startup

Definition at line 1470 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::timeoutSteady

Timeout - steady-state

Definition at line 1469 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup

Startup XO core bias current trim

Definition at line 1464 of file em_cmu.h .

Referenced by CMU_HFXOInit() .

uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState

Steady-state XO core bias current trim

Definition at line 1465 of file em_cmu.h .

Referenced by CMU_HFXOInit() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_cmu.h