MSDSCSI_ReadCapacity_TypeDef Struct ReferenceKit Drivers > Msd
SCSI Read Capacity Command Descriptor Block (CDB) typedef.
       Definition at line
       
        175
       
       of file
       
        msdscsi.h
       
       .
      
      
       #include <
       
     
        msdscsi.h
       
       >
      
| Data Fields | |
| struct { | |
| uint8_t Obsolete : 1 | |
| uint8_t Reserved1 : 7 | |
| }; | |
| struct { | |
| uint8_t Pmi : 1 | |
| uint8_t Reserved3 : 7 | |
| }; | |
| uint8_t | Control | 
| uint32_t | Lba | 
| uint8_t | OpCode | 
| uint16_t | Reserved2 | 
Field Documentation
| uint8_t MSDSCSI_ReadCapacity_TypeDef::Control | 
Control byte.
        Definition at line
        
         187
        
        of file
        
         msdscsi.h
        
        .
       
| uint32_t MSDSCSI_ReadCapacity_TypeDef::Lba | 
Logical Block (sector) Address.
        Definition at line
        
         181
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_ReadCapacity_TypeDef::Obsolete | 
Obsolete, expect any value.
        Definition at line
        
         178
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_ReadCapacity_TypeDef::OpCode | 
Command opcode.
        Definition at line
        
         176
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_ReadCapacity_TypeDef::Pmi | 
Partial medium indicator.
        Definition at line
        
         184
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved1 | 
Reserved, expect 0.
        Definition at line
        
         179
        
        of file
        
         msdscsi.h
        
        .
       
| uint16_t MSDSCSI_ReadCapacity_TypeDef::Reserved2 | 
Reserved, expect 0.
        Definition at line
        
         182
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved3 | 
Reserved, expect 0.
        Definition at line
        
         185
        
        of file
        
         msdscsi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       msdscsi.h