LEUART_TypeDef Struct ReferenceDevices > LEUART
LEUART Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32mg1p_leuart.h
       
       .
      
      
       #include <
       
     
        efr32mg1p_leuart.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CLKDIV | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | FREEZE | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | INPUT | 
| __IOM uint32_t | PULSECTRL | 
| uint32_t | RESERVED0 [3] | 
| uint32_t | RESERVED1 [2] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IOM uint32_t | ROUTEPEN | 
| __IM uint32_t | RXDATA | 
| __IM uint32_t | RXDATAX | 
| __IM uint32_t | RXDATAXP | 
| __IOM uint32_t | SIGFRAME | 
| __IOM uint32_t | STARTFRAME | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IOM uint32_t | TXDATA | 
| __IOM uint32_t | TXDATAX | 
Field Documentation
| __IOM uint32_t LEUART_TypeDef::CLKDIV | 
Clock Control Register
        Definition at line
        
         53
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_BaudrateGet() , LEUART_BaudrateSet() , and LEUART_Reset() .
| __IOM uint32_t LEUART_TypeDef::CMD | 
Command Register
        Definition at line
        
         51
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Enable() , LEUART_Init() , LEUART_Reset() , LEUART_RxDmaInEM2Enable() , LEUART_TxDmaInEM2Enable() , and UARTDRV_InitLeuart() .
| __IOM uint32_t LEUART_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Init() , LEUART_Reset() , LEUART_RxDmaInEM2Enable() , and LEUART_TxDmaInEM2Enable() .
| __IOM uint32_t LEUART_TypeDef::FREEZE | 
Freeze Register
        Definition at line
        
         67
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_FreezeEnable() .
| __IOM uint32_t LEUART_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         64
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_IntDisable() , LEUART_IntEnable() , LEUART_IntGetEnabled() , and LEUART_Reset() .
| __IM uint32_t LEUART_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         61
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_IntGet() , and LEUART_IntGetEnabled() .
| __IOM uint32_t LEUART_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         63
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_IntClear() , and LEUART_Reset() .
| __IOM uint32_t LEUART_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         62
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_IntSet() .
| __IOM uint32_t LEUART_TypeDef::INPUT | 
LEUART Input Register
        Definition at line
        
         74
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
| __IOM uint32_t LEUART_TypeDef::PULSECTRL | 
Pulse Control Register
        Definition at line
        
         65
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Reset() .
| uint32_t LEUART_TypeDef::RESERVED0[3] | 
Reserved for future use
        Definition at line
        
         70
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
| uint32_t LEUART_TypeDef::RESERVED1[2] | 
Reserved for future use
        Definition at line
        
         73
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
| __IOM uint32_t LEUART_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         72
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Reset() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| __IOM uint32_t LEUART_TypeDef::ROUTEPEN | 
I/O Routing Pin Enable Register
        Definition at line
        
         71
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Reset() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .
| __IM uint32_t LEUART_TypeDef::RXDATA | 
Receive Buffer Data Register
        Definition at line
        
         57
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Rx() , and LEUART_RxDataGet() .
| __IM uint32_t LEUART_TypeDef::RXDATAX | 
Receive Buffer Data Extended Register
        Definition at line
        
         56
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_RxDataXGet() , and LEUART_RxExt() .
| __IM uint32_t LEUART_TypeDef::RXDATAXP | 
Receive Buffer Data Extended Peek Register
        Definition at line
        
         58
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
| __IOM uint32_t LEUART_TypeDef::SIGFRAME | 
Signal Frame Register
        Definition at line
        
         55
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Reset() .
| __IOM uint32_t LEUART_TypeDef::STARTFRAME | 
Start Frame Register
        Definition at line
        
         54
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Reset() .
| __IM uint32_t LEUART_TypeDef::STATUS | 
Status Register
        Definition at line
        
         52
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Rx() , LEUART_RxDmaInEM2Enable() , LEUART_RxExt() , LEUART_StatusGet() , LEUART_Tx() , LEUART_TxDmaInEM2Enable() , and LEUART_TxExt() .
| __IM uint32_t LEUART_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         68
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_FreezeEnable() , and UARTDRV_InitLeuart() .
| __IOM uint32_t LEUART_TypeDef::TXDATA | 
Transmit Buffer Data Register
        Definition at line
        
         60
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_Tx() .
| __IOM uint32_t LEUART_TypeDef::TXDATAX | 
Transmit Buffer Data Extended Register
        Definition at line
        
         59
        
        of file
        
         efr32mg1p_leuart.h
        
        .
       
Referenced by LEUART_TxExt() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG1P/Include/
       efr32mg1p_leuart.h