TIMER_CC_TypeDef Struct ReferenceDevicesDevices > | TIMER
TIMER_CC TIMER CC Register
.
       Definition at line
       
        47
       
       of file
       
        efr32mg1p_timer_cc.h
       
       .
      
      
       #include <
       
     
        efr32mg1p_timer_cc.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CCV | 
| __IOM uint32_t | CCVB | 
| __IM uint32_t | CCVP | 
| __IOM uint32_t | CTRL | 
Field Documentation
| __IOM uint32_t TIMER_CC_TypeDef::CCV | 
CC Channel Value Register
        Definition at line
        
         49
        
        of file
        
         efr32mg1p_timer_cc.h
        
        .
       
Referenced by TIMER_CaptureGet() , TIMER_CompareSet() , and TIMER_Reset() .
| __IOM uint32_t TIMER_CC_TypeDef::CCVB | 
CC Channel Buffer Register
        Definition at line
        
         51
        
        of file
        
         efr32mg1p_timer_cc.h
        
        .
       
Referenced by TIMER_CompareBufSet() , and TIMER_Reset() .
| __IM uint32_t TIMER_CC_TypeDef::CCVP | 
CC Channel Value Peek Register
        Definition at line
        
         50
        
        of file
        
         efr32mg1p_timer_cc.h
        
        .
       
| __IOM uint32_t TIMER_CC_TypeDef::CTRL | 
CC Channel Control Register
        Definition at line
        
         48
        
        of file
        
         efr32mg1p_timer_cc.h
        
        .
       
Referenced by TIMER_InitCC() , and TIMER_Reset() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG1P/Include/
       efr32mg1p_timer_cc.h