LETIMEREMLIB
Detailed Description
Low Energy Timer (LETIMER) Peripheral API.
This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.
Data Structures | |
struct | LETIMER_Init_TypeDef |
Macros | |
#define | LETIMER_INIT_DEFAULT |
Enumerations | |
enum | LETIMER_RepeatMode_TypeDef { letimerRepeatFree = _LETIMER_CTRL_REPMODE_FREE, letimerRepeatOneshot = _LETIMER_CTRL_REPMODE_ONESHOT, letimerRepeatBuffered = _LETIMER_CTRL_REPMODE_BUFFERED, letimerRepeatDouble = _LETIMER_CTRL_REPMODE_DOUBLE } |
enum | LETIMER_UFOA_TypeDef { letimerUFOANone = _LETIMER_CTRL_UFOA0_NONE, letimerUFOAToggle = _LETIMER_CTRL_UFOA0_TOGGLE, letimerUFOAPulse = _LETIMER_CTRL_UFOA0_PULSE, letimerUFOAPwm = _LETIMER_CTRL_UFOA0_PWM } |
Functions | |
uint32_t | LETIMER_CompareGet (LETIMER_TypeDef *letimer, unsigned int comp) |
Get the LETIMER compare register value. | |
void | LETIMER_CompareSet (LETIMER_TypeDef *letimer, unsigned int comp, uint32_t value) |
Set the LETIMER compare register value. | |
__STATIC_INLINE uint32_t | LETIMER_CounterGet (LETIMER_TypeDef *letimer) |
Get LETIMER counter value. | |
void | LETIMER_Enable (LETIMER_TypeDef *letimer, bool enable) |
Start/stop LETIMER. | |
void | LETIMER_Init (LETIMER_TypeDef *letimer, const LETIMER_Init_TypeDef *init) |
Initialize LETIMER. | |
__STATIC_INLINE void | LETIMER_IntClear (LETIMER_TypeDef *letimer, uint32_t flags) |
Clear one or more pending LETIMER interrupts. | |
__STATIC_INLINE void | LETIMER_IntDisable (LETIMER_TypeDef *letimer, uint32_t flags) |
Disable one or more LETIMER interrupts. | |
__STATIC_INLINE void | LETIMER_IntEnable (LETIMER_TypeDef *letimer, uint32_t flags) |
Enable one or more LETIMER interrupts. | |
__STATIC_INLINE uint32_t | LETIMER_IntGet (LETIMER_TypeDef *letimer) |
Get pending LETIMER interrupt flags. | |
__STATIC_INLINE uint32_t | LETIMER_IntGetEnabled (LETIMER_TypeDef *letimer) |
Get enabled and pending LETIMER interrupt flags. | |
__STATIC_INLINE void | LETIMER_IntSet (LETIMER_TypeDef *letimer, uint32_t flags) |
Set one or more pending LETIMER interrupts from SW. | |
uint32_t | LETIMER_RepeatGet (LETIMER_TypeDef *letimer, unsigned int rep) |
Get the LETIMER repeat register value. | |
void | LETIMER_RepeatSet (LETIMER_TypeDef *letimer, unsigned int rep, uint32_t value) |
Set the LETIMER repeat counter register value. | |
void | LETIMER_Reset (LETIMER_TypeDef *letimer) |
Reset LETIMER to the same state that it was in after a hardware reset. | |
Macro Definition Documentation
#define LETIMER_INIT_DEFAULT |
Default configuration for LETIMER initialization structure.
Definition at line 126
of file em_letimer.h
.
Referenced by MIC_init().
Enumeration Type Documentation
Repeat mode.
Definition at line 59
of file em_letimer.h
.
enum LETIMER_UFOA_TypeDef |
Underflow action on output.
Definition at line 77
of file em_letimer.h
.
Function Documentation
uint32_t LETIMER_CompareGet | ( | LETIMER_TypeDef * | letimer, |
unsigned int | comp |
||
) |
Get the LETIMER compare register value.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block. [in] comp
A compare register to get, either 0 or 1.
- Returns
- A compare register value, 0 if invalid register selected.
Definition at line 135
of file em_letimer.c
.
References LETIMER_TypeDef::COMP0, and LETIMER_TypeDef::COMP1.
void LETIMER_CompareSet | ( | LETIMER_TypeDef * | letimer, |
unsigned int | comp, |
||
uint32_t | value |
||
) |
Set the LETIMER compare register value.
- Note
- The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block. [in] comp
A compare register to set, either 0 or 1. [in] value
An initialization value (<= 0x0000ffff).
Definition at line 180
of file em_letimer.c
.
References _LETIMER_COMP0_COMP0_MASK, _LETIMER_COMP0_COMP0_SHIFT, LETIMER_TypeDef::COMP0, and LETIMER_TypeDef::COMP1.
Referenced by MIC_init().
__STATIC_INLINE uint32_t LETIMER_CounterGet | ( | LETIMER_TypeDef * | letimer | ) |
Get LETIMER counter value.
- Parameters
-
[in] letimer
Pointer to the LETIMER peripheral register block.
- Returns
- Current LETIMER counter value.
Definition at line 159
of file em_letimer.h
.
References LETIMER_TypeDef::CNT.
void LETIMER_Enable | ( | LETIMER_TypeDef * | letimer, |
bool | enable |
||
) |
Start/stop LETIMER.
- Note
- The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block. [in] enable
True to enable counting, false to disable.
Definition at line 233
of file em_letimer.c
.
References LETIMER_TypeDef::CMD, LETIMER_CMD_START, LETIMER_CMD_STOP, and LETIMER_SYNCBUSY_CMD.
void LETIMER_Init | ( | LETIMER_TypeDef * | letimer, |
const LETIMER_Init_TypeDef * | init |
||
) |
Initialize LETIMER.
Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet(). That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.
- Note
- The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block. [in] init
A pointer to the LETIMER initialization structure.
Definition at line 323
of file em_letimer.c
.
References _LETIMER_CTRL_REPMODE_SHIFT, _LETIMER_CTRL_UFOA0_SHIFT, _LETIMER_CTRL_UFOA1_SHIFT, LETIMER_Init_TypeDef::bufTop, LETIMER_TypeDef::CMD, LETIMER_Init_TypeDef::comp0Top, LETIMER_TypeDef::CTRL, LETIMER_Init_TypeDef::debugRun, LETIMER_Init_TypeDef::enable, LETIMER_CMD_START, LETIMER_CMD_STOP, LETIMER_CTRL_BUFTOP, LETIMER_CTRL_COMP0TOP, LETIMER_CTRL_DEBUGRUN, LETIMER_CTRL_OPOL0, LETIMER_CTRL_OPOL1, LETIMER_STATUS_RUNNING, LETIMER_SYNCBUSY_CMD, LETIMER_Init_TypeDef::out0Pol, LETIMER_Init_TypeDef::out1Pol, LETIMER_Init_TypeDef::repMode, LETIMER_TypeDef::STATUS, LETIMER_Init_TypeDef::ufoa0, and LETIMER_Init_TypeDef::ufoa1.
Referenced by MIC_init().
__STATIC_INLINE void LETIMER_IntClear | ( | LETIMER_TypeDef * | letimer, |
uint32_t | flags |
||
) |
Clear one or more pending LETIMER interrupts.
- Parameters
-
[in] letimer
Pointer to LETIMER peripheral register block. [in] flags
Pending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line 182
of file em_letimer.h
.
References LETIMER_TypeDef::IFC.
__STATIC_INLINE void LETIMER_IntDisable | ( | LETIMER_TypeDef * | letimer, |
uint32_t | flags |
||
) |
Disable one or more LETIMER interrupts.
- Parameters
-
[in] letimer
Pointer to LETIMER peripheral register block. [in] flags
LETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line 198
of file em_letimer.h
.
References LETIMER_TypeDef::IEN.
__STATIC_INLINE void LETIMER_IntEnable | ( | LETIMER_TypeDef * | letimer, |
uint32_t | flags |
||
) |
Enable one or more LETIMER interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] letimer
Pointer to the LETIMER peripheral register block. [in] flags
LETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line 219
of file em_letimer.h
.
References LETIMER_TypeDef::IEN.
__STATIC_INLINE uint32_t LETIMER_IntGet | ( | LETIMER_TypeDef * | letimer | ) |
Get pending LETIMER interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
-
[in] letimer
Pointer to LETIMER peripheral register block.
- Returns
- LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line 238
of file em_letimer.h
.
References LETIMER_TypeDef::IF.
__STATIC_INLINE uint32_t LETIMER_IntGetEnabled | ( | LETIMER_TypeDef * | letimer | ) |
Get enabled and pending LETIMER interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
-
[in] letimer
Pointer to LETIMER peripheral register block.
- Returns
- Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
- the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).
Definition at line 264
of file em_letimer.h
.
References LETIMER_TypeDef::IEN, and LETIMER_TypeDef::IF.
__STATIC_INLINE void LETIMER_IntSet | ( | LETIMER_TypeDef * | letimer, |
uint32_t | flags |
||
) |
Set one or more pending LETIMER interrupts from SW.
- Parameters
-
[in] letimer
Pointer to LETIMER peripheral register block. [in] flags
LETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
Definition at line 287
of file em_letimer.h
.
References LETIMER_TypeDef::IFS.
uint32_t LETIMER_RepeatGet | ( | LETIMER_TypeDef * | letimer, |
unsigned int | rep |
||
) |
Get the LETIMER repeat register value.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block. [in] rep
Repeat register to get, either 0 or 1.
- Returns
- Repeat register value, 0 if invalid register selected.
Definition at line 403
of file em_letimer.c
.
References LETIMER_TypeDef::REP0, and LETIMER_TypeDef::REP1.
void LETIMER_RepeatSet | ( | LETIMER_TypeDef * | letimer, |
unsigned int | rep, |
||
uint32_t | value |
||
) |
Set the LETIMER repeat counter register value.
- Note
- The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block. [in] rep
Repeat counter register to set, either 0 or 1. [in] value
An initialization value (<= 0x0000ffff).
Definition at line 448
of file em_letimer.c
.
References _LETIMER_REP0_REP0_MASK, _LETIMER_REP0_REP0_SHIFT, LETIMER_TypeDef::REP0, and LETIMER_TypeDef::REP1.
Referenced by MIC_init().
void LETIMER_Reset | ( | LETIMER_TypeDef * | letimer | ) |
Reset LETIMER to the same state that it was in after a hardware reset.
- Note
- The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
- Parameters
-
[in] letimer
A pointer to the LETIMER peripheral register block.
Definition at line 502
of file em_letimer.c
.
References _LETIMER_COMP0_RESETVALUE, _LETIMER_COMP1_RESETVALUE, _LETIMER_CTRL_RESETVALUE, _LETIMER_IEN_RESETVALUE, _LETIMER_IFC_MASK, _LETIMER_REP0_RESETVALUE, _LETIMER_REP1_RESETVALUE, LETIMER_TypeDef::CMD, LETIMER_TypeDef::COMP0, LETIMER_TypeDef::COMP1, LETIMER_TypeDef::CTRL, LETIMER_TypeDef::IEN, LETIMER_TypeDef::IFC, LETIMER_CMD_CLEAR, LETIMER_CMD_CTO0, LETIMER_CMD_CTO1, LETIMER_CMD_STOP, LETIMER_TypeDef::REP0, and LETIMER_TypeDef::REP1.