GPCRC_TypeDef Struct ReferenceDevices > GPCRC
GPCRC Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32mg14p_gpcrc.h
       
       .
      
      
       #include <
       
     
        efr32mg14p_gpcrc.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IM uint32_t | DATA | 
| __IM uint32_t | DATABYTEREV | 
| __IM uint32_t | DATAREV | 
| __IOM uint32_t | INIT | 
| __IOM uint32_t | INPUTDATA | 
| __IOM uint32_t | INPUTDATABYTE | 
| __IOM uint32_t | INPUTDATAHWORD | 
| __IOM uint32_t | POLY | 
Field Documentation
| __IOM uint32_t GPCRC_TypeDef::CMD | 
| __IOM uint32_t GPCRC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_Enable() , GPCRC_Init() , and GPCRC_Reset() .
| __IM uint32_t GPCRC_TypeDef::DATA | 
CRC Data Register
        Definition at line
        
         57
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_DataRead() .
| __IM uint32_t GPCRC_TypeDef::DATABYTEREV | 
CRC Data Byte Reverse Register
        Definition at line
        
         59
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_DataReadByteReversed() .
| __IM uint32_t GPCRC_TypeDef::DATAREV | 
CRC Data Reverse Register
        Definition at line
        
         58
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_DataReadBitReversed() .
| __IOM uint32_t GPCRC_TypeDef::INIT | 
CRC Init Value
        Definition at line
        
         52
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_Init() , GPCRC_InitValueSet() , and GPCRC_Reset() .
| __IOM uint32_t GPCRC_TypeDef::INPUTDATA | 
Input 32-bit Data Register
        Definition at line
        
         54
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_InputU32() .
| __IOM uint32_t GPCRC_TypeDef::INPUTDATABYTE | 
Input 8-bit Data Register
        Definition at line
        
         56
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_InputU8() .
| __IOM uint32_t GPCRC_TypeDef::INPUTDATAHWORD | 
Input 16-bit Data Register
        Definition at line
        
         55
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_InputU16() .
| __IOM uint32_t GPCRC_TypeDef::POLY | 
CRC Polynomial Value
        Definition at line
        
         53
        
        of file
        
         efr32mg14p_gpcrc.h
        
        .
       
Referenced by GPCRC_Init() , and GPCRC_Reset() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG14P/Include/
       efr32mg14p_gpcrc.h