CMU_TypeDef Struct ReferenceDevices > CMU
CMU Register Declaration
Definition at line 49
of file efr32mg14p_cmu.h
.
#include <
efr32mg14p_cmu.h
>
Data Fields | |
__IOM uint32_t | ADCCTRL |
__IOM uint32_t | AUXHFRCOCTRL |
__IOM uint32_t | CALCNT |
__IOM uint32_t | CALCTRL |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | DBGCLKSEL |
__IOM uint32_t | DPLLCTRL |
__IOM uint32_t | DPLLCTRL1 |
__IOM uint32_t | FREEZE |
__IOM uint32_t | HFBUSCLKEN0 |
__IOM uint32_t | HFCLKSEL |
__IM uint32_t | HFCLKSTATUS |
__IOM uint32_t | HFCOREPRESC |
__IOM uint32_t | HFEXPPRESC |
__IOM uint32_t | HFPERCLKEN0 |
__IOM uint32_t | HFPERPRESC |
__IOM uint32_t | HFPRESC |
__IOM uint32_t | HFRCOCTRL |
__IOM uint32_t | HFRCOSS |
__IOM uint32_t | HFXOCTRL |
__IOM uint32_t | HFXOSTARTUPCTRL |
__IOM uint32_t | HFXOSTEADYSTATECTRL |
__IOM uint32_t | HFXOTIMEOUTCTRL |
__IM uint32_t | HFXOTRIMSTATUS |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | LFACLKEN0 |
__IOM uint32_t | LFACLKSEL |
__IOM uint32_t | LFAPRESC0 |
__IOM uint32_t | LFBCLKEN0 |
__IOM uint32_t | LFBCLKSEL |
__IOM uint32_t | LFBPRESC0 |
__IOM uint32_t | LFECLKEN0 |
__IOM uint32_t | LFECLKSEL |
__IOM uint32_t | LFEPRESC0 |
__IOM uint32_t | LFRCOCTRL |
__IOM uint32_t | LFXOCTRL |
__IOM uint32_t | LOCK |
__IOM uint32_t | OSCENCMD |
__IOM uint32_t | PCNTCTRL |
uint32_t | RESERVED0 [3] |
uint32_t | RESERVED1 [1] |
uint32_t | RESERVED10 [1] |
uint32_t | RESERVED11 [3] |
uint32_t | RESERVED12 [7] |
uint32_t | RESERVED13 [1] |
uint32_t | RESERVED14 [1] |
uint32_t | RESERVED15 [3] |
uint32_t | RESERVED16 [1] |
uint32_t | RESERVED17 [1] |
uint32_t | RESERVED18 [2] |
uint32_t | RESERVED19 [1] |
uint32_t | RESERVED2 [1] |
uint32_t | RESERVED20 [1] |
uint32_t | RESERVED21 [3] |
uint32_t | RESERVED22 [2] |
uint32_t | RESERVED23 [2] |
uint32_t | RESERVED24 [4] |
uint32_t | RESERVED25 [1] |
uint32_t | RESERVED3 [1] |
uint32_t | RESERVED4 [1] |
uint32_t | RESERVED5 [2] |
uint32_t | RESERVED6 [2] |
uint32_t | RESERVED7 [2] |
uint32_t | RESERVED8 [2] |
uint32_t | RESERVED9 [1] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTELOC1 |
__IOM uint32_t | ROUTEPEN |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t CMU_TypeDef::ADCCTRL |
ADC Control Register
Definition at line 130
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::AUXHFRCOCTRL |
AUXHFRCO Control Register
Definition at line 56
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::CALCNT |
Calibration Counter Register
Definition at line 73
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::CALCTRL |
Calibration Control Register
Definition at line 72
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::CMD |
Command Register
Definition at line 76
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::CTRL |
CMU Control Register
Definition at line 50
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::DBGCLKSEL |
Debug Trace Clock Select
Definition at line 78
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::DPLLCTRL |
DPLL Control Register
Definition at line 69
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::DPLLCTRL1 |
DPLL Control Register
Definition at line 70
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::FREEZE |
Freeze Register
Definition at line 125
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFBUSCLKEN0 |
High Frequency Bus Clock Enable Register 0
Definition at line 94
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFCLKSEL |
High Frequency Clock Select Command Register
Definition at line 79
of file efr32mg14p_cmu.h
.
__IM uint32_t CMU_TypeDef::HFCLKSTATUS |
HFCLK Status Register
Definition at line 87
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFCOREPRESC |
High Frequency Core Clock Prescaler Register
Definition at line 110
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFEXPPRESC |
High Frequency Export Clock Prescaler Register
Definition at line 114
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFPERCLKEN0 |
High Frequency Peripheral Clock Enable Register 0
Definition at line 97
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFPERPRESC |
High Frequency Peripheral Clock Prescaler Register
Definition at line 111
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFPRESC |
High Frequency Clock Prescaler Register
Definition at line 107
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFRCOCTRL |
HFRCO Control Register
Definition at line 53
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFRCOSS |
HFRCO Spread Spectrum Register
Definition at line 138
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFXOCTRL |
HFXO Control Register
Definition at line 60
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFXOSTARTUPCTRL |
HFXO Startup Control
Definition at line 63
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFXOSTEADYSTATECTRL |
HFXO Steady State Control
Definition at line 64
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFXOTIMEOUTCTRL |
HFXO Timeout Control
Definition at line 65
of file efr32mg14p_cmu.h
.
__IM uint32_t CMU_TypeDef::HFXOTRIMSTATUS |
HFXO Trim Status
Definition at line 89
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line 93
of file efr32mg14p_cmu.h
.
__IM uint32_t CMU_TypeDef::IF |
Interrupt Flag Register
Definition at line 90
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 92
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 91
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFACLKEN0 |
Low Frequency a Clock Enable Register 0 (Async Reg)
Definition at line 100
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFACLKSEL |
Low Frequency A Clock Select Register
Definition at line 81
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFAPRESC0 |
Low Frequency a Prescaler Register 0 (Async Reg)
Definition at line 117
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFBCLKEN0 |
Low Frequency B Clock Enable Register 0 (Async Reg)
Definition at line 102
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFBCLKSEL |
Low Frequency B Clock Select Register
Definition at line 82
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFBPRESC0 |
Low Frequency B Prescaler Register 0 (Async Reg)
Definition at line 119
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFECLKEN0 |
Low Frequency E Clock Enable Register 0 (Async Reg)
Definition at line 105
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFECLKSEL |
Low Frequency E Clock Select Register
Definition at line 83
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFEPRESC0 |
Low Frequency E Prescaler Register 0 (Async Reg)
Definition at line 121
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFRCOCTRL |
LFRCO Control Register
Definition at line 59
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFXOCTRL |
LFXO Control Register
Definition at line 66
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 137
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::OSCENCMD |
Oscillator Enable/Disable Command Register
Definition at line 75
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::PCNTCTRL |
PCNT Control Register
Definition at line 127
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 52
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 55
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED10[1] |
Reserved for future use
Definition at line 88
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED11[3] |
Reserved for future use
Definition at line 96
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED12[7] |
Reserved for future use
Definition at line 99
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED13[1] |
Reserved for future use
Definition at line 101
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED14[1] |
Reserved for future use
Definition at line 104
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED15[3] |
Reserved for future use
Definition at line 106
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED16[1] |
Reserved for future use
Definition at line 109
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED17[1] |
Reserved for future use
Definition at line 113
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED18[2] |
Reserved for future use
Definition at line 116
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED19[1] |
Reserved for future use
Definition at line 118
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 58
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED20[1] |
Reserved for future use
Definition at line 120
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED21[3] |
Reserved for future use
Definition at line 123
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED22[2] |
Reserved for future use
Definition at line 126
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED23[2] |
Reserved for future use
Definition at line 129
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED24[4] |
Reserved for future use
Definition at line 132
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED25[1] |
Reserved for future use
Definition at line 136
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED3[1] |
Reserved for future use
Definition at line 62
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED4[1] |
Reserved for future use
Definition at line 68
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED5[2] |
Reserved for future use
Definition at line 71
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED6[2] |
Reserved for future use
Definition at line 74
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED7[2] |
Reserved for future use
Definition at line 77
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED8[2] |
Reserved for future use
Definition at line 80
of file efr32mg14p_cmu.h
.
uint32_t CMU_TypeDef::RESERVED9[1] |
Reserved for future use
Definition at line 85
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 134
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::ROUTELOC1 |
I/O Routing Location Register
Definition at line 135
of file efr32mg14p_cmu.h
.
__IOM uint32_t CMU_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line 133
of file efr32mg14p_cmu.h
.
__IM uint32_t CMU_TypeDef::STATUS |
Status Register
Definition at line 86
of file efr32mg14p_cmu.h
.
__IM uint32_t CMU_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 124
of file efr32mg14p_cmu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG14P/Include/
efr32mg14p_cmu.h