ADC_TypeDef Struct ReferenceDevices > ADC
ADC Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32mg14p_adc.h
       
       .
      
      
       #include <
       
     
        efr32mg14p_adc.h
       
       >
      
| Data Fields | |
| __IM uint32_t | APORTCONFLICT | 
| __IOM uint32_t | APORTMASTERDIS | 
| __IM uint32_t | APORTREQ | 
| __IOM uint32_t | BIASPROG | 
| __IOM uint32_t | CAL | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CMPTHR | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [4] | 
| uint32_t | RESERVED2 [3] | 
| __IOM uint32_t | SCANCTRL | 
| __IOM uint32_t | SCANCTRLX | 
| __IM uint32_t | SCANDATA | 
| __IM uint32_t | SCANDATAP | 
| __IM uint32_t | SCANDATAX | 
| __IM uint32_t | SCANDATAXP | 
| __IOM uint32_t | SCANFIFOCLEAR | 
| __IM uint32_t | SCANFIFOCOUNT | 
| __IOM uint32_t | SCANINPUTSEL | 
| __IOM uint32_t | SCANMASK | 
| __IOM uint32_t | SCANNEGSEL | 
| __IOM uint32_t | SINGLECTRL | 
| __IOM uint32_t | SINGLECTRLX | 
| __IM uint32_t | SINGLEDATA | 
| __IM uint32_t | SINGLEDATAP | 
| __IOM uint32_t | SINGLEFIFOCLEAR | 
| __IM uint32_t | SINGLEFIFOCOUNT | 
| __IM uint32_t | STATUS | 
Field Documentation
| __IM uint32_t ADC_TypeDef::APORTCONFLICT | 
APORT Conflict Status Register
        Definition at line
        
         78
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::APORTMASTERDIS | 
APORT Bus Master Disable Register
        Definition at line
        
         83
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IM uint32_t ADC_TypeDef::APORTREQ | 
APORT Request Status Register
        Definition at line
        
         77
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::BIASPROG | 
Bias Programming Register for Various Analog Blocks Used in ADC Operation
        Definition at line
        
         62
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::CAL | 
Calibration Register
        Definition at line
        
         63
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::CMD | 
Command Register
        Definition at line
        
         52
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_Init() , ADC_InitScan() , ADC_InitSingle() , ADC_Reset() , and ADC_Start() .
| __IOM uint32_t ADC_TypeDef::CMPTHR | 
Compare Threshold Register
        Definition at line
        
         61
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_Init() , ADC_InitScan() , ADC_InitSingle() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         67
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_IntDisable() , ADC_IntEnable() , ADC_IntGetEnabled() , and ADC_Reset() .
| __IM uint32_t ADC_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         64
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_IntGet() , and ADC_IntGetEnabled() .
| __IOM uint32_t ADC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         66
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_IntClear() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         65
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_IntSet() .
| uint32_t ADC_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         51
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| uint32_t ADC_TypeDef::RESERVED1[4] | 
Reserved for future use
        Definition at line
        
         72
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| uint32_t ADC_TypeDef::RESERVED2[3] | 
Reserved for future use
        Definition at line
        
         76
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::SCANCTRL | 
Scan Control Register
        Definition at line
        
         56
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SCANCTRLX | 
Scan Control Register Continued
        Definition at line
        
         57
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SCANDATA | 
Scan Conversion Result Data
        Definition at line
        
         69
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_DataScanGet() .
| __IM uint32_t ADC_TypeDef::SCANDATAP | 
Scan Sequence Result Data Peek Register
        Definition at line
        
         71
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_DataScanPeek() .
| __IM uint32_t ADC_TypeDef::SCANDATAX | 
Scan Sequence Result Data + Data Source Register
        Definition at line
        
         73
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_DataIdScanGet() .
| __IM uint32_t ADC_TypeDef::SCANDATAXP | 
Scan Sequence Result Data + Data Source Peek Register
        Definition at line
        
         74
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::SCANFIFOCLEAR | 
Scan FIFO Clear Register
        Definition at line
        
         82
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SCANFIFOCOUNT | 
Scan FIFO Count Register
        Definition at line
        
         80
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IOM uint32_t ADC_TypeDef::SCANINPUTSEL | 
Input Selection Register for Scan Mode
        Definition at line
        
         59
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SCANMASK | 
Scan Sequence Input Mask Register
        Definition at line
        
         58
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SCANNEGSEL | 
Negative Input Select Register for Scan
        Definition at line
        
         60
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitScan() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SINGLECTRL | 
Single Channel Control Register
        Definition at line
        
         54
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and ADC_Reset() .
| __IOM uint32_t ADC_TypeDef::SINGLECTRLX | 
Single Channel Control Register Continued
        Definition at line
        
         55
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SINGLEDATA | 
Single Conversion Result Data
        Definition at line
        
         68
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_DataSingleGet() .
| __IM uint32_t ADC_TypeDef::SINGLEDATAP | 
Single Conversion Result Data Peek Register
        Definition at line
        
         70
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_DataSinglePeek() .
| __IOM uint32_t ADC_TypeDef::SINGLEFIFOCLEAR | 
Single FIFO Clear Register
        Definition at line
        
         81
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_Reset() .
| __IM uint32_t ADC_TypeDef::SINGLEFIFOCOUNT | 
Single FIFO Count Register
        Definition at line
        
         79
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
| __IM uint32_t ADC_TypeDef::STATUS | 
Status Register
        Definition at line
        
         53
        
        of file
        
         efr32mg14p_adc.h
        
        .
       
Referenced by ADC_InitScan() , and ADC_InitSingle() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG14P/Include/
       efr32mg14p_adc.h