CMU_LFXOInit_TypeDef Struct ReferenceEMLIB > CMU
LFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Definition at line 1401
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
uint8_t | ctune |
uint8_t | gain |
CMU_OscMode_TypeDef | mode |
uint8_t | timeout |
Field Documentation
uint8_t CMU_LFXOInit_TypeDef::ctune |
CTUNE (load capacitance) value
Definition at line 1403
of file em_cmu.h
.
Referenced by BSP_initClocks(), and CMU_LFXOInit().
uint8_t CMU_LFXOInit_TypeDef::gain |
CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode |
uint8_t CMU_LFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_cmu.h