SMU_Init_TypeDef Struct ReferenceEMLIB > SMU
SMU initialization structure.
       Definition at line
       
        588
       
       of file
       
        em_smu.h
       
       .
      
      
       #include <
       
     
        em_smu.h
       
       >
      
| Data Fields | |
| bool | enable | 
| union { | |
| SMU_PrivilegedAccess_TypeDef access | |
| uint32_t reg [2] | |
| } | ppu | 
Field Documentation
| SMU_PrivilegedAccess_TypeDef SMU_Init_TypeDef::access | 
Peripheral access control array.
        Definition at line
        
         591
        
        of file
        
         em_smu.h
        
        .
       
| bool SMU_Init_TypeDef::enable | 
SMU enable flag. When set, SMU_Init() will enable SMU.
        Definition at line
        
         593
        
        of file
        
         em_smu.h
        
        .
       
Referenced by SMU_Init() .
| uint32_t SMU_Init_TypeDef::reg[2] | 
Peripheral access control array.
        Definition at line
        
         590
        
        of file
        
         em_smu.h
        
        .
       
Referenced by SMU_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_smu.h