Plugin_ManagerEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Plugin manager, see Plugin System Layer for detailed documentation.

.

Data Structures

struct  EZRADIODRV_HandleData
 

Macros

#define ECODE_EMDRV_EZRADIODRV_AUTO_ACK_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000400)
 Receive plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_CRC_ERROR_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000300)
 CRC error plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_DIRECT_RECEIVE_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000800)
 Receive plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000700)
 Transmit plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000001)
 Illegal SPI handle.
 
#define ECODE_EMDRV_EZRADIODRV_OK   (ECODE_OK)
 Success return value.
 
#define ECODE_EMDRV_EZRADIODRV_PN9_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000600)
 Receive plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_RECEIVE_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000200)
 Receive plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_TRANSMIT_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000100)
 Transmit plugin base error code.
 
#define ECODE_EMDRV_EZRADIODRV_UNMOD_CARRIER_PLUGIN_BASE   (ECODE_EMDRV_EZRADIODRV_BASE | 0x00000500)
 Receive plugin base error code.
 
#define EZRADIODRV_INIT_DEFAULT
 Configuration data for EzRadio plugin manager.
 
#define RADIO_CONFIG_DATA_FIELD_LENGTH
 
#define RADIO_CONFIG_DATA_MAX_PACKET_LENGTH   RADIO_CONFIG_DATA_FIELD1_LENGTH
 

Typedefs

typedef void(* EZRADIODRV_Callback_t) (EZRADIODRV_Handle_t handle, Ecode_t status)
 EZRADIODRV feature callback function interface.
 
typedef EZRADIODRV_HandleData_tEZRADIODRV_Handle_t
 EZRadio driver instance handle.
 
typedef struct EZRADIODRV_HandleData EZRADIODRV_HandleData_t
 Interface for EZRADIODRV_HandleData structure type defined below.
 
typedef ezradio_cmd_reply_t * EZRADIODRV_ReplyHandle_t
 EZradio reply union handle.
 

Functions

void ezradioInit (EZRADIODRV_Handle_t handle)
 Radio Initialization.
 
Ecode_t ezradioPluginManager (EZRADIODRV_Handle_t handle)
 EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly.
 
void ezradioResetTRxFifo (void)
 Resets both the TX and RX FIFOs.
 

Macro Definition Documentation

#define EZRADIODRV_INIT_DEFAULT
Value:
{ \
EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT /* Tx plugin init */ \
EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT /* Rx plugin init */ \
EZRADIODRV_CRC_ERROR_PLUGIN_INIT_DEFAULT /* CRC error plugin init */ \
EZRADIODRV_AUTO_ACK_PLUGIN_INIT_DEFAULT /* Auto-ack plugin init */ \
EZRADIODRV_UNMOD_CARRIER_PLUGIN_INIT_DEFAULT /* CW plugin init */ \
EZRADIODRV_PN9_PLUGIN_INIT_DEFAULT /* PN9 plugin init */ \
EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT /* Direct Tx plugin init */ \
EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT /* Direct Rx plugin init */ \
}

Configuration data for EzRadio plugin manager.

Definition at line 337 of file ezradio_plugin_manager.h.

#define RADIO_CONFIG_DATA_FIELD_LENGTH
Value:
{ \
RADIO_CONFIG_DATA_FIELD1_LENGTH, \
0u, \
0u, \
0u, \
0u, \
}

Definition at line 142 of file ezradio_plugin_manager.h.

Typedef Documentation

typedef void(* EZRADIODRV_Callback_t) (EZRADIODRV_Handle_t handle, Ecode_t status)

EZRADIODRV feature callback function interface.

Parameters
[in]handleEZRadioDrv instance handler.
[in]statusCallback status.
Returns
None

Definition at line 282 of file ezradio_plugin_manager.h.

Function Documentation

void ezradioInit ( EZRADIODRV_Handle_t  handle)

Radio Initialization.

Parameters
[in]handleEzRadio driver instance handler.

Definition at line 81 of file ezradio_plugin_manager.c.

References EZRADIO_CONFIG_SUCCESS, ezradio_configuration_init(), ezradio_get_int_status(), ezradio_hal_GpioInit(), ezradio_hal_SpiInit(), USTIMER_DeInit(), USTIMER_Delay(), and USTIMER_Init().

Ecode_t ezradioPluginManager ( EZRADIODRV_Handle_t  radioHandle)

EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly.

Parameters
[in]radioHandleEzRadio driver instance handler.

Definition at line 126 of file ezradio_plugin_manager.c.

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE, ECODE_EMDRV_EZRADIODRV_OK, and ezradio_get_int_status().