ROMTABLE_TypeDef Struct ReferenceDevices > EZR32WG_ROMTABLE

Definition at line 48 of file ezr32wg_romtable.h.

Data Fields

__IM uint32_t CID0
 
__IM uint32_t PID0
 
__IM uint32_t PID1
 
__IM uint32_t PID2
 
__IM uint32_t PID3
 
__IM uint32_t PID4
 
__IM uint32_t PID5
 
__IM uint32_t PID6
 
__IM uint32_t PID7
 

Field Documentation

__IM uint32_t ROMTABLE_TypeDef::CID0

Unused

Definition at line 57 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID0

Chip family LSB, chip major revision

Definition at line 53 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID1

JEP_106_NO, Chip family MSB

Definition at line 54 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID2

Chip minor rev MSB, JEP_106_PRESENT, JEP_106_NO

Definition at line 55 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID3

Chip minor rev LSB

Definition at line 56 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID4

JEP_106_BANK

Definition at line 49 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID5

Unused

Definition at line 50 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID6

Unused

Definition at line 51 of file ezr32wg_romtable.h.

__IM uint32_t ROMTABLE_TypeDef::PID7

Unused

Definition at line 52 of file ezr32wg_romtable.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/ezr32wg_romtable.h