ACMP_TypeDef Struct ReferenceDevices > EZR32WG_ACMP
Definition at line
48
of file
ezr32wg_acmp.h
.
Data Fields |
|
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INPUTSEL |
__IOM uint32_t | ROUTE |
__IM uint32_t | STATUS |
Field Documentation
__IOM uint32_t ACMP_TypeDef::CTRL |
Control Register
Definition at line
49
of file
ezr32wg_acmp.h
.
Referenced by ACMP_CapsenseInit() , ACMP_Disable() , ACMP_Enable() , ACMP_GPIOSetup() , ACMP_Init() , and ACMP_Reset() .
__IOM uint32_t ACMP_TypeDef::IEN |
Interrupt Enable Register
Definition at line
52
of file
ezr32wg_acmp.h
.
Referenced by ACMP_IntDisable() , ACMP_IntEnable() , ACMP_IntGetEnabled() , and ACMP_Reset() .
__IM uint32_t ACMP_TypeDef::IF |
Interrupt Flag Register
Definition at line
53
of file
ezr32wg_acmp.h
.
Referenced by ACMP_IntGet() , and ACMP_IntGetEnabled() .
__IOM uint32_t ACMP_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
55
of file
ezr32wg_acmp.h
.
Referenced by ACMP_IntClear() , and ACMP_Reset() .
__IOM uint32_t ACMP_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
54
of file
ezr32wg_acmp.h
.
Referenced by ACMP_IntSet() .
__IOM uint32_t ACMP_TypeDef::INPUTSEL |
Input Selection Register
Definition at line
50
of file
ezr32wg_acmp.h
.
Referenced by ACMP_CapsenseChannelSet() , ACMP_CapsenseInit() , ACMP_ChannelSet() , ACMP_Init() , and ACMP_Reset() .
__IOM uint32_t ACMP_TypeDef::ROUTE |
I/O Routing Register
Definition at line
56
of file
ezr32wg_acmp.h
.
Referenced by ACMP_GPIOSetup() .
__IM uint32_t ACMP_TypeDef::STATUS |
Status Register
Definition at line
51
of file
ezr32wg_acmp.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/
ezr32wg_acmp.h