EMU_TypeDef Struct ReferenceDevices > EZR32WG_EMU
Definition at line 48
of file ezr32wg_emu.h
.
Data Fields | |
__IOM uint32_t | AUXCTRL |
__IOM uint32_t | BUACT |
__IOM uint32_t | BUBODBUVINCAL |
__IOM uint32_t | BUBODUNREGCAL |
__IOM uint32_t | BUCTRL |
__IOM uint32_t | BUINACT |
__IOM uint32_t | CTRL |
__IOM uint32_t | EM4CONF |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | LOCK |
__IOM uint32_t | PWRCONF |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [6] |
uint32_t | RESERVED2 [1] |
__IOM uint32_t | ROUTE |
__IM uint32_t | STATUS |
Field Documentation
__IOM uint32_t EMU_TypeDef::AUXCTRL |
Auxiliary Control Register
Definition at line 55
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::BUACT |
Backup mode active configuration register
Definition at line 62
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::BUBODBUVINCAL |
BU_VIN Backup BOD calibration
Definition at line 69
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::BUBODUNREGCAL |
Unregulated power Backup BOD calibration
Definition at line 70
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::BUCTRL |
Backup Power configuration register
Definition at line 59
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::BUINACT |
Backup mode inactive configuration register
Definition at line 61
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::CTRL |
Control Register
Definition at line 49
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::EM4CONF |
Energy mode 4 configuration register
Definition at line 58
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line 68
of file ezr32wg_emu.h
.
__IM uint32_t EMU_TypeDef::IF |
Interrupt Flag Register
Definition at line 65
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 67
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 66
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 52
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::PWRCONF |
Power connection configuration register
Definition at line 60
of file ezr32wg_emu.h
.
uint32_t EMU_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 51
of file ezr32wg_emu.h
.
uint32_t EMU_TypeDef::RESERVED1[6] |
Reserved for future use
Definition at line 54
of file ezr32wg_emu.h
.
uint32_t EMU_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 57
of file ezr32wg_emu.h
.
__IOM uint32_t EMU_TypeDef::ROUTE |
I/O Routing Register
Definition at line 64
of file ezr32wg_emu.h
.
__IM uint32_t EMU_TypeDef::STATUS |
Status register
Definition at line 63
of file ezr32wg_emu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/
ezr32wg_emu.h