DMA_TypeDef Struct ReferenceDevices > EZR32WG_DMA
Definition at line
48
of file
ezr32wg_dma.h
.
Data Fields |
|
| __IM uint32_t | ALTCTRLBASE |
| DMA_CH_TypeDef | CH [12U] |
| __OM uint32_t | CHALTC |
| __IOM uint32_t | CHALTS |
| __OM uint32_t | CHENC |
| __IOM uint32_t | CHENS |
| __OM uint32_t | CHPRIC |
| __IOM uint32_t | CHPRIS |
| __OM uint32_t | CHREQMASKC |
| __IOM uint32_t | CHREQMASKS |
| __IM uint32_t | CHREQSTATUS |
| __IM uint32_t | CHSREQSTATUS |
| __OM uint32_t | CHSWREQ |
| __OM uint32_t | CHUSEBURSTC |
| __IOM uint32_t | CHUSEBURSTS |
| __IM uint32_t | CHWAITSTATUS |
| __OM uint32_t | CONFIG |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | CTRLBASE |
| __IOM uint32_t | ERRORC |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | LOOP0 |
| __IOM uint32_t | LOOP1 |
| __IOM uint32_t | RDS |
| __IOM uint32_t | RECT0 |
| uint32_t | RESERVED0 [3U] |
| uint32_t | RESERVED1 [880U] |
| uint32_t | RESERVED2 [1U] |
| uint32_t | RESERVED3 [121U] |
| uint32_t | RESERVED4 [2U] |
| uint32_t | RESERVED5 [14U] |
| uint32_t | RESERVED6 [39U] |
| __IM uint32_t | STATUS |
Field Documentation
| __IM uint32_t DMA_TypeDef::ALTCTRLBASE |
Channel Alternate Control Data Base Pointer Register
Definition at line
52
of file
ezr32wg_dma.h
.
| DMA_CH_TypeDef DMA_TypeDef::CH[12U] |
Channel registers
Definition at line
88
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CHALTC |
Channel Alternate Clear Register
Definition at line
62
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CHALTS |
Channel Alternate Set Register
Definition at line
61
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CHENC |
Channel Enable Clear Register
Definition at line
60
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CHENS |
Channel Enable Set Register
Definition at line
59
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CHPRIC |
Channel Priority Clear Register
Definition at line
64
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CHPRIS |
Channel Priority Set Register
Definition at line
63
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CHREQMASKC |
Channel Request Mask Clear Register
Definition at line
58
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CHREQMASKS |
Channel Request Mask Set Register
Definition at line
57
of file
ezr32wg_dma.h
.
| __IM uint32_t DMA_TypeDef::CHREQSTATUS |
Channel Request Status
Definition at line
69
of file
ezr32wg_dma.h
.
| __IM uint32_t DMA_TypeDef::CHSREQSTATUS |
Channel Single Request Status
Definition at line
71
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CHSWREQ |
Channel Software Request Register
Definition at line
54
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CHUSEBURSTC |
Channel Useburst Clear Register
Definition at line
56
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CHUSEBURSTS |
Channel Useburst Set Register
Definition at line
55
of file
ezr32wg_dma.h
.
| __IM uint32_t DMA_TypeDef::CHWAITSTATUS |
Channel Wait on Request Status Register
Definition at line
53
of file
ezr32wg_dma.h
.
| __OM uint32_t DMA_TypeDef::CONFIG |
DMA Configuration Register
Definition at line
50
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CTRL |
DMA Control Register
Definition at line
78
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::CTRLBASE |
Channel Control Data Base Pointer Register
Definition at line
51
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::ERRORC |
Bus Error Clear Register
Definition at line
66
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::IEN |
Interrupt Enable register
Definition at line
77
of file
ezr32wg_dma.h
.
| __IM uint32_t DMA_TypeDef::IF |
Interrupt Flag Register
Definition at line
74
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
76
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
75
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::LOOP0 |
Channel 0 Loop Register
Definition at line
82
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::LOOP1 |
Channel 1 Loop Register
Definition at line
83
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::RDS |
DMA Retain Descriptor State
Definition at line
79
of file
ezr32wg_dma.h
.
| __IOM uint32_t DMA_TypeDef::RECT0 |
Channel 0 Rectangle Register
Definition at line
85
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED0[3U] |
Reserved for future use
Definition at line
65
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED1[880U] |
Reserved for future use
Definition at line
68
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED2[1U] |
Reserved for future use
Definition at line
70
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED3[121U] |
Reserved for future use
Definition at line
73
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED4[2U] |
Reserved for future use
Definition at line
81
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED5[14U] |
Reserved for future use
Definition at line
84
of file
ezr32wg_dma.h
.
| uint32_t DMA_TypeDef::RESERVED6[39U] |
Reserved registers
Definition at line
87
of file
ezr32wg_dma.h
.
| __IM uint32_t DMA_TypeDef::STATUS |
DMA Status Registers
Definition at line
49
of file
ezr32wg_dma.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/
ezr32wg_dma.h