USB_EndpointDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB Endpoint Descriptor.
Definition at line
490
of file
em_usb.h
.
#include <
em_usb.h
>
Data Fields |
|
| uint8_t | bDescriptorType |
| uint8_t | bEndpointAddress |
| uint8_t | bInterval |
| uint8_t | bLength |
| uint8_t | bmAttributes |
| uint16_t | wMaxPacketSize |
Field Documentation
| uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType |
Constant ENDPOINT Descriptor Type
Definition at line
492
of file
em_usb.h
.
Referenced by USBH_PrintEndpointDescriptor() .
| uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress |
The address of the endpoint
Definition at line
493
of file
em_usb.h
.
Referenced by USBD_Init() , USBH_AssignHostChannel() , and USBH_PrintEndpointDescriptor() .
| uint8_t USB_EndpointDescriptor_TypeDef::bInterval |
Interval for polling EP for data transfers
Definition at line
496
of file
em_usb.h
.
Referenced by USBH_PrintEndpointDescriptor() , USBH_Read() , and USBH_Write() .
| uint8_t USB_EndpointDescriptor_TypeDef::bLength |
Size of this descriptor in bytes
Definition at line
491
of file
em_usb.h
.
Referenced by USBH_PrintEndpointDescriptor() .
| uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes |
This field describes the endpoint attributes
Definition at line
494
of file
em_usb.h
.
Referenced by USBD_Init() , USBH_AssignHostChannel() , and USBH_PrintEndpointDescriptor() .
| uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize |
Maximum packet size for the endpoint
Definition at line
495
of file
em_usb.h
.
Referenced by USBD_Init() , USBH_AssignHostChannel() , and USBH_PrintEndpointDescriptor() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
em_usb.h