EMU_TypeDef Struct ReferenceDevices > EZR32WG_EMU
Definition at line
47
of file
ezr32wg_emu.h
.
Data Fields |
|
| __IOM uint32_t | AUXCTRL |
| __IOM uint32_t | BUACT |
| __IOM uint32_t | BUBODBUVINCAL |
| __IOM uint32_t | BUBODUNREGCAL |
| __IOM uint32_t | BUCTRL |
| __IOM uint32_t | BUINACT |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | EM4CONF |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | LOCK |
| __IOM uint32_t | PWRCONF |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [6U] |
| uint32_t | RESERVED2 [1U] |
| __IOM uint32_t | ROUTE |
| __IM uint32_t | STATUS |
Field Documentation
| __IOM uint32_t EMU_TypeDef::AUXCTRL |
Auxiliary Control Register
Definition at line
54
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::BUACT |
Backup mode active configuration register
Definition at line
61
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::BUBODBUVINCAL |
BU_VIN Backup BOD calibration
Definition at line
68
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::BUBODUNREGCAL |
Unregulated power Backup BOD calibration
Definition at line
69
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::BUCTRL |
Backup Power configuration register
Definition at line
58
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::BUINACT |
Backup mode inactive configuration register
Definition at line
60
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::CTRL |
Control Register
Definition at line
48
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::EM4CONF |
Energy mode 4 configuration register
Definition at line
57
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line
67
of file
ezr32wg_emu.h
.
| __IM uint32_t EMU_TypeDef::IF |
Interrupt Flag Register
Definition at line
64
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
66
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
65
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line
51
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::PWRCONF |
Power connection configuration register
Definition at line
59
of file
ezr32wg_emu.h
.
| uint32_t EMU_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
50
of file
ezr32wg_emu.h
.
| uint32_t EMU_TypeDef::RESERVED1[6U] |
Reserved for future use
Definition at line
53
of file
ezr32wg_emu.h
.
| uint32_t EMU_TypeDef::RESERVED2[1U] |
Reserved for future use
Definition at line
56
of file
ezr32wg_emu.h
.
| __IOM uint32_t EMU_TypeDef::ROUTE |
I/O Routing Register
Definition at line
63
of file
ezr32wg_emu.h
.
| __IM uint32_t EMU_TypeDef::STATUS |
Status register
Definition at line
62
of file
ezr32wg_emu.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EZR32WG/Include/
ezr32wg_emu.h