LESENSE_DecStAll_TypeDef Struct ReferenceEMLIB > LESENSE

Configuration structure for decoder.

Definition at line 1068 of file em_lesense.h .

#include < em_lesense.h >

Data Fields

LESENSE_DecStDesc_TypeDef St [ LESENSE_NUM_DECODER_STATES ]

Field Documentation

Descriptor of the 16 or 32 decoder states depending on the device.

Definition at line 1070 of file em_lesense.h .

Referenced by LESENSE_DecoderStateAllConfig() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_lesense.h