TOUCH_Pos_TypeDef Struct ReferenceKit Drivers > Touch
Touch panel position structure
       Definition at line
       
        47
       
       of file
       
        touch.h
       
       .
      
      
       #include <
       
     
        touch.h
       
       >
      
| Data Fields | |
| uint16_t | adcx | 
| uint16_t | adcy | 
| uint8_t | pen | 
| uint16_t | x | 
| uint16_t | y | 
Field Documentation
| uint16_t TOUCH_Pos_TypeDef::adcx | 
ADC X readings
        Definition at line
        
         50
        
        of file
        
         touch.h
        
        .
       
Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , and TOUCH_RecalculatePosition() .
| uint16_t TOUCH_Pos_TypeDef::adcy | 
ADC Y readings
        Definition at line
        
         51
        
        of file
        
         touch.h
        
        .
       
Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , and TOUCH_RecalculatePosition() .
| uint8_t TOUCH_Pos_TypeDef::pen | 
0=not pressed, 1=touched
        Definition at line
        
         52
        
        of file
        
         touch.h
        
        .
       
Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , TOUCH_RecalculatePosition() , and TOUCH_StateChanged() .
| uint16_t TOUCH_Pos_TypeDef::x | 
x position
        Definition at line
        
         48
        
        of file
        
         touch.h
        
        .
       
Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , TOUCH_RecalculatePosition() , and TOUCH_StateChanged() .
| uint16_t TOUCH_Pos_TypeDef::y | 
y position
        Definition at line
        
         49
        
        of file
        
         touch.h
        
        .
       
Referenced by ADC0_IRQHandler() , TOUCH_GetPos() , TOUCH_RecalculatePosition() , and TOUCH_StateChanged() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/hardware/kit/common/drivers/
       touch.h