LESENSE_CoreCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE

Core control (LESENSE_CTRL) descriptor structure.

Definition at line 488 of file em_lesense.h .

#include < em_lesense.h >

Data Fields

LESENSE_BiasMode_TypeDef biasMode
bool bufOverWr
LESENSE_BufTrigLevel_TypeDef bufTrigLevel
bool debugRun
bool dualSample
bool invACMP0
bool invACMP1
LESENSE_PRSSel_TypeDef prsSel
LESENSE_ScanConfSel_TypeDef scanConfSel
LESENSE_ScanMode_TypeDef scanStart
bool storeScanRes
LESENSE_DMAWakeUp_TypeDef wakeupOnDMA

Field Documentation

LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode

Select bias mode.

Definition at line 522 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr

Set to true in order to always make LESENSE write to the result buffer, even if it is full.

Definition at line 513 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel

Select trigger conditions for the interrupt and DMA.

Definition at line 516 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_CoreCtrlDesc_TypeDef::debugRun

Set to true to keep LESENSE running in the debug mode.

Definition at line 525 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_CoreCtrlDesc_TypeDef::dualSample

Set to true to sample both ACMPs simultaneously.

Definition at line 505 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0

Set to true to invert ACMP0 output.

Definition at line 499 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1

Set to true to invert ACMP1 output.

Definition at line 502 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel

Select PRS source for scan start if scanMode is set to lesensePrsPulse.

Definition at line 493 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel

Select scan configuration register usage strategy.

Definition at line 496 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart

Select scan start mode to control how the scan start is being triggered.

Definition at line 490 of file em_lesense.h .

Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_Init() .

bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes

Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.

Definition at line 509 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA

Configure trigger condition for the DMA wakeup from EM2.

Definition at line 519 of file em_lesense.h .

Referenced by LESENSE_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/ em_lesense.h