Common BSP for all kitsBSP
         Macros | 
       |
| #define | BSP_INIT_BCC 0x04 | 
| #define | BSP_INIT_DK_EBI 0x02 | 
| #define | BSP_INIT_DK_SPI 0x01 | 
| #define | BSP_INIT_IOEXP 0x08 | 
| #define | BSP_STATUS_ILLEGAL_PARAM (-1) | 
| #define | BSP_STATUS_IOEXP_FAILURE (-4) | 
| #define | BSP_STATUS_NOT_IMPLEMENTED (-2) | 
| #define | BSP_STATUS_OK 0 | 
| #define | BSP_STATUS_UNSUPPORTED_MODE (-3) | 
         Functions | 
       |
| int | BSP_Disable (void) | 
| 
         Deinitialize board support package functionality. Reverse actions performed by
         
          BSP_Init()
         
         . This function is a dummy on STK's.
          | 
       |
| int | BSP_Init (uint32_t flags) | 
| 
         Initialize board support package functionality.
          | 
       |
| int | BSP_LedClear (int ledNo) | 
| 
         Turn off a single LED.
          | 
       |
| int | BSP_LedGet (int ledNo) | 
| 
         Get current status of a single LED.
          | 
       |
| int | BSP_LedSet (int ledNo) | 
| 
         Turn on a single LED.
          | 
       |
| uint32_t | BSP_LedsGet (void) | 
| 
         Get status of all LEDs.
          | 
       |
| int | BSP_LedsInit (void) | 
| 
         Initialize LED drivers.
          | 
       |
| int | BSP_LedsSet (uint32_t leds) | 
| 
         Update all LED's.
          | 
       |
| int | BSP_LedToggle (int ledNo) | 
| 
         Toggle a single LED.
          | 
       |
| int | BSP_PeripheralAccess ( BSP_Peripheral_TypeDef perf, bool enable) | 
| 
         DK Peripheral Access Control Enable or disable access to on-board peripherals through switches and SPI switch where applicable. Turn off conflicting peripherals when enabling another.
          | 
       |
| bool | BSP_TraceProfilerSetup (void) | 
| 
         Configure SWO trace output for Energy Profiler.
          | 
       |
| void | BSP_TraceSwoSetup (void) | 
| 
         Energy Profiler SWO setup.
          | 
       |
Macro Definition Documentation
| #define BSP_INIT_BCC 0x04 | 
Mode flag for BSP_Init() , init board controller communication.
        Definition at line
        
         58
        
        of file
        
         bsp.h
        
        .
       
| #define BSP_INIT_DK_EBI 0x02 | 
Mode flag for BSP_Init() , init DK in EBI mode (DK3x50 only).
        Definition at line
        
         57
        
        of file
        
         bsp.h
        
        .
       
Referenced by BSP_Disable() , BSP_Init() , BSP_RegisterRead() , and BSP_RegisterWrite() .
| #define BSP_INIT_DK_SPI 0x01 | 
Mode flag for BSP_Init() , init DK in SPI mode (DK3x50 only).
        Definition at line
        
         56
        
        of file
        
         bsp.h
        
        .
       
Referenced by BSP_Disable() , and BSP_Init() .
| #define BSP_INIT_IOEXP 0x08 | 
Mode flag for BSP_Init() , init io-expander on some radio boards
        Definition at line
        
         59
        
        of file
        
         bsp.h
        
        .
       
Referenced by BSP_initBoard() .
| #define BSP_STATUS_ILLEGAL_PARAM (-1) | 
BSP API return code, illegal input parameter.
        Definition at line
        
         50
        
        of file
        
         bsp.h
        
        .
       
Referenced by BSP_BusControlModeSet() , BSP_LedClear() , BSP_LedGet() , BSP_LedSet() , and BSP_LedToggle() .
| #define BSP_STATUS_IOEXP_FAILURE (-4) | 
BSP API return code, io-expander communication failed
        Definition at line
        
         53
        
        of file
        
         bsp.h
        
        .
       
| #define BSP_STATUS_NOT_IMPLEMENTED (-2) | 
BSP API return code, function not implemented (dummy).
        Definition at line
        
         51
        
        of file
        
         bsp.h
        
        .
       
Referenced by BSP_EbiDeInit() , BSP_EbiInit() , BSP_McuBoard_UsbStatusLedEnable() , and BSP_McuBoard_UsbVbusPowerEnable() .
| #define BSP_STATUS_OK 0 | 
BSP API return code, no errors.
        Definition at line
        
         49
        
        of file
        
         bsp.h
        
        .
       
Referenced by BSP_BccDeInit() , BSP_BccInit() , BSP_BccPacketSend() , BSP_BusControlModeSet() , BSP_Disable() , BSP_DisplayControl() , BSP_EbiDeInit() , BSP_EbiExtendedAddressRange() , BSP_EbiInit() , BSP_EnergyModeSet() , BSP_Init() , BSP_InterruptDisable() , BSP_InterruptEnable() , BSP_InterruptFlagsClear() , BSP_InterruptFlagsSet() , BSP_LedClear() , BSP_LedSet() , BSP_LedsInit() , BSP_LedsSet() , BSP_LedToggle() , BSP_McuBoard_DeInit() , BSP_McuBoard_Init() , BSP_McuBoard_UsbStatusLedEnable() , BSP_McuBoard_UsbVbusPowerEnable() , BSP_PeripheralAccess() , and BSP_RegisterWrite() .
| #define BSP_STATUS_UNSUPPORTED_MODE (-3) | 
BSP API return code, unsupported BSP mode.
        Definition at line
        
         52
        
        of file
        
         bsp.h
        
        .
       
Function Documentation
| int BSP_Disable | ( | void | 
           
           
           | 
          ) | 
Deinitialize board support package functionality. Reverse actions performed by BSP_Init() . This function is a dummy on STK's.
- Returns
 - BSP_STATUS_OK on DK's, BSP_STATUS_NOT_IMPLEMENTED on STK's.
 
        Definition at line
        
         104
        
        of file
        
         bsp_dk_3201.c
        
        .
       
References BSP_BusControl_OFF , BSP_BusControlModeSet() , BSP_INIT_DK_EBI , BSP_INIT_DK_SPI , and BSP_STATUS_OK .
| int BSP_Init | ( | uint32_t | 
           
            flags
           
           | 
          ) | 
Initialize board support package functionality.
- Parameters
 - 
         
[in] flagsDK3x50: Initialize in EBI or SPI mode using BSP_INIT_DK_EBI or BSP_INIT_DK_SPI . Gxxx_DK: Use 0. STK: Use BSP_INIT_BCC to initialize board controller UART, 0 otherwise.  
The value BSP_INIT_DEFAULT is defined and is: BSP_INIT_DK_EBI on DK3x50, 0 on all other kits.
- Returns
 - BSP_STATUS_OK
 
        Definition at line
        
         132
        
        of file
        
         bsp_dk_3201.c
        
        .
       
References BC_REGISTER , BSP_BusControl_EBI , BSP_BusControl_SPI , BSP_BusControlModeSet() , BSP_INIT_DK_EBI , BSP_INIT_DK_SPI , BSP_RegisterRead() , BSP_RegisterWrite() , and BSP_STATUS_OK .
Referenced by BSP_initBoard() .
| int BSP_LedClear | ( | int | 
           
            ledNo
           
           | 
          ) | 
Turn off a single LED.
- Parameters
 - 
         
[in] ledNoThe number of the LED (counting from zero) to turn off.  
- Returns
 - BSP_STATUS_OK or BSP_STATUS_ILLEGAL_PARAM if illegal LED number.
 
        Definition at line
        
         72
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterRead() , BSP_RegisterWrite() , BSP_STATUS_ILLEGAL_PARAM , and BSP_STATUS_OK .
| int BSP_LedGet | ( | int | 
           
            ledNo
           
           | 
          ) | 
Get current status of a single LED.
- Parameters
 - 
         
[in] ledNoThe number of the LED (counting from zero) to check.  
- Returns
 - 1 if LED is on, 0 if LED is off, BSP_STATUS_ILLEGAL_PARAM if illegal LED number.
 
        Definition at line
        
         92
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterRead() , and BSP_STATUS_ILLEGAL_PARAM .
| int BSP_LedSet | ( | int | 
           
            ledNo
           
           | 
          ) | 
Turn on a single LED.
- Parameters
 - 
         
[in] ledNoThe number of the LED (counting from zero) to turn on.  
- Returns
 - BSP_STATUS_OK or BSP_STATUS_ILLEGAL_PARAM if illegal LED number.
 
        Definition at line
        
         110
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterRead() , BSP_RegisterWrite() , BSP_STATUS_ILLEGAL_PARAM , and BSP_STATUS_OK .
| uint32_t BSP_LedsGet | ( | void | 
           
           
           | 
          ) | 
Get status of all LEDs.
- Returns
 - Bitmask with current status for all LED's.
 
        Definition at line
        
         48
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterRead() .
| int BSP_LedsInit | ( | void | 
           
           
           | 
          ) | 
Initialize LED drivers.
- Note
 - LED's are initially turned off.
 
- Returns
 - BSP_STATUS_OK
 
        Definition at line
        
         37
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterWrite() , and BSP_STATUS_OK .
Referenced by BSP_initBoard() .
| int BSP_LedsSet | ( | uint32_t | 
           
            leds
           
           | 
          ) | 
Update all LED's.
- Parameters
 - 
         
[in] ledsBitmask representing new status for all LED's. A 1 turns a LED on, a 0 turns a LED off.  
- Returns
 - BSP_STATUS_OK
 
        Definition at line
        
         60
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterWrite() , and BSP_STATUS_OK .
| int BSP_LedToggle | ( | int | 
           
            ledNo
           
           | 
          ) | 
Toggle a single LED.
- Parameters
 - 
         
[in] ledNoThe number of the LED (counting from zero) to toggle.  
- Returns
 - BSP_STATUS_OK or BSP_STATUS_ILLEGAL_PARAM if illegal LED number.
 
        Definition at line
        
         129
        
        of file
        
         bsp_dk_leds.c
        
        .
       
References BSP_RegisterRead() , BSP_RegisterWrite() , BSP_STATUS_ILLEGAL_PARAM , and BSP_STATUS_OK .
| int BSP_PeripheralAccess | ( | BSP_Peripheral_TypeDef | 
           
            perf,
           
           | 
         
| bool | 
           
            enable
           
           | 
         ||
| ) | 
DK Peripheral Access Control Enable or disable access to on-board peripherals through switches and SPI switch where applicable. Turn off conflicting peripherals when enabling another.
- Parameters
 - 
         
[in] perfWhich peripheral to configure. Use enum BSP_Peripheral_TypeDef or BSP_Peripheral_Typedef according to DK type. [in] enableIf true, set up access to peripheral, if false disable access.  
- Returns
 - BSP_STATUS_OK .
 
        Definition at line
        
         459
        
        of file
        
         bsp_dk_3201.c
        
        .
       
References BC_PERICON_ANALOG_DIFF_SHIFT , BC_PERICON_ANALOG_SE_SHIFT , BC_PERICON_AUDIO_IN_SHIFT , BC_PERICON_AUDIO_OUT_SEL_SHIFT , BC_PERICON_AUDIO_OUT_SHIFT , BC_PERICON_I2C_SHIFT , BC_PERICON_I2S_ETH_SEL_SHIFT , BC_PERICON_I2S_ETH_SHIFT , BC_PERICON_RS232_LEUART_SHIFT , BC_PERICON_RS232_SHUTDOWN_SHIFT , BC_PERICON_RS232_UART_SHIFT , BC_PERICON_SPI_SHIFT , BC_PERICON_TOUCH_SHIFT , BC_PERICON_TRACE_SHIFT , BC_REGISTER , BSP_ANALOG_DIFF , BSP_ANALOG_SE , BSP_AUDIO_IN , BSP_AUDIO_OUT , BSP_ETH , BSP_I2C , BSP_I2S , BSP_MICROSD , BSP_RegisterRead() , BSP_RegisterWrite() , BSP_RS232_LEUART , BSP_RS232_SHUTDOWN , BSP_RS232_UART , BSP_STATUS_OK , BSP_TFT , BSP_TOUCH , and BSP_TRACE .
Referenced by BSP_initBoard() , TFT_DirectInit() , and TOUCH_Init() .
| bool BSP_TraceProfilerSetup | ( | void | 
           
           
           | 
          ) | 
Configure SWO trace output for Energy Profiler.
- Note
 - Enabling SWO trace will add ~150uA current consumption in EM0.
 
- Returns
 - Always true
 
        Definition at line
        
         106
        
        of file
        
         bsp_trace.c
        
        .
       
References CMU_ClockFreqGet() , and cmuClock_DBG .
Referenced by BSP_TraceSwoSetup() .
| void BSP_TraceSwoSetup | ( | void | 
           
           
           | 
          ) | 
Energy Profiler SWO setup.
- 
         
          
Deprecated: - Deprecated function. New code should call BSP_TraceProfilerSetup() .
 
        Definition at line
        
         183
        
        of file
        
         bsp_trace.c
        
        .
       
References BSP_TraceProfilerSetup() .
Referenced by RETARGET_SwoInit() .