BCP_Packet_ Struct ReferenceBSP > API for STKs and WSTKs
BCP Packet Structure - Board controller communication protocol version 1.
       Definition at line
       
        75
       
       of file
       
        bsp_bcp.h
       
       .
      
      
       #include <
       
     
        bsp_bcp.h
       
       >
      
         Data Fields | 
       |
| uint8_t | data [ BSP_BCP_PACKET_SIZE ] | 
| uint8_t | magic | 
| uint8_t | payloadLength | 
| uint8_t | type | 
Field Documentation
| uint8_t BCP_Packet_::data[ BSP_BCP_PACKET_SIZE ] | 
BCP Packet Data payload
        Definition at line
        
         79
        
        of file
        
         bsp_bcp.h
        
        .
       
| uint8_t BCP_Packet_::magic | 
Magic - start of packet - must be BSP_BCP_MAGIC
        Definition at line
        
         76
        
        of file
        
         bsp_bcp.h
        
        .
       
| uint8_t BCP_Packet_::payloadLength | 
Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE
        Definition at line
        
         78
        
        of file
        
         bsp_bcp.h
        
        .
       
| uint8_t BCP_Packet_::type | 
Type of packet
        Definition at line
        
         77
        
        of file
        
         bsp_bcp.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/hardware/kit/common/bsp/
       
bsp_bcp.h