Gecko USB MSDKit Drivers
Detailed Description
USB Mass Storage Class (MSC).
MSC Implementation for Device
      The source code of the device implementation resides in kits/common/drivers/msdd.c and
      
       msdd.h
      
      . The driver includes "msddmedia.h" to get the API definitions needed for media access. The drivers use the Bulk-Only Transport (BOT) mode of the MSC specification.
     
MSC Device Configuration Options
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file.
// USB interface number. Interfaces are numbered from zero to one less than // the number of concurrent interfaces supported by the configuration. // The interface number must be 0 for a standalone MSC device, for a // composite device which includes a MSC interface it must not be in conflict // with other device interfaces. #define MSD_INTERFACE_NO ( 0 ) // Endpoint address for data reception. #define MSD_BULK_OUT ( 0x01 ) // Endpoint address for data transmission. #define MSD_BULK_IN ( 0x81 )
         Data Structures | 
       |
| struct | MSDBOT_CBW_TypeDef | 
| 
         Bulk Only Transport (BOT) Command Block Wrapper (CBW) typedef.
          | 
       |
| struct | MSDBOT_CSW_TypeDef | 
| 
         Bulk Only Transport (BOT) Command Status Wrapper (CSW) typedef.
          | 
       |
| struct | MSDD_CmdStatus_TypeDef | 
| 
         Status info for one BOT CBW -> Data I/O -> CSW cycle.
          | 
       |
| struct | MSDSCSI_Inquiry_TypeDef | 
| 
         SCSI Inquiry Command Descriptor Block (CDB) typedef.
          | 
       |
| struct | MSDSCSI_InquiryData_TypeDef | 
| 
         SCSI Inquiry response data typedef.
          | 
       |
| struct | MSDSCSI_Read10_TypeDef | 
| 
         SCSI Read 10 Command Descriptor Block (CDB) typedef.
          | 
       |
| struct | MSDSCSI_ReadCapacity_TypeDef | 
| 
         SCSI Read Capacity Command Descriptor Block (CDB) typedef.
          | 
       |
| struct | MSDSCSI_ReadCapacityData_TypeDef | 
| 
         SCSI Read Capacity response data typedef.
          | 
       |
| struct | MSDSCSI_RequestSense_TypeDef | 
| 
         SCSI Request Sense Command Descriptor Block (CDB) typedef.
          | 
       |
| struct | MSDSCSI_RequestSenseData_TypeDef | 
| 
         SCSI Request Sense response data typedef.
          | 
       |
| struct | MSDSCSI_StartStopUnit_TypeDef | 
| 
         SCSI Start Stop Unit Command Descriptor Block (CDB) typedef.
          | 
       |
| struct | MSDSCSI_Verify10_TypeDef | 
| 
         SCSI Verify 10 Command Descriptor Block (CDB) typedef.
          | 
       |
| struct | MSDSCSI_Write10_TypeDef | 
| 
         SCSI Write 10 Command Descriptor Block (CDB) typedef.
          | 
       |
         Macros | 
       |
| #define | MEDIA_BUFSIZ 4096 | 
| #define | SCSI_INQUIRY 0x12 | 
| #define | SCSI_INQUIRYDATA_LEN 36U | 
| #define | SCSI_READ10 0x28 | 
| #define | SCSI_READ10_LEN 10U | 
| #define | SCSI_READCAPACITY 0x25 | 
| #define | SCSI_READCAPACITY_LEN 10U | 
| #define | SCSI_READCAPACITYDATA_LEN 8U | 
| #define | SCSI_REQUESTSENSE 0x03 | 
| #define | SCSI_REQUESTSENSE_LEN 6U | 
| #define | SCSI_REQUESTSENSEDATA_LEN 18U | 
| #define | SCSI_STARTSTOP_UNIT 0x1B | 
| #define | SCSI_STARTSTOPUNIT_LEN 6U | 
| #define | SCSI_TESTUNIT_READY 0x00 | 
| #define | SCSI_VERIFY10 0x2F | 
| #define | SCSI_VERIFY10_LEN 10U | 
| #define | SCSI_WRITE10 0x2A | 
| #define | SCSI_WRITE10_LEN 10U | 
         Enumerations | 
       |
| enum | 
         
          MSDBOT_Status_TypeDef
         
         {
          MSDBOT_STATUS_OK = 0, MSDBOT_INIT_ERROR = -1, MSDBOT_CMD_FAILED = -2, MSDBOT_XFER_ERROR = -3 }  | 
       
| 
         MSDBOT status enumerator.
          | 
       |
         Functions | 
       |
| int | MSDBOT_Init (USBH_Ep_TypeDef *out, USBH_Ep_TypeDef *in) | 
| 
         MSDBOT module initialization.
          | 
       |
| int | MSDBOT_Xfer (void *cbw, void *data) | 
| 
         Perform an MSD Bulk Only Transfer (BOT).
          | 
       |
| bool | MSDD_Handler (void) | 
| 
         Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler.
          | 
       |
| void | MSDD_Init (int activityLedPort, uint32_t activityLedPin) | 
| 
         Initialize MSD device.
          | 
       |
| int | MSDD_SetupCmd (const USB_Setup_TypeDef *setup) | 
| 
         Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN".
          | 
       |
| void | MSDD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| 
         Called whenever the USB device has changed its device state.
          | 
       |
| bool | MSDH_GetBlockSize (uint32_t *blockSize) | 
| 
         Get blocksize from the device.
          | 
       |
| bool | MSDH_GetSectorCount (uint32_t *sectorCount) | 
| 
         Get sectorcount from the device.
          | 
       |
| bool | MSDH_GetSectorSize (uint16_t *sectorSize) | 
| 
         Get sectorsize from the device.
          | 
       |
| bool | MSDH_Init (uint8_t *usbDeviceInfo, int usbDeviceInfoSize) | 
| 
         Initialize an USB connected Mass Storage Device. Checks if the device is a valid MSD device. Will perform all necessary MSD initialization.
          | 
       |
| bool | MSDH_ReadSectors (uint32_t lba, uint16_t sectors, void *data) | 
| 
         Read sectors from device.
          | 
       |
| bool | MSDH_WriteSectors (uint32_t lba, uint16_t sectors, const void *data) | 
| 
         Write sectors to device.
          | 
       |
Macro Definition Documentation
| #define MEDIA_BUFSIZ 4096 | 
Intermediate media storage buffer size
        Definition at line
        
         34
        
        of file
        
         msdd.h
        
        .
       
| #define SCSI_INQUIRY 0x12 | 
SCSI Inquiry command opcode.
        Definition at line
        
         37
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_INQUIRYDATA_LEN 36U | 
SCSI Inquiry response data length.
        Definition at line
        
         47
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() , MSDSCSI_Init() , and MSDSCSI_Inquiry() .
| #define SCSI_READ10 0x28 | 
SCSI Read (10) command opcode.
        Definition at line
        
         40
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_READ10_LEN 10U | 
SCSI Read (10) CBD length.
        Definition at line
        
         44
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() , and MSDSCSI_Init() .
| #define SCSI_READCAPACITY 0x25 | 
SCSI Read Capacity command opcode.
        Definition at line
        
         39
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_READCAPACITY_LEN 10U | 
SCSI Read Capacity CDB length.
        Definition at line
        
         51
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() .
| #define SCSI_READCAPACITYDATA_LEN 8U | 
SCSI Read Capacity response data length.
        Definition at line
        
         52
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() , MSDSCSI_Init() , and MSDSCSI_ReadCapacity() .
| #define SCSI_REQUESTSENSE 0x03 | 
SCSI Request Sense command opcode.
        Definition at line
        
         36
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_REQUESTSENSE_LEN 6U | 
SCSI Request Sense CDB length.
        Definition at line
        
         49
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() .
| #define SCSI_REQUESTSENSEDATA_LEN 18U | 
SCSI Request Sense response data length.
        Definition at line
        
         50
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() , MSDSCSI_Init() , and MSDSCSI_RequestSense() .
| #define SCSI_STARTSTOP_UNIT 0x1B | 
SCSI Start Stop Unit command opcode.
        Definition at line
        
         38
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Handler() .
| #define SCSI_STARTSTOPUNIT_LEN 6U | 
SCSI Start Stop Unit CDB length.
        Definition at line
        
         48
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() .
| #define SCSI_TESTUNIT_READY 0x00 | 
SCSI Test Unit Ready command opcode.
        Definition at line
        
         35
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_VERIFY10 0x2F | 
SCSI Verify (10) command opcode.
        Definition at line
        
         42
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_VERIFY10_LEN 10U | 
| #define SCSI_WRITE10 0x2A | 
SCSI Write (10) command opcode.
        Definition at line
        
         41
        
        of file
        
         msdscsi.h
        
        .
       
| #define SCSI_WRITE10_LEN 10U | 
SCSI Write (10) CDB length.
        Definition at line
        
         45
        
        of file
        
         msdscsi.h
        
        .
       
Referenced by MSDD_Init() , and MSDSCSI_Init() .
Enumeration Type Documentation
Function Documentation
| int MSDBOT_Init | ( | USBH_Ep_TypeDef * | 
           
            out,
           
           | 
         
| USBH_Ep_TypeDef * | 
           
            in
           
           | 
         ||
| ) | 
MSDBOT module initialization.
- Parameters
 - 
         
[in] outPointer to an MSD bulk OUT endpoint structure. [in] inPointer to an MSD bulk IN endpoint structure.  
- Returns
 - MSDBOT_STATUS_OK on success, else MSDBOT_INIT_ERROR .
 
        Definition at line
        
         69
        
        of file
        
         msdbot.c
        
        .
       
References MSDBOT_INIT_ERROR , and MSDBOT_STATUS_OK .
Referenced by MSDSCSI_Init() .
| int MSDBOT_Xfer | ( | void * | 
           
            cbw,
           
           | 
         
| void * | 
           
            data
           
           | 
         ||
| ) | 
Perform an MSD Bulk Only Transfer (BOT).
- Parameters
 - 
         
[in] cbwPointer to a Command Block Wrapper (CBW) data structure. [in] dataData buffer for data to be transferred.  
- Returns
 - 
         A positive (or zero) value indicating the number of bytes transferred.
         
A negative value indicates a transfer error code enumerated in MSDBOT_Status_TypeDef . 
        Definition at line
        
         109
        
        of file
        
         msdbot.c
        
        .
       
References MSDBOT_CSW_TypeDef::bCSWStatus , MSDBOT_CBW_TypeDef::dCBWDataTransferLength , MSDBOT_CBW_TypeDef::Direction , MSDBOT_CMD_FAILED , and MSDBOT_XFER_ERROR .
Referenced by MSDSCSI_Inquiry() , MSDSCSI_Read10() , MSDSCSI_ReadCapacity() , MSDSCSI_RequestSense() , MSDSCSI_TestUnitReady() , and MSDSCSI_Write10() .
| bool MSDD_Handler | ( | void | 
           
           
           | 
          ) | 
Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler.
- Returns
 - Returns true if there is no pending tasks to perform. This means that energymodes (sleep) functionality can be used.
 
        Definition at line
        
         258
        
        of file
        
         msdd.c
        
        .
       
References MSDBOT_CBW_TypeDef::CBWCB , SCSI_STARTSTOP_UNIT , and SL_MIN .
| void MSDD_Init | ( | int | 
           
            activityLedPort,
           
           | 
         
| uint32_t | 
           
            activityLedPin
           
           | 
         ||
| ) | 
Initialize MSD device.
- Parameters
 - 
         
[in] activityLedPortSpecify a GPIO port for a LED activity indicator (i.e. enum gpioPortX) Pass -1 if no indicator LED is available. [in] activityLedPinPin number on activityLedPort for the LED activity indicator.  
        Definition at line
        
         216
        
        of file
        
         msdd.c
        
        .
       
References CMU_ClockEnable() , cmuClock_GPIO , GPIO_PinModeSet() , gpioModePushPull , SCSI_INQUIRYDATA_LEN , SCSI_READ10_LEN , SCSI_READCAPACITY_LEN , SCSI_READCAPACITYDATA_LEN , SCSI_REQUESTSENSE_LEN , SCSI_REQUESTSENSEDATA_LEN , SCSI_STARTSTOPUNIT_LEN , SCSI_VERIFY10_LEN , and SCSI_WRITE10_LEN .
| int MSDD_SetupCmd | ( | const USB_Setup_TypeDef * | 
           
            setup
           
           | 
          ) | 
Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN".
- Parameters
 - 
         
[in] setupPointer to an USB setup packet.  
- Returns
 - An appropriate status/error code. See USB_Status_TypeDef.
 
        Definition at line
        
         321
        
        of file
        
         msdd.c
        
        .
       
| void MSDD_StateChangeEvent | ( | USBD_State_TypeDef | 
           
            oldState,
           
           | 
         
| USBD_State_TypeDef | 
           
            newState
           
           | 
         ||
| ) | 
Called whenever the USB device has changed its device state.
- Parameters
 - 
         
[in] oldStateThe device USB state just leaved. See USBD_State_TypeDef. [in] newStateNew (the current) USB device state. See USBD_State_TypeDef.  
        Definition at line
        
         396
        
        of file
        
         msdd.c
        
        .
       
| bool MSDH_GetBlockSize | ( | uint32_t * | 
           
            blockSize
           
           | 
          ) | 
Get blocksize from the device.
- Note
 - This function assumes that block size equals sector size.
 
- Parameters
 - 
         
[out] blockSizeThe block size of device storage memory.  
- Returns
 - Returns true on success, false otherwise.
 
        Definition at line
        
         238
        
        of file
        
         msdh.c
        
        .
       
References MSDSCSI_ReadCapacity() , SL_ALIGN , and SL_ATTRIBUTE_ALIGN .
| bool MSDH_GetSectorCount | ( | uint32_t * | 
           
            sectorCount
           
           | 
          ) | 
Get sectorcount from the device.
- Parameters
 - 
         
[out] sectorCountNumber of sectors on the device.  
- Returns
 - Returns true on success, false otherwise.
 
        Definition at line
        
         187
        
        of file
        
         msdh.c
        
        .
       
References MSDSCSI_ReadCapacity() , SL_ALIGN , and SL_ATTRIBUTE_ALIGN .
| bool MSDH_GetSectorSize | ( | uint16_t * | 
           
            sectorSize
           
           | 
          ) | 
Get sectorsize from the device.
- Parameters
 - 
         
[out] sectorSizeThe size of device sectors.  
- Returns
 - Returns true on success, false otherwise.
 
        Definition at line
        
         211
        
        of file
        
         msdh.c
        
        .
       
References MSDSCSI_ReadCapacity() , SL_ALIGN , and SL_ATTRIBUTE_ALIGN .
| bool MSDH_Init | ( | uint8_t * | 
           
            usbDeviceInfo,
           
           | 
         
| int | 
           
            usbDeviceInfoSize
           
           | 
         ||
| ) | 
Initialize an USB connected Mass Storage Device. Checks if the device is a valid MSD device. Will perform all necessary MSD initialization.
- Note
 - This function assumes that prior calls to USBH_Init() and USBH_WaitForDeviceConnectionB() have been performed. The contents of the usbDeviceInfo data buffer will be overwritten.
 
- Parameters
 - 
         
[in] usbDeviceInfoPointer to USB enumeration information. usbDeviceInfo must have been initialized by a prior call to USBH_WaitForDeviceConnectionB(). [in] usbDeviceInfoSizeThe size of the usbDeviceInfo data buffer.  
- Returns
 - Returns true on success, false otherwise.
 
        Definition at line
        
         72
        
        of file
        
         msdh.c
        
        .
       
References MSDSCSI_Init() , MSDSCSI_Inquiry() , MSDSCSI_ReadCapacity() , MSDSCSI_RequestSense() , MSDSCSI_TestUnitReady() , SL_ALIGN , and SL_ATTRIBUTE_ALIGN .
| bool MSDH_ReadSectors | ( | uint32_t | 
           
            lba,
           
           | 
         
| uint16_t | 
           
            sectors,
           
           | 
         ||
| void * | 
           
            data
           
           | 
         ||
| ) | 
Read sectors from device.
- Parameters
 - 
         
[in] lbaSector address (LBA) of first sector to read. [in] sectorsNumber of sectors to read. [out] dataData buffer through which data is returned to caller.  
- Returns
 - Returns true on success, false otherwise.
 
        Definition at line
        
         268
        
        of file
        
         msdh.c
        
        .
       
References MSDSCSI_Read10() .
| bool MSDH_WriteSectors | ( | uint32_t | 
           
            lba,
           
           | 
         
| uint16_t | 
           
            sectors,
           
           | 
         ||
| const void * | 
           
            data
           
           | 
         ||
| ) | 
Write sectors to device.
- Parameters
 - 
         
[in] lbaSector address (LBA) of first sector to write. [in] sectorsNumber of sectors to write. [out] dataData buffer containing data to be written.  
- Returns
 - Returns true on success, false otherwise.
 
        Definition at line
        
         289
        
        of file
        
         msdh.c
        
        .
       
References MSDSCSI_Write10() .