EZRADIODRV_AutoAckHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Auto_ACK_Plugin
EzRadio auto acknowledge plug-in instance initialization and handler structure.
       Definition at line
       
        63
       
       of file
       
        ezradio_auto_ack_plugin.h
       
       .
      
      
       #include <
       
     
        ezradio_auto_ack_plugin.h
       
       >
      
         Data Fields | 
       |
| EZRADIODRV_AutoAckMode_t | ackMode | 
| 
         Auto ack mode.
          | 
       |
| EZRADIODRV_PacketLengthConfig_t | lenConfig | 
| 
         Pakcet length config for auto ack.
          | 
       |
| uint8_t * | pktBuf | 
| 
         Pointer to the buffer that holds the auto ack packet.
          | 
       |
| uint16_t | pktId | 
| 
         Auto ack packet ID.
          | 
       |
| EZRADIODRV_AutoAckPacketMode_t | pktMode | 
| 
         Packet mode for aut ack.
          | 
       |
| EZRADIODRV_Callback_t | userCallback | 
| 
         User callback.
          | 
       |
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emdrv/ezradiodrv/plugins/inc/
       
ezradio_auto_ack_plugin.h