TFTKit Drivers
Detailed Description
Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode.
         Functions | 
       |
| void | SPI_TFT_Init (void) | 
| 
         Initialize SPI interface to TFT-LCD SSD2119 controller.
          | 
       |
| void | SPI_TFT_WriteRegister (uint8_t reg, uint16_t data) | 
| 
         Write registers to SSD2119 controller.
          | 
       |
| bool | TFT_AddressMappedInit (void) | 
| 
         TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
          | 
       |
| void | TFT_DirectGPIOConfig (void) | 
| 
         GPIO configuration for TFT direct drive.
          | 
       |
| bool | TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit) | 
| 
         TFT initialization funxction. Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
          | 
       |
         Variables | 
       |
| static const USART_InitSync_TypeDef | inittft | 
| static bool | runOnce = true | 
| static bool | runOnce = true | 
Function Documentation
| void SPI_TFT_Init | ( | void | 
           
           
           | 
          ) | 
Initialize SPI interface to TFT-LCD SSD2119 controller.
- Note
 - To enable access, be sure to call the function BSP_PeripheralAccess() before using this interface.
 
        Definition at line
        
         56
        
        of file
        
         tftspi.c
        
        .
       
References CMU_ClockEnable() , cmuClock_GPIO , cmuClock_HFPER , cmuClock_USART1 , GPIO_PinModeSet() , gpioModeInput , gpioModePushPull , USART_InitSync() , and USART_Reset() .
| void SPI_TFT_WriteRegister | ( | uint8_t | 
           
            reg,
           
           | 
         
| uint16_t | 
           
            data
           
           | 
         ||
| ) | 
Write registers to SSD2119 controller.
- Parameters
 - 
         
[in] regRegister to write to [in] data16-bit data to write into register  
- Note
 - It is not possible to read back register value through SSD2119 SPI interface.
 
        Definition at line
        
         91
        
        of file
        
         tftspi.c
        
        .
       
References GPIO_PinOutClear() , GPIO_PinOutSet() , USART_Rx() , and USART_Tx() .
| bool TFT_AddressMappedInit | ( | void | 
           
           
           | 
          ) | 
TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
- Returns
 - true if we should redraw into buffer, false if BC has control over display
 
        Definition at line
        
         48
        
        of file
        
         tftamapped.c
        
        .
       
References BC_ARB_CTRL_EBI , BC_REGISTER , BC_SPI_DEMUX_SLAVE_AUDIO , BC_SPI_DEMUX_SLAVE_DISPLAY , BC_SSD2119_BASE , BC_UIF_AEM_EFM , BSP_Display_EBI , BSP_Display_Mode8080 , BSP_Display_PowerDisable , BSP_Display_PowerEnable , BSP_Display_ResetAssert , BSP_Display_ResetRelease , BSP_DisplayControl() , BSP_RegisterRead() , BSP_RegisterWrite() , runOnce , and SystemCoreClockGet() .
| bool TFT_DirectInit | ( | const EBI_TFTInit_TypeDef * | 
           
            tftInit
           
           | 
          ) | 
TFT initialization funxction. Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
- Parameters
 - 
         
[in] tftInitPointer to EBI TFT initialization structure  
- Returns
 - true if we should redraw into buffer, false if BC has control over display
 
        Definition at line
        
         64
        
        of file
        
         tftdirect.c
        
        .
       
References BC_ARB_CTRL_EBI , BC_REGISTER , BC_UIF_AEM_EFM , BSP_Display_EBI , BSP_Display_ModeGeneric , BSP_Display_PowerDisable , BSP_Display_PowerEnable , BSP_Display_ResetAssert , BSP_Display_ResetRelease , BSP_DisplayControl() , BSP_PeripheralAccess() , BSP_RegisterRead() , BSP_TFT , runOnce , SystemCoreClockGet() , and TFT_DirectGPIOConfig() .
Variable Documentation
           
  | 
          static | 
           em_usart.h:131
          
         
           em_usart.h:186
          
         
           em_usart.h:109
          
         Set default values for tft synchronous mode init structure
        Definition at line
        
         37
        
        of file
        
         tftspi.c
        
        .
       
           
  | 
          static | 
Flag to indicate that we need to initialize once if starting up in
        Definition at line
        
         38
        
        of file
        
         tftdirect.c
        
        .
       
Referenced by TFT_DirectInit() .
           
  | 
          static | 
Flag to indicate that we need to initialize once if starting up in
        Definition at line
        
         39
        
        of file
        
         tftamapped.c
        
        .
       
Referenced by TFT_AddressMappedInit() .