Direct_Transmit_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Direct transmit plugin, see Plugin System Layer for detailed documentation.
.
         Data Structures | 
       |
| struct | EZRADIODRV_DirectTxHandle | 
| 
         EzRadio direct tx plug-in instance initialization and handler structure.
          | 
       |
         Macros | 
       |
| #define | EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT | 
| 
         Configuration data for EzRadio direct tx plug-in.
          | 
       |
         Typedefs | 
       |
| typedef struct EZRADIODRV_DirectTxHandle | EZRADIODRV_DirectTxHandle_t | 
| 
         EzRadio direct tx plug-in instance initialization and handler structure.
          | 
       |
         Functions | 
       |
| Ecode_t | ezradioStartDirectTransmit ( EZRADIODRV_Handle_t radioHandle) | 
| 
         Starts direct transmission with the radio configurations from the radioHandle parameter.
          | 
       |
| Ecode_t | ezradioStopDirectTransmit (void) | 
| 
         Stops direct transmission.
          | 
       |
Macro Definition Documentation
| #define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT | 
Configuration data for EzRadio direct tx plug-in.
        Definition at line
        
         58
        
        of file
        
         ezradio_direct_transmit_plugin.h
        
        .
       
Function Documentation
| Ecode_t ezradioStartDirectTransmit | ( | EZRADIODRV_Handle_t | 
           
            radioHandle
           
           | 
          ) | 
Starts direct transmission with the radio configurations from the radioHandle parameter.
- Parameters
 - 
         
radioHandleHandler of the EzRadio driver instance where channel configuration is set.  
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         41
        
        of file
        
         ezradio_direct_transmit_plugin.c
        
        .
       
References EZRADIODRV_DirectTxHandle::channel , EZRADIODRV_HandleData::directTx , ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED , ezradio_get_int_status() , ezradio_request_device_state() , and ezradio_start_tx() .
| Ecode_t ezradioStopDirectTransmit | ( | void | 
           
           
           | 
          ) | 
Stops direct transmission.
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         72
        
        of file
        
         ezradio_direct_transmit_plugin.c
        
        .
       
References ECODE_EMDRV_EZRADIODRV_OK , and ezradio_change_state() .