HAL_LayerEMDRV > EZRADIODRV
Detailed Description
EzRadio HAL Layer
.
         Functions | 
       |
| void | ezradio_hal_AssertShutdown (void) | 
| void | ezradio_hal_ClearNsel (void) | 
| void | ezradio_hal_DeassertShutdown (void) | 
| void | ezradio_hal_GpioInit ( GPIOINT_IrqCallbackPtr_t ezradioIrqCallback, bool enablePTI) | 
| uint8_t | ezradio_hal_NirqLevel (void) | 
| void | ezradio_hal_SetNsel (void) | 
| void | ezradio_hal_SpiInit (void) | 
| void | ezradio_hal_SpiReadByte (uint8_t *readByte) | 
| void | ezradio_hal_SpiReadData (uint8_t byteCount, uint8_t *pData) | 
| void | ezradio_hal_SpiWriteByte (uint8_t byteToWrite) | 
| void | ezradio_hal_SpiWriteData (uint8_t byteCount, uint8_t *pData) | 
| void | ezradio_hal_SpiWriteReadData (uint8_t byteCount, uint8_t *txData, uint8_t *rxData) | 
Function Documentation
| void ezradio_hal_AssertShutdown | ( | void | 
           
           
           | 
          ) | 
Asserts SDN pin of the EZRadio device.
        Definition at line
        
         122
        
        of file
        
         ezradio_hal.c
        
        .
       
References GPIO_PinOutSet() .
Referenced by ezradio_reset() .
| void ezradio_hal_ClearNsel | ( | void | 
           
           
           | 
          ) | 
Clears nSEL pin of the EZRadio device.
        Definition at line
        
         138
        
        of file
        
         ezradio_hal.c
        
        .
       
References GPIO_PinOutClear() .
Referenced by ezradio_comm_GetResp() , ezradio_comm_ReadData() , ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
| void ezradio_hal_DeassertShutdown | ( | void | 
           
           
           | 
          ) | 
Deasserts SDN pin of the EZRadio device.
        Definition at line
        
         130
        
        of file
        
         ezradio_hal.c
        
        .
       
References GPIO_PinOutClear() .
Referenced by ezradio_reset() .
| void ezradio_hal_GpioInit | ( | GPIOINT_IrqCallbackPtr_t | 
           
            ezradioIrqCallback,
           
           | 
         
| bool | 
           
            enablePTI
           
           | 
         ||
| ) | 
Configures the EZRadio GPIO port and pins
- Parameters
 - 
         
[in] ezradioIrqCallbackEZRadio interrupt callback configuration [in] enablePTIIf true enables the radio PTI bridge in the controller.  
        Definition at line
        
         51
        
        of file
        
         ezradio_hal.c
        
        .
       
References CMU_ClockEnable() , cmuClock_PRS , GPIO_InputSenseSet() , GPIO_IntConfig() , GPIO_PinModeSet() , GPIOINT_CallbackRegister() , gpioModeInput , gpioModeInputPull , gpioModePushPull , and PRS_SourceAsyncSignalSet() .
Referenced by ezradioInit() .
| uint8_t ezradio_hal_NirqLevel | ( | void | 
           
           
           | 
          ) | 
Reads nIRQ pin of the EZRadio device.
- Returns
 - Value of nIRQ pin.
 
        Definition at line
        
         156
        
        of file
        
         ezradio_hal.c
        
        .
       
References GPIO_PinInGet() .
Referenced by ezradio_configuration_init() .
| void ezradio_hal_SetNsel | ( | void | 
           
           
           | 
          ) | 
Sets nSEL pin of the EZRadio device.
        Definition at line
        
         146
        
        of file
        
         ezradio_hal.c
        
        .
       
References GPIO_PinOutSet() .
Referenced by ezradio_comm_GetResp() , ezradio_comm_ReadData() , ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
| void ezradio_hal_SpiInit | ( | void | 
           
           
           | 
          ) | 
Initializes SPI driver for the EZRadio device.
        Definition at line
        
         108
        
        of file
        
         ezradio_hal.c
        
        .
       
References SPIDRV_Init::bitRate , SPIDRV_Init::csControl , SPIDRV_Init() , and spidrvCsControlApplication .
Referenced by ezradioInit() .
| void ezradio_hal_SpiReadByte | ( | uint8_t * | 
           
            readByte
           
           | 
          ) | 
Reads a single byte from the EZRadio SPI port.
- Parameters
 - 
         
readByteRead byte.  
        Definition at line
        
         188
        
        of file
        
         ezradio_hal.c
        
        .
       
References SPIDRV_MReceiveB() .
Referenced by ezradio_comm_GetResp() .
| void ezradio_hal_SpiReadData | ( | uint8_t | 
           
            byteCount,
           
           | 
         
| uint8_t * | 
           
            pData
           
           | 
         ||
| ) | 
Reads byteCount number of bytes from the EZRadio SPI port.
- Parameters
 - 
         
byteCountNumber of bytes to write. pDataPointer to the byte array.  
        Definition at line
        
         210
        
        of file
        
         ezradio_hal.c
        
        .
       
References SPIDRV_MReceiveB() .
Referenced by ezradio_comm_GetResp() , and ezradio_comm_ReadData() .
| void ezradio_hal_SpiWriteByte | ( | uint8_t | 
           
            byteToWrite
           
           | 
          ) | 
Writes a single byte to the EZRadio SPI port.
- Parameters
 - 
         
byteToWriteByte to write.  
        Definition at line
        
         178
        
        of file
        
         ezradio_hal.c
        
        .
       
References SPIDRV_MTransmitB() .
Referenced by ezradio_comm_GetResp() , ezradio_comm_ReadData() , and ezradio_comm_WriteData() .
| void ezradio_hal_SpiWriteData | ( | uint8_t | 
           
            byteCount,
           
           | 
         
| uint8_t * | 
           
            pData
           
           | 
         ||
| ) | 
Writes byteCount number of bytes to the EZRadio SPI port.
- Parameters
 - 
         
byteCountNumber of bytes to write. pDataPointer to the byte array.  
        Definition at line
        
         199
        
        of file
        
         ezradio_hal.c
        
        .
       
References SPIDRV_MTransmitB() .
Referenced by ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
| void ezradio_hal_SpiWriteReadData | ( | uint8_t | 
           
            byteCount,
           
           | 
         
| uint8_t * | 
           
            txData,
           
           | 
         ||
| uint8_t * | 
           
            rxData
           
           | 
         ||
| ) | 
Reads byteCount number of bytes from the EZRadio SPI port.
- Parameters
 - 
         
byteCountNumber of bytes to write. pDataPointer to the byte array.  
        Definition at line
        
         221
        
        of file
        
         ezradio_hal.c
        
        .
       
References SPIDRV_MTransferB() .
Referenced by ezradio_comm_GetResp() , and ezradio_comm_ReadData() .