MSDSCSI_StartStopUnit_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
SCSI Start Stop Unit Command Descriptor Block (CDB) typedef.
       Definition at line
       
        279
       
       of file
       
        msdscsi.h
       
       .
      
      
       #include <
       
     
        msdscsi.h
       
       >
      
         Data Fields | 
       |
| struct { | |
| uint8_t Immed : 1 | |
| uint8_t Reserved1 : 7 | |
| }; | |
| struct { | |
| uint8_t PowerConditionModifier : 4 | |
| uint8_t Reserved3 : 4 | |
| }; | |
| struct { | |
| uint8_t LoEj : 1 | |
| uint8_t No_Flush : 1 | |
| uint8_t PowerCondition : 4 | |
| uint8_t Reserved4 : 1 | |
| uint8_t Start : 1 | |
| }; | |
| uint8_t | Control | 
| uint8_t | OpCode | 
| uint8_t | Reserved2 | 
Field Documentation
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Control | 
Control byte.
        Definition at line
        
         297
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Immed | 
Immediate bit.
        Definition at line
        
         282
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::LoEj | 
Load Eject.
        Definition at line
        
         292
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::No_Flush | 
Dont flush cached data to the medium.
        Definition at line
        
         293
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::OpCode | 
Command opcode.
        Definition at line
        
         280
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::PowerCondition | 
Power Condition field.
        Definition at line
        
         295
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::PowerConditionModifier | 
Additional power condition info.
        Definition at line
        
         287
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved1 | 
Reserved, expect 0.
        Definition at line
        
         283
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved2 | 
Reserved, expect 0.
        Definition at line
        
         285
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved3 | 
Reserved, expect 0.
        Definition at line
        
         288
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved4 | 
Reserved, expect 0.
        Definition at line
        
         294
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_StartStopUnit_TypeDef::Start | 
Start bit.
        Definition at line
        
         291
        
        of file
        
         msdscsi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/
       
msdscsi.h