TIMER_InitDTI_TypeDef Struct ReferenceEMLIB > TIMER
TIMER Dead Time Insertion (DTI) initialization structure.
       Definition at line
       
        451
       
       of file
       
        em_timer.h
       
       .
      
      
       #include <
       
     
        em_timer.h
       
       >
      
         Data Fields | 
       |
| bool | activeLowOut | 
| bool | autoRestart | 
| bool | enable | 
| bool | enableFaultSourceCoreLockup | 
| bool | enableFaultSourceDebugger | 
| bool | enableFaultSourcePrsSel0 | 
| bool | enableFaultSourcePrsSel1 | 
| bool | enablePrsSource | 
| unsigned int | fallTime | 
| TIMER_DtiFaultAction_TypeDef | faultAction | 
| TIMER_PRSSEL_TypeDef | faultSourcePrsSel0 | 
| TIMER_PRSSEL_TypeDef | faultSourcePrsSel1 | 
| bool | invertComplementaryOut | 
| uint32_t | outputsEnableMask | 
| TIMER_Prescale_TypeDef | prescale | 
| TIMER_PRSSEL_TypeDef | prsSel | 
| unsigned int | riseTime | 
Field Documentation
| bool TIMER_InitDTI_TypeDef::activeLowOut | 
| bool TIMER_InitDTI_TypeDef::autoRestart | 
Enable Automatic Start-up functionality (when debugger exits).
        Definition at line
        
         462
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enable | 
Enable DTI or leave it disabled until TIMER_EnableDTI() is called.
        Definition at line
        
         453
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourceCoreLockup | 
Enable core lockup as a fault source.
        Definition at line
        
         487
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourceDebugger | 
Enable debugger as a fault source.
        Definition at line
        
         490
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel0 | 
        Enable PRS fault source 0 (
        
         faultSourcePrsSel0
        
        ).
       
        Definition at line
        
         493
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel1 | 
        Enable PRS fault source 1 (
        
         faultSourcePrsSel1
        
        ).
       
        Definition at line
        
         499
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::enablePrsSource | 
Enable/disable PRS as DTI input.
        Definition at line
        
         465
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| unsigned int TIMER_InitDTI_TypeDef::fallTime | 
| TIMER_DtiFaultAction_TypeDef TIMER_InitDTI_TypeDef::faultAction | 
| TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel0 | 
Select which PRS signal to be PRS fault source 0.
        Definition at line
        
         496
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel1 | 
Select which PRS signal to be PRS fault source 1.
        Definition at line
        
         502
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| bool TIMER_InitDTI_TypeDef::invertComplementaryOut | 
DTI Complementary Output Invert.
        Definition at line
        
         459
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| uint32_t TIMER_InitDTI_TypeDef::outputsEnableMask | 
DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2. This value should consist of one or more TIMER_DTOGEN_DTOGnnnEN flags (defined in <part_name>_timer.h) OR'ed together.
        Definition at line
        
         484
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| TIMER_Prescale_TypeDef TIMER_InitDTI_TypeDef::prescale | 
DTI prescaling factor, if HFPER / HFPERB clock used.
        Definition at line
        
         472
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::prsSel | 
        Select which PRS channel as DTI input. Only valid if
        
         enablePrsSource
        
        is enabled.
       
        Definition at line
        
         469
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitDTI() .
| unsigned int TIMER_InitDTI_TypeDef::riseTime | 
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       
em_timer.h