SL_EFPDRVKit Drivers
Detailed Description
EFP (Energy Friendly PMIC) driver.
- Note
- This version of the sl_efpdrv is Alpha level only. Silicon Labs will NOT support any production deployments with this Alpha version. Production deployments will only be supported with the GA version of this feature. This version is intended for lab and evaluation purpose only.
Documentation placeholder.
Data Structures |
|
struct | sl_efpdrv_init_data |
EFP driver initialization structure.
|
|
Macros |
|
#define | _EFP01_ADC_CC_CTRL_ADC_IIR_TAU_MASK 0x38 |
#define | _EFP01_ADC_CC_CTRL_ADC_IIR_TAU_SHIFT 3 |
#define | _EFP01_ADC_CC_CTRL_ADC_INTERVAL_MASK 0x07 |
#define | _EFP01_ADC_CC_CTRL_ADC_INTERVAL_SHIFT 0 |
#define | _EFP01_ADC_CC_CTRL_ADDRESS 0x5C |
#define | _EFP01_ADC_CC_CTRL_RESETVALUE 0x00 |
#define | _EFP01_ADC_LIMITS_ADC_T_LIM_MASK 0x07 |
#define | _EFP01_ADC_LIMITS_ADC_T_LIM_SHIFT 0 |
#define | _EFP01_ADC_LIMITS_ADC_V_LIM_MASK 0xF8 |
#define | _EFP01_ADC_LIMITS_ADC_V_LIM_SHIFT 3 |
#define | _EFP01_ADC_LIMITS_ADDRESS 0x5D |
#define | _EFP01_ADC_LIMITS_RESETVALUE 0x00 |
#define | _EFP01_BB_CTRL3_ADDRESS 0x50 |
#define | _EFP01_BB_CTRL3_BB_MODE_AUTONOMOUS 0x01 |
#define | _EFP01_BB_CTRL3_BB_MODE_DISABLED 0x00 |
#define | _EFP01_BB_CTRL3_BB_MODE_FORCEBOOST 0x04 |
#define | _EFP01_BB_CTRL3_BB_MODE_FORCEBUCK 0x02 |
#define | _EFP01_BB_CTRL3_BB_MODE_FORCENTM 0x03 |
#define | _EFP01_BB_CTRL3_BB_MODE_MASK 0x07 |
#define | _EFP01_BB_CTRL3_BB_MODE_SHIFT 0 |
#define | _EFP01_BB_CTRL3_BB_MODE_WIREDBOOST 0x07 |
#define | _EFP01_BB_CTRL3_BB_MODE_WIREDBUCK 0x06 |
#define | _EFP01_BB_CTRL3_BB_MODE_WIREDBUCKLDO 0x05 |
#define | _EFP01_BB_CTRL3_NTM_DUR_107PCT 0x02 |
#define | _EFP01_BB_CTRL3_NTM_DUR_130PCT 0x03 |
#define | _EFP01_BB_CTRL3_NTM_DUR_60PCT 0x00 |
#define | _EFP01_BB_CTRL3_NTM_DUR_83PCT 0x01 |
#define | _EFP01_BB_CTRL3_NTM_DUR_MASK 0x18 |
#define | _EFP01_BB_CTRL3_NTM_DUR_SHIFT 3 |
#define | _EFP01_BB_CTRL3_NTM_LDO_THRSH_MASK 0xE0 |
#define | _EFP01_BB_CTRL3_NTM_LDO_THRSH_SHIFT 5 |
#define | _EFP01_BB_CTRL3_RESETVALUE 0x00 |
#define | _EFP01_BB_CTRL5_ADDRESS 0x51 |
#define | _EFP01_BB_CTRL5_BB_DRVR_SPEED_MASK 0xC0 |
#define | _EFP01_BB_CTRL5_BB_DRVR_SPEED_SHIFT 6 |
#define | _EFP01_BB_CTRL5_BB_IPK_BOOST_MASK 0x3F |
#define | _EFP01_BB_CTRL5_BB_IPK_BOOST_SHIFT 0 |
#define | _EFP01_BB_CTRL5_RESETVALUE 0x00 |
#define | _EFP01_BB_CTRL6_ADDRESS 0x52 |
#define | _EFP01_BB_CTRL6_BB_IPK_NOADJ_MASK 0x80 |
#define | _EFP01_BB_CTRL6_BB_IPK_NOADJ_SHIFT 7 |
#define | _EFP01_BB_CTRL6_BB_IRI_CON_MASK 0x3C |
#define | _EFP01_BB_CTRL6_BB_IRI_CON_SHIFT 2 |
#define | _EFP01_BB_CTRL6_BB_TOFF_MAX_0P9US 0x01 |
#define | _EFP01_BB_CTRL6_BB_TOFF_MAX_1P5US 0x02 |
#define | _EFP01_BB_CTRL6_BB_TOFF_MAX_2P1US 0x03 |
#define | _EFP01_BB_CTRL6_BB_TOFF_MAX_MASK 0x03 |
#define | _EFP01_BB_CTRL6_BB_TOFF_MAX_NOLIMIT 0x00 |
#define | _EFP01_BB_CTRL6_BB_TOFF_MAX_SHIFT 0 |
#define | _EFP01_BB_CTRL6_RESETVALUE 0x00 |
#define | _EFP01_BB_CTRL6_SW_FAST_MASK 0x40 |
#define | _EFP01_BB_CTRL6_SW_FAST_SHIFT 6 |
#define | _EFP01_BB_IPK_ADDRESS 0x4F |
#define | _EFP01_BB_IPK_BB_IPK_EM2_MASK 0xE0 |
#define | _EFP01_BB_IPK_BB_IPK_EM2_SHIFT 5 |
#define | _EFP01_BB_IPK_BB_IPK_MASK 0x1F |
#define | _EFP01_BB_IPK_BB_IPK_SHIFT 0 |
#define | _EFP01_BB_IPK_RESETVALUE 0x00 |
#define | _EFP01_BBK_CTRL_ADDRESS 0x5A |
#define | _EFP01_BBK_CTRL_BBK_TON_MAX_TRANS_MASK 0x20 |
#define | _EFP01_BBK_CTRL_BBK_TON_MAX_TRANS_SHIFT 5 |
#define | _EFP01_BBK_CTRL_BBK_ZC_FIX_MASK 0x10 |
#define | _EFP01_BBK_CTRL_BBK_ZC_FIX_SHIFT 4 |
#define | _EFP01_BBK_CTRL_BBK_ZC_VAL_MASK 0x0F |
#define | _EFP01_BBK_CTRL_BBK_ZC_VAL_SHIFT 0 |
#define | _EFP01_BBK_CTRL_RESETVALUE 0x00 |
#define | _EFP01_BIAS_SW_ADDRESS 0x4E |
#define | _EFP01_BIAS_SW_BIAS0_100NA 0x01 |
#define | _EFP01_BIAS_SW_BIAS0_114NA 0x02 |
#define | _EFP01_BIAS_SW_BIAS0_147NA 0x03 |
#define | _EFP01_BIAS_SW_BIAS0_325NA 0x04 |
#define | _EFP01_BIAS_SW_BIAS0_386NA 0x05 |
#define | _EFP01_BIAS_SW_BIAS0_453NA 0x06 |
#define | _EFP01_BIAS_SW_BIAS0_600NA 0x07 |
#define | _EFP01_BIAS_SW_BIAS0_87NA 0x00 |
#define | _EFP01_BIAS_SW_BIAS0_MASK 0x07 |
#define | _EFP01_BIAS_SW_BIAS0_SHIFT 0 |
#define | _EFP01_BIAS_SW_BIAS2_100NA 0x01 |
#define | _EFP01_BIAS_SW_BIAS2_114NA 0x02 |
#define | _EFP01_BIAS_SW_BIAS2_147NA 0x03 |
#define | _EFP01_BIAS_SW_BIAS2_325NA 0x04 |
#define | _EFP01_BIAS_SW_BIAS2_386NA 0x05 |
#define | _EFP01_BIAS_SW_BIAS2_453NA 0x06 |
#define | _EFP01_BIAS_SW_BIAS2_600NA 0x07 |
#define | _EFP01_BIAS_SW_BIAS2_87NA 0x00 |
#define | _EFP01_BIAS_SW_BIAS2_MASK 0x38 |
#define | _EFP01_BIAS_SW_BIAS2_SHIFT 3 |
#define | _EFP01_BIAS_SW_RESETVALUE 0x00 |
#define | _EFP01_BIAS_SW_VOA_SW_CON_MASK 0xC0 |
#define | _EFP01_BIAS_SW_VOA_SW_CON_OFF 0x00 |
#define | _EFP01_BIAS_SW_VOA_SW_CON_ON 0x01 |
#define | _EFP01_BIAS_SW_VOA_SW_CON_ONINEM0 0x02 |
#define | _EFP01_BIAS_SW_VOA_SW_CON_ONINEM02 0x03 |
#define | _EFP01_BIAS_SW_VOA_SW_CON_SHIFT 6 |
#define | _EFP01_BK_CTRL0_ADDRESS 0x56 |
#define | _EFP01_BK_CTRL0_BK_DIS_OV_PROT_MASK 0x02 |
#define | _EFP01_BK_CTRL0_BK_DIS_OV_PROT_SHIFT 1 |
#define | _EFP01_BK_CTRL0_CLAMPB_MASK 0x01 |
#define | _EFP01_BK_CTRL0_CLAMPB_SHIFT 0 |
#define | _EFP01_BK_CTRL0_RESETVALUE 0x00 |
#define | _EFP01_BK_CTRL1_ADDRESS 0x57 |
#define | _EFP01_BK_CTRL1_BK_DRVR_SPEED_MASK 0x06 |
#define | _EFP01_BK_CTRL1_BK_DRVR_SPEED_SHIFT 1 |
#define | _EFP01_BK_CTRL1_BK_MODE_BUCKLDO 0x03 |
#define | _EFP01_BK_CTRL1_BK_MODE_BUCKONLY 0x01 |
#define | _EFP01_BK_CTRL1_BK_MODE_DISABLED 0x00 |
#define | _EFP01_BK_CTRL1_BK_MODE_LDOONLY 0x02 |
#define | _EFP01_BK_CTRL1_BK_MODE_MASK 0x18 |
#define | _EFP01_BK_CTRL1_BK_MODE_SHIFT 3 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_1190NS 0x04 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_1470NS 0x05 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_1750NS 0x06 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_2030NS 0x07 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_350NS 0x01 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_630NS 0x02 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_910NS 0x03 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_MASK 0xE0 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_NOLIMIT 0x00 |
#define | _EFP01_BK_CTRL1_BK_TON_MAX_SHIFT 5 |
#define | _EFP01_BK_CTRL1_RESETVALUE 0x00 |
#define | _EFP01_BK_CTRL2_ADDRESS 0x59 |
#define | _EFP01_BK_CTRL2_BK_IRI_CON_MASK 0x0F |
#define | _EFP01_BK_CTRL2_BK_IRI_CON_SHIFT 0 |
#define | _EFP01_BK_CTRL2_BK_LDO_THRESH_MASK 0x70 |
#define | _EFP01_BK_CTRL2_BK_LDO_THRESH_SHIFT 4 |
#define | _EFP01_BK_CTRL2_BK_RES_TON_ONLY_MASK 0x80 |
#define | _EFP01_BK_CTRL2_BK_RES_TON_ONLY_SHIFT 7 |
#define | _EFP01_BK_CTRL2_RESETVALUE 0x00 |
#define | _EFP01_BK_IPK_ADDRESS 0x58 |
#define | _EFP01_BK_IPK_BK_IPK_EM2_MASK 0xE0 |
#define | _EFP01_BK_IPK_BK_IPK_EM2_SHIFT 5 |
#define | _EFP01_BK_IPK_BK_IPK_MASK 0x1F |
#define | _EFP01_BK_IPK_BK_IPK_SHIFT 0 |
#define | _EFP01_BK_IPK_RESETVALUE 0x00 |
#define | _EFP01_CC_CAL_ADDRESS 0x0A |
#define | _EFP01_CC_CAL_CC_CAL_NREQ_MASK 0xE0 |
#define | _EFP01_CC_CAL_CC_CAL_NREQ_SHIFT 5 |
#define | _EFP01_CC_CAL_CCL_LVL_11200UA 0x06 |
#define | _EFP01_CC_CAL_CCL_LVL_14000UA 0x07 |
#define | _EFP01_CC_CAL_CCL_LVL_440UA 0x00 |
#define | _EFP01_CC_CAL_CCL_LVL_550UA 0x01 |
#define | _EFP01_CC_CAL_CCL_LVL_700UA 0x02 |
#define | _EFP01_CC_CAL_CCL_LVL_7060UA 0x04 |
#define | _EFP01_CC_CAL_CCL_LVL_875UA 0x03 |
#define | _EFP01_CC_CAL_CCL_LVL_8830UA 0x05 |
#define | _EFP01_CC_CAL_CCL_LVL_MASK 0x07 |
#define | _EFP01_CC_CAL_CCL_LVL_SHIFT 0 |
#define | _EFP01_CC_CAL_CCL_SEL_MASK 0x18 |
#define | _EFP01_CC_CAL_CCL_SEL_NONE 0x00 |
#define | _EFP01_CC_CAL_CCL_SEL_SHIFT 3 |
#define | _EFP01_CC_CAL_CCL_SEL_VOA 0x01 |
#define | _EFP01_CC_CAL_CCL_SEL_VOB 0x02 |
#define | _EFP01_CC_CAL_CCL_SEL_VOC 0x03 |
#define | _EFP01_CC_CAL_RESETVALUE 0x00 |
#define | _EFP01_CC_CTRL_ADDRESS 0x41 |
#define | _EFP01_CC_CTRL_CC_ENA_MASK 0x10 |
#define | _EFP01_CC_CTRL_CC_ENA_SHIFT 4 |
#define | _EFP01_CC_CTRL_CC_PRESCL_MASK 0x0C |
#define | _EFP01_CC_CTRL_CC_PRESCL_SHIFT 2 |
#define | _EFP01_CC_CTRL_CC_THRSH_50PCT 0x00 |
#define | _EFP01_CC_CTRL_CC_THRSH_62PCT 0x01 |
#define | _EFP01_CC_CTRL_CC_THRSH_75PCT 0x02 |
#define | _EFP01_CC_CTRL_CC_THRSH_87PCT 0x03 |
#define | _EFP01_CC_CTRL_CC_THRSH_MASK 0x60 |
#define | _EFP01_CC_CTRL_CC_THRSH_SHIFT 5 |
#define | _EFP01_CC_CTRL_RESETVALUE 0x00 |
#define | _EFP01_CC_MODE_ADDRESS 0x12 |
#define | _EFP01_CC_MODE_CCA_MODE_AUTO 0x01 |
#define | _EFP01_CC_MODE_CCA_MODE_BOOST 0x02 |
#define | _EFP01_CC_MODE_CCA_MODE_BUCK 0x00 |
#define | _EFP01_CC_MODE_CCA_MODE_LDO 0x03 |
#define | _EFP01_CC_MODE_CCA_MODE_MASK 0x03 |
#define | _EFP01_CC_MODE_CCA_MODE_SHIFT 0 |
#define | _EFP01_CC_MODE_CCB_MODE_BUCK 0x00 |
#define | _EFP01_CC_MODE_CCB_MODE_LDOB 0x01 |
#define | _EFP01_CC_MODE_CCB_MODE_MASK 0x04 |
#define | _EFP01_CC_MODE_CCB_MODE_SHIFT 2 |
#define | _EFP01_CC_MODE_RESETVALUE 0x00 |
#define | _EFP01_CC_MODE_SC_MODE_MASK 0x08 |
#define | _EFP01_CC_MODE_SC_MODE_SHIFT 3 |
#define | _EFP01_CCA_LSBY_ADDRESS 0x14 |
#define | _EFP01_CCA_LSBY_CCA_LSBY_MASK 0xFF |
#define | _EFP01_CCA_LSBY_CCA_LSBY_SHIFT 0 |
#define | _EFP01_CCA_LSBY_RESETVALUE 0x00 |
#define | _EFP01_CCA_MSBY_ADDRESS 0x13 |
#define | _EFP01_CCA_MSBY_CCA_MSBY_MASK 0xFF |
#define | _EFP01_CCA_MSBY_CCA_MSBY_SHIFT 0 |
#define | _EFP01_CCA_MSBY_RESETVALUE 0x00 |
#define | _EFP01_CCB0_LSBY_ADDRESS 0x16 |
#define | _EFP01_CCB0_LSBY_CCB0_LSBY_MASK 0xFF |
#define | _EFP01_CCB0_LSBY_CCB0_LSBY_SHIFT 0 |
#define | _EFP01_CCB0_LSBY_RESETVALUE 0x00 |
#define | _EFP01_CCB0_MSBY_ADDRESS 0x15 |
#define | _EFP01_CCB0_MSBY_CCB0_MSBY_MASK 0xFF |
#define | _EFP01_CCB0_MSBY_CCB0_MSBY_SHIFT 0 |
#define | _EFP01_CCB0_MSBY_RESETVALUE 0x00 |
#define | _EFP01_CCB2_LSBY_ADDRESS 0x18 |
#define | _EFP01_CCB2_LSBY_CCB2_LSBY_MASK 0xFF |
#define | _EFP01_CCB2_LSBY_CCB2_LSBY_SHIFT 0 |
#define | _EFP01_CCB2_LSBY_RESETVALUE 0x00 |
#define | _EFP01_CCB2_MSBY_ADDRESS 0x17 |
#define | _EFP01_CCB2_MSBY_CCB2_MSBY_MASK 0xFF |
#define | _EFP01_CCB2_MSBY_CCB2_MSBY_SHIFT 0 |
#define | _EFP01_CCB2_MSBY_RESETVALUE 0x00 |
#define | _EFP01_CCC_LSBY_ADDRESS 0x1A |
#define | _EFP01_CCC_LSBY_CCC_LSBY_MASK 0xFF |
#define | _EFP01_CCC_LSBY_CCC_LSBY_SHIFT 0 |
#define | _EFP01_CCC_LSBY_RESETVALUE 0x00 |
#define | _EFP01_CCC_MSBY_ADDRESS 0x19 |
#define | _EFP01_CCC_MSBY_CCC_MSBY_MASK 0xFF |
#define | _EFP01_CCC_MSBY_CCC_MSBY_SHIFT 0 |
#define | _EFP01_CCC_MSBY_RESETVALUE 0x00 |
#define | _EFP01_CMD_ADC_CLR_MASK 0x40 |
#define | _EFP01_CMD_ADC_CLR_SHIFT 6 |
#define | _EFP01_CMD_ADC_START_MASK 0x80 |
#define | _EFP01_CMD_ADC_START_SHIFT 7 |
#define | _EFP01_CMD_ADDRESS 0x10 |
#define | _EFP01_CMD_CC_CAL_STRT_MASK 0x10 |
#define | _EFP01_CMD_CC_CAL_STRT_SHIFT 4 |
#define | _EFP01_CMD_CC_CLR_MASK 0x20 |
#define | _EFP01_CMD_CC_CLR_SHIFT 5 |
#define | _EFP01_CMD_OTP_REREAD_MASK 0x04 |
#define | _EFP01_CMD_OTP_REREAD_SHIFT 2 |
#define | _EFP01_CMD_REFRESH_FST_TRIG_MASK 0x08 |
#define | _EFP01_CMD_REFRESH_FST_TRIG_SHIFT 3 |
#define | _EFP01_CMD_RESET_MASK 0x01 |
#define | _EFP01_CMD_RESET_SHIFT 0 |
#define | _EFP01_CMD_RESETVALUE 0x00 |
#define | _EFP01_DEVREV_ID_ADDRESS 0x05 |
#define | _EFP01_DEVREV_ID_DEV_ID_MASK 0x1F |
#define | _EFP01_DEVREV_ID_DEV_ID_SHIFT 0 |
#define | _EFP01_DEVREV_ID_RESETVALUE 0x00 |
#define | _EFP01_DEVREV_ID_REV_ID_MASK 0xE0 |
#define | _EFP01_DEVREV_ID_REV_ID_SHIFT 5 |
#define | _EFP01_EM_CRSREG_CTRL_ADDRESS 0x43 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_BYP_MASK 0x10 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_BYP_SHIFT 4 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_EN_A_MASK 0x20 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_EN_A_SHIFT 5 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_EN_B_MASK 0x40 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_EN_B_SHIFT 6 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_EN_C_MASK 0x80 |
#define | _EFP01_EM_CRSREG_CTRL_CRSREG_EN_C_SHIFT 7 |
#define | _EFP01_EM_CRSREG_CTRL_EM_0ONI2CST_MASK 0x08 |
#define | _EFP01_EM_CRSREG_CTRL_EM_0ONI2CST_SHIFT 3 |
#define | _EFP01_EM_CRSREG_CTRL_EM_DIRECTEN_MASK 0x01 |
#define | _EFP01_EM_CRSREG_CTRL_EM_DIRECTEN_SHIFT 0 |
#define | _EFP01_EM_CRSREG_CTRL_EM_STSEL_EM0 0x00 |
#define | _EFP01_EM_CRSREG_CTRL_EM_STSEL_EM2 0x02 |
#define | _EFP01_EM_CRSREG_CTRL_EM_STSEL_EM4 0x03 |
#define | _EFP01_EM_CRSREG_CTRL_EM_STSEL_MASK 0x06 |
#define | _EFP01_EM_CRSREG_CTRL_EM_STSEL_RESERVED 0x01 |
#define | _EFP01_EM_CRSREG_CTRL_EM_STSEL_SHIFT 1 |
#define | _EFP01_EM_CRSREG_CTRL_RESETVALUE 0x00 |
#define | _EFP01_I2C_CTRL_ADDRESS 0x40 |
#define | _EFP01_I2C_CTRL_I2C_DEVADDR_MASK 0x70 |
#define | _EFP01_I2C_CTRL_I2C_DEVADDR_SHIFT 4 |
#define | _EFP01_I2C_CTRL_I2C_PU_MASK 0x01 |
#define | _EFP01_I2C_CTRL_I2C_PU_SHIFT 0 |
#define | _EFP01_I2C_CTRL_IO_DIS_DEGLITCH_MASK 0x04 |
#define | _EFP01_I2C_CTRL_IO_DIS_DEGLITCH_SHIFT 2 |
#define | _EFP01_I2C_CTRL_IO_SLOW_MODE_MASK 0x08 |
#define | _EFP01_I2C_CTRL_IO_SLOW_MODE_SHIFT 3 |
#define | _EFP01_I2C_CTRL_RESETVALUE 0x00 |
#define | _EFP01_LDOB_CTRL_ADDRESS 0x53 |
#define | _EFP01_LDOB_CTRL_LDO_NO_AUTO_BYP_MASK 0x80 |
#define | _EFP01_LDOB_CTRL_LDO_NO_AUTO_BYP_SHIFT 7 |
#define | _EFP01_LDOB_CTRL_LDOB_BYP_MASK 0x40 |
#define | _EFP01_LDOB_CTRL_LDOB_BYP_SHIFT 6 |
#define | _EFP01_LDOB_CTRL_LDOB_IGAIN_MASK 0x0F |
#define | _EFP01_LDOB_CTRL_LDOB_IGAIN_SHIFT 0 |
#define | _EFP01_LDOB_CTRL_LDOB_VMIN_MASK 0x30 |
#define | _EFP01_LDOB_CTRL_LDOB_VMIN_SHIFT 4 |
#define | _EFP01_LDOB_CTRL_RESETVALUE 0x00 |
#define | _EFP01_LDOC_BB_CTRL_ADDRESS 0x55 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_1190NS 0x04 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_1470NS 0x05 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_1750NS 0x06 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_2030NS 0x07 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_350NS 0x01 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_630NS 0x02 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_910NS 0x03 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_MASK 0x70 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_NOLIMIT 0x00 |
#define | _EFP01_LDOC_BB_CTRL_BB_TON_MAX_SHIFT 4 |
#define | _EFP01_LDOC_BB_CTRL_RESETVALUE 0x00 |
#define | _EFP01_LDOC_BB_CTRL_SEQ_BB_FIRST_MASK 0x80 |
#define | _EFP01_LDOC_BB_CTRL_SEQ_BB_FIRST_SHIFT 7 |
#define | _EFP01_LDOC_BB_CTRL_VOC_IRI_CON_MASK 0x0F |
#define | _EFP01_LDOC_BB_CTRL_VOC_IRI_CON_SHIFT 0 |
#define | _EFP01_LDOC_CTRL_ADDRESS 0x54 |
#define | _EFP01_LDOC_CTRL_LDOC_BYP_MASK 0x40 |
#define | _EFP01_LDOC_CTRL_LDOC_BYP_SHIFT 6 |
#define | _EFP01_LDOC_CTRL_LDOC_ENA_SA_MASK 0x80 |
#define | _EFP01_LDOC_CTRL_LDOC_ENA_SA_SHIFT 7 |
#define | _EFP01_LDOC_CTRL_LDOC_IGAIN_MASK 0x0F |
#define | _EFP01_LDOC_CTRL_LDOC_IGAIN_SHIFT 0 |
#define | _EFP01_LDOC_CTRL_LDOC_VMIN_MASK 0x30 |
#define | _EFP01_LDOC_CTRL_LDOC_VMIN_SHIFT 4 |
#define | _EFP01_LDOC_CTRL_RESETVALUE 0x00 |
#define | _EFP01_OTP_ADDR_ADDRESS 0x0B |
#define | _EFP01_OTP_ADDR_OTP_ADDR_MASK 0x7F |
#define | _EFP01_OTP_ADDR_OTP_ADDR_SHIFT 0 |
#define | _EFP01_OTP_ADDR_RESETVALUE 0x00 |
#define | _EFP01_OTP_RDATA_ADDRESS 0x0C |
#define | _EFP01_OTP_RDATA_OTP_RDATA_MASK 0xFF |
#define | _EFP01_OTP_RDATA_OTP_RDATA_SHIFT 0 |
#define | _EFP01_OTP_RDATA_RESETVALUE 0x00 |
#define | _EFP01_OTP_STATCTRL_ADDRESS 0x0E |
#define | _EFP01_OTP_STATCTRL_ARR_PRGFAIL_MASK 0x40 |
#define | _EFP01_OTP_STATCTRL_ARR_PRGFAIL_SHIFT 6 |
#define | _EFP01_OTP_STATCTRL_CMD_READOTP_MASK 0x04 |
#define | _EFP01_OTP_STATCTRL_CMD_READOTP_SHIFT 2 |
#define | _EFP01_OTP_STATCTRL_MRG_READEN_MASK 0x01 |
#define | _EFP01_OTP_STATCTRL_MRG_READEN_SHIFT 0 |
#define | _EFP01_OTP_STATCTRL_OTP_BUSY_MASK 0x08 |
#define | _EFP01_OTP_STATCTRL_OTP_BUSY_SHIFT 3 |
#define | _EFP01_OTP_STATCTRL_PROGVER_EN_MASK 0x10 |
#define | _EFP01_OTP_STATCTRL_PROGVER_EN_SHIFT 4 |
#define | _EFP01_OTP_STATCTRL_PROGVER_STAT_MASK 0x20 |
#define | _EFP01_OTP_STATCTRL_PROGVER_STAT_SHIFT 5 |
#define | _EFP01_OTP_STATCTRL_RESETVALUE 0x00 |
#define | _EFP01_STATUS_G_ADDRESS 0x00 |
#define | _EFP01_STATUS_G_CC_FULL_MASK 0x20 |
#define | _EFP01_STATUS_G_CC_FULL_SHIFT 5 |
#define | _EFP01_STATUS_G_CCC_ISDONE_MASK 0x40 |
#define | _EFP01_STATUS_G_CCC_ISDONE_SHIFT 6 |
#define | _EFP01_STATUS_G_I2C_FAULT_MASK 0x04 |
#define | _EFP01_STATUS_G_I2C_FAULT_SHIFT 2 |
#define | _EFP01_STATUS_G_OTP_CRC_FAULT_MASK 0x02 |
#define | _EFP01_STATUS_G_OTP_CRC_FAULT_SHIFT 1 |
#define | _EFP01_STATUS_G_OTP_READ_MASK 0x01 |
#define | _EFP01_STATUS_G_OTP_READ_SHIFT 0 |
#define | _EFP01_STATUS_G_RESETVALUE 0x00 |
#define | _EFP01_STATUS_G_TEMP_FAULT_MASK 0x08 |
#define | _EFP01_STATUS_G_TEMP_FAULT_SHIFT 3 |
#define | _EFP01_STATUS_G_VDD_LOW_MASK 0x80 |
#define | _EFP01_STATUS_G_VDD_LOW_SHIFT 7 |
#define | _EFP01_STATUS_G_VOLT_FAULT_MASK 0x10 |
#define | _EFP01_STATUS_G_VOLT_FAULT_SHIFT 4 |
#define | _EFP01_STATUS_GM_ADDRESS 0x02 |
#define | _EFP01_STATUS_GM_CC_FULL_UNMASK_MASK 0x20 |
#define | _EFP01_STATUS_GM_CC_FULL_UNMASK_SHIFT 5 |
#define | _EFP01_STATUS_GM_CCC_ISDONE_UNMASK_MASK 0x40 |
#define | _EFP01_STATUS_GM_CCC_ISDONE_UNMASK_SHIFT 6 |
#define | _EFP01_STATUS_GM_I2C_FAULT_UNMASK_MASK 0x04 |
#define | _EFP01_STATUS_GM_I2C_FAULT_UNMASK_SHIFT 2 |
#define | _EFP01_STATUS_GM_OTP_CRC_FAULT_UNMASK_MASK 0x02 |
#define | _EFP01_STATUS_GM_OTP_CRC_FAULT_UNMASK_SHIFT 1 |
#define | _EFP01_STATUS_GM_OTP_READ_UNMASK_MASK 0x01 |
#define | _EFP01_STATUS_GM_OTP_READ_UNMASK_SHIFT 0 |
#define | _EFP01_STATUS_GM_RESETVALUE 0x00 |
#define | _EFP01_STATUS_GM_TEMP_FAULT_UNMASK_MASK 0x08 |
#define | _EFP01_STATUS_GM_TEMP_FAULT_UNMASK_SHIFT 3 |
#define | _EFP01_STATUS_GM_VDD_LOW_UNMASK_MASK 0x80 |
#define | _EFP01_STATUS_GM_VDD_LOW_UNMASK_SHIFT 7 |
#define | _EFP01_STATUS_GM_VOLT_FAULT_UNMASK_MASK 0x10 |
#define | _EFP01_STATUS_GM_VOLT_FAULT_UNMASK_SHIFT 4 |
#define | _EFP01_STATUS_LIVE_ADDRESS 0x04 |
#define | _EFP01_STATUS_LIVE_CCC_LIVE_MASK 0x20 |
#define | _EFP01_STATUS_LIVE_CCC_LIVE_SHIFT 5 |
#define | _EFP01_STATUS_LIVE_RESETVALUE 0x00 |
#define | _EFP01_STATUS_LIVE_TEMP_HI_LIVE_MASK 0x10 |
#define | _EFP01_STATUS_LIVE_TEMP_HI_LIVE_SHIFT 4 |
#define | _EFP01_STATUS_LIVE_VDD_LOW_LIVE_MASK 0x08 |
#define | _EFP01_STATUS_LIVE_VDD_LOW_LIVE_SHIFT 3 |
#define | _EFP01_STATUS_LIVE_VOA_INREG_LIVE_MASK 0x01 |
#define | _EFP01_STATUS_LIVE_VOA_INREG_LIVE_SHIFT 0 |
#define | _EFP01_STATUS_LIVE_VOB_INREG_LIVE_MASK 0x02 |
#define | _EFP01_STATUS_LIVE_VOB_INREG_LIVE_SHIFT 1 |
#define | _EFP01_STATUS_LIVE_VOC_INREG_LIVE_MASK 0x04 |
#define | _EFP01_STATUS_LIVE_VOC_INREG_LIVE_SHIFT 2 |
#define | _EFP01_STATUS_V_ADDRESS 0x01 |
#define | _EFP01_STATUS_V_RESETVALUE 0x00 |
#define | _EFP01_STATUS_V_VOA_ISGOOD_MASK 0x01 |
#define | _EFP01_STATUS_V_VOA_ISGOOD_SHIFT 0 |
#define | _EFP01_STATUS_V_VOA_ISLOW_MASK 0x08 |
#define | _EFP01_STATUS_V_VOA_ISLOW_SHIFT 3 |
#define | _EFP01_STATUS_V_VOB_ISGOOD_MASK 0x02 |
#define | _EFP01_STATUS_V_VOB_ISGOOD_SHIFT 1 |
#define | _EFP01_STATUS_V_VOB_ISLOW_MASK 0x10 |
#define | _EFP01_STATUS_V_VOB_ISLOW_SHIFT 4 |
#define | _EFP01_STATUS_V_VOC_ISGOOD_MASK 0x04 |
#define | _EFP01_STATUS_V_VOC_ISGOOD_SHIFT 2 |
#define | _EFP01_STATUS_V_VOC_ISLOW_MASK 0x20 |
#define | _EFP01_STATUS_V_VOC_ISLOW_SHIFT 5 |
#define | _EFP01_STATUS_VM_ADDRESS 0x03 |
#define | _EFP01_STATUS_VM_RESETVALUE 0x00 |
#define | _EFP01_STATUS_VM_VOA_ISGOOD_UNMASK_MASK 0x01 |
#define | _EFP01_STATUS_VM_VOA_ISGOOD_UNMASK_SHIFT 0 |
#define | _EFP01_STATUS_VM_VOA_ISLOW_UNMASK_MASK 0x08 |
#define | _EFP01_STATUS_VM_VOA_ISLOW_UNMASK_SHIFT 3 |
#define | _EFP01_STATUS_VM_VOB_ISGOOD_UNMASK_MASK 0x02 |
#define | _EFP01_STATUS_VM_VOB_ISGOOD_UNMASK_SHIFT 1 |
#define | _EFP01_STATUS_VM_VOB_ISLOW_UNMASK_MASK 0x10 |
#define | _EFP01_STATUS_VM_VOB_ISLOW_UNMASK_SHIFT 4 |
#define | _EFP01_STATUS_VM_VOC_ISGOOD_UNMASK_MASK 0x04 |
#define | _EFP01_STATUS_VM_VOC_ISGOOD_UNMASK_SHIFT 2 |
#define | _EFP01_STATUS_VM_VOC_ISLOW_UNMASK_MASK 0x20 |
#define | _EFP01_STATUS_VM_VOC_ISLOW_UNMASK_SHIFT 5 |
#define | _EFP01_VDD_AVG_LSBY_ADDRESS 0x1C |
#define | _EFP01_VDD_AVG_LSBY_RESETVALUE 0x00 |
#define | _EFP01_VDD_AVG_LSBY_VDD_AVG_LSBY_MASK 0xFF |
#define | _EFP01_VDD_AVG_LSBY_VDD_AVG_LSBY_SHIFT 0 |
#define | _EFP01_VDD_AVG_MSN_ADDRESS 0x1B |
#define | _EFP01_VDD_AVG_MSN_RESETVALUE 0x00 |
#define | _EFP01_VDD_AVG_MSN_VDD_AVG_MSN_MASK 0x0F |
#define | _EFP01_VDD_AVG_MSN_VDD_AVG_MSN_SHIFT 0 |
#define | _EFP01_VDD_MAX_LSBY_ADDRESS 0x20 |
#define | _EFP01_VDD_MAX_LSBY_RESETVALUE 0x00 |
#define | _EFP01_VDD_MAX_LSBY_VDD_MAX_LSBY_MASK 0xFF |
#define | _EFP01_VDD_MAX_LSBY_VDD_MAX_LSBY_SHIFT 0 |
#define | _EFP01_VDD_MAX_MSN_ADDRESS 0x1F |
#define | _EFP01_VDD_MAX_MSN_RESETVALUE 0x00 |
#define | _EFP01_VDD_MAX_MSN_VDD_MAX_MSN_MASK 0x0F |
#define | _EFP01_VDD_MAX_MSN_VDD_MAX_MSN_SHIFT 0 |
#define | _EFP01_VDD_MIN_LSBY_ADDRESS 0x1E |
#define | _EFP01_VDD_MIN_LSBY_RESETVALUE 0x00 |
#define | _EFP01_VDD_MIN_LSBY_VDD_MIN_LSBY_MASK 0xFF |
#define | _EFP01_VDD_MIN_LSBY_VDD_MIN_LSBY_SHIFT 0 |
#define | _EFP01_VDD_MIN_MSN_ADDRESS 0x1D |
#define | _EFP01_VDD_MIN_MSN_RESETVALUE 0x00 |
#define | _EFP01_VDD_MIN_MSN_VDD_MIN_MSN_MASK 0x0F |
#define | _EFP01_VDD_MIN_MSN_VDD_MIN_MSN_SHIFT 0 |
#define | _EFP01_VOA_SW_STAT_ADDRESS 0x23 |
#define | _EFP01_VOA_SW_STAT_RESETVALUE 0x00 |
#define | _EFP01_VOA_SW_STAT_VOA_SW_ISBAD_MASK 0x01 |
#define | _EFP01_VOA_SW_STAT_VOA_SW_ISBAD_SHIFT 0 |
#define | _EFP01_VOA_V_ADDRESS 0x49 |
#define | _EFP01_VOA_V_RESETVALUE 0x00 |
#define | _EFP01_VOA_V_VOA_V_MASK 0x7F |
#define | _EFP01_VOA_V_VOA_V_SHIFT 0 |
#define | _EFP01_VOB_EM0_V_ADDRESS 0x4C |
#define | _EFP01_VOB_EM0_V_OOR_DIS_MASK 0x80 |
#define | _EFP01_VOB_EM0_V_OOR_DIS_SHIFT 7 |
#define | _EFP01_VOB_EM0_V_RESETVALUE 0x00 |
#define | _EFP01_VOB_EM0_V_VOB_EM0_V_MASK 0x7F |
#define | _EFP01_VOB_EM0_V_VOB_EM0_V_SHIFT 0 |
#define | _EFP01_VOB_EM2_V_ADDRESS 0x4D |
#define | _EFP01_VOB_EM2_V_RESETVALUE 0x00 |
#define | _EFP01_VOB_EM2_V_VOB_EM2_V_MASK 0x7F |
#define | _EFP01_VOB_EM2_V_VOB_EM2_V_SHIFT 0 |
#define | _EFP01_VOC_V_ADDRESS 0x4B |
#define | _EFP01_VOC_V_RESETVALUE 0x00 |
#define | _EFP01_VOC_V_VOC_V_MASK 0x3F |
#define | _EFP01_VOC_V_VOC_V_SHIFT 0 |
#define | EFP01_ADC_CC_CTRL 0x5C |
#define | EFP01_ADC_LIMITS 0x5D |
#define | EFP01_BB_CTRL3 0x50 |
#define | EFP01_BB_CTRL3_BB_MODE_AUTONOMOUS (_EFP01_BB_CTRL3_BB_MODE_AUTONOMOUS << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_DISABLED (_EFP01_BB_CTRL3_BB_MODE_DISABLED << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_FORCEBOOST (_EFP01_BB_CTRL3_BB_MODE_FORCEBOOST << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_FORCEBUCK (_EFP01_BB_CTRL3_BB_MODE_FORCEBUCK << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_FORCENTM (_EFP01_BB_CTRL3_BB_MODE_FORCENTM << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_WIREDBOOST (_EFP01_BB_CTRL3_BB_MODE_WIREDBOOST << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_WIREDBUCK (_EFP01_BB_CTRL3_BB_MODE_WIREDBUCK << 0) |
#define | EFP01_BB_CTRL3_BB_MODE_WIREDBUCKLDO (_EFP01_BB_CTRL3_BB_MODE_WIREDBUCKLDO << 0) |
#define | EFP01_BB_CTRL3_NTM_DUR_107PCT (_EFP01_BB_CTRL3_NTM_DUR_107PCT << 3) |
#define | EFP01_BB_CTRL3_NTM_DUR_130PCT (_EFP01_BB_CTRL3_NTM_DUR_130PCT << 3) |
#define | EFP01_BB_CTRL3_NTM_DUR_60PCT (_EFP01_BB_CTRL3_NTM_DUR_60PCT << 3) |
#define | EFP01_BB_CTRL3_NTM_DUR_83PCT (_EFP01_BB_CTRL3_NTM_DUR_83PCT << 3) |
#define | EFP01_BB_CTRL5 0x51 |
#define | EFP01_BB_CTRL6 0x52 |
#define | EFP01_BB_CTRL6_BB_TOFF_MAX_0P9US (_EFP01_BB_CTRL6_BB_TOFF_MAX_0P9US << 0) |
#define | EFP01_BB_CTRL6_BB_TOFF_MAX_1P5US (_EFP01_BB_CTRL6_BB_TOFF_MAX_1P5US << 0) |
#define | EFP01_BB_CTRL6_BB_TOFF_MAX_2P1US (_EFP01_BB_CTRL6_BB_TOFF_MAX_2P1US << 0) |
#define | EFP01_BB_CTRL6_BB_TOFF_MAX_NOLIMIT (_EFP01_BB_CTRL6_BB_TOFF_MAX_NOLIMIT << 0) |
#define | EFP01_BB_IPK 0x4F |
#define | EFP01_BBK_CTRL 0x5A |
#define | EFP01_BIAS_SW 0x4E |
#define | EFP01_BIAS_SW_BIAS0_100NA (_EFP01_BIAS_SW_BIAS0_100NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_114NA (_EFP01_BIAS_SW_BIAS0_114NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_147NA (_EFP01_BIAS_SW_BIAS0_147NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_325NA (_EFP01_BIAS_SW_BIAS0_325NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_386NA (_EFP01_BIAS_SW_BIAS0_386NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_453NA (_EFP01_BIAS_SW_BIAS0_453NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_600NA (_EFP01_BIAS_SW_BIAS0_600NA << 0) |
#define | EFP01_BIAS_SW_BIAS0_87NA (_EFP01_BIAS_SW_BIAS0_87NA << 0) |
#define | EFP01_BIAS_SW_BIAS2_100NA (_EFP01_BIAS_SW_BIAS2_100NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_114NA (_EFP01_BIAS_SW_BIAS2_114NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_147NA (_EFP01_BIAS_SW_BIAS2_147NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_325NA (_EFP01_BIAS_SW_BIAS2_325NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_386NA (_EFP01_BIAS_SW_BIAS2_386NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_453NA (_EFP01_BIAS_SW_BIAS2_453NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_600NA (_EFP01_BIAS_SW_BIAS2_600NA << 3) |
#define | EFP01_BIAS_SW_BIAS2_87NA (_EFP01_BIAS_SW_BIAS2_87NA << 3) |
#define | EFP01_BIAS_SW_VOA_SW_CON_OFF (_EFP01_BIAS_SW_VOA_SW_CON_OFF << 6) |
#define | EFP01_BIAS_SW_VOA_SW_CON_ON (_EFP01_BIAS_SW_VOA_SW_CON_ON << 6) |
#define | EFP01_BIAS_SW_VOA_SW_CON_ONINEM0 (_EFP01_BIAS_SW_VOA_SW_CON_ONINEM0 << 6) |
#define | EFP01_BIAS_SW_VOA_SW_CON_ONINEM02 (_EFP01_BIAS_SW_VOA_SW_CON_ONINEM02 << 6) |
#define | EFP01_BK_CTRL0 0x56 |
#define | EFP01_BK_CTRL1 0x57 |
#define | EFP01_BK_CTRL1_BK_MODE_BUCKLDO (_EFP01_BK_CTRL1_BK_MODE_BUCKLDO << 3) |
#define | EFP01_BK_CTRL1_BK_MODE_BUCKONLY (_EFP01_BK_CTRL1_BK_MODE_BUCKONLY << 3) |
#define | EFP01_BK_CTRL1_BK_MODE_DISABLED (_EFP01_BK_CTRL1_BK_MODE_DISABLED << 3) |
#define | EFP01_BK_CTRL1_BK_MODE_LDOONLY (_EFP01_BK_CTRL1_BK_MODE_LDOONLY << 3) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_1190NS (_EFP01_BK_CTRL1_BK_TON_MAX_1190NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_1470NS (_EFP01_BK_CTRL1_BK_TON_MAX_1470NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_1750NS (_EFP01_BK_CTRL1_BK_TON_MAX_1750NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_2030NS (_EFP01_BK_CTRL1_BK_TON_MAX_2030NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_350NS (_EFP01_BK_CTRL1_BK_TON_MAX_350NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_630NS (_EFP01_BK_CTRL1_BK_TON_MAX_630NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_910NS (_EFP01_BK_CTRL1_BK_TON_MAX_910NS << 5) |
#define | EFP01_BK_CTRL1_BK_TON_MAX_NOLIMIT (_EFP01_BK_CTRL1_BK_TON_MAX_NOLIMIT << 5) |
#define | EFP01_BK_CTRL2 0x59 |
#define | EFP01_BK_IPK 0x58 |
#define | EFP01_CC_CAL 0x0A |
#define | EFP01_CC_CAL_CCL_LVL_11200UA (_EFP01_CC_CAL_CCL_LVL_11200UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_14000UA (_EFP01_CC_CAL_CCL_LVL_14000UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_440UA (_EFP01_CC_CAL_CCL_LVL_440UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_550UA (_EFP01_CC_CAL_CCL_LVL_550UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_700UA (_EFP01_CC_CAL_CCL_LVL_700UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_7060UA (_EFP01_CC_CAL_CCL_LVL_7060UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_875UA (_EFP01_CC_CAL_CCL_LVL_875UA << 0) |
#define | EFP01_CC_CAL_CCL_LVL_8830UA (_EFP01_CC_CAL_CCL_LVL_8830UA << 0) |
#define | EFP01_CC_CAL_CCL_SEL_NONE (_EFP01_CC_CAL_CCL_SEL_NONE << 3) |
#define | EFP01_CC_CAL_CCL_SEL_VOA (_EFP01_CC_CAL_CCL_SEL_VOA << 3) |
#define | EFP01_CC_CAL_CCL_SEL_VOB (_EFP01_CC_CAL_CCL_SEL_VOB << 3) |
#define | EFP01_CC_CAL_CCL_SEL_VOC (_EFP01_CC_CAL_CCL_SEL_VOC << 3) |
#define | EFP01_CC_CTRL 0x41 |
#define | EFP01_CC_CTRL_CC_THRSH_50PCT (_EFP01_CC_CTRL_CC_THRSH_50PCT << 5) |
#define | EFP01_CC_CTRL_CC_THRSH_62PCT (_EFP01_CC_CTRL_CC_THRSH_62PCT << 5) |
#define | EFP01_CC_CTRL_CC_THRSH_75PCT (_EFP01_CC_CTRL_CC_THRSH_75PCT << 5) |
#define | EFP01_CC_CTRL_CC_THRSH_87PCT (_EFP01_CC_CTRL_CC_THRSH_87PCT << 5) |
#define | EFP01_CC_MODE 0x12 |
#define | EFP01_CC_MODE_CCA_MODE_AUTO (_EFP01_CC_MODE_CCA_MODE_AUTO << 0) |
#define | EFP01_CC_MODE_CCA_MODE_BOOST (_EFP01_CC_MODE_CCA_MODE_BOOST << 0) |
#define | EFP01_CC_MODE_CCA_MODE_BUCK (_EFP01_CC_MODE_CCA_MODE_BUCK << 0) |
#define | EFP01_CC_MODE_CCA_MODE_LDO (_EFP01_CC_MODE_CCA_MODE_LDO << 0) |
#define | EFP01_CC_MODE_CCB_MODE_BUCK (_EFP01_CC_MODE_CCB_MODE_BUCK << 2) |
#define | EFP01_CC_MODE_CCB_MODE_LDOB (_EFP01_CC_MODE_CCB_MODE_LDOB << 2) |
#define | EFP01_CCA_LSBY 0x14 |
#define | EFP01_CCA_MSBY 0x13 |
#define | EFP01_CCB0_LSBY 0x16 |
#define | EFP01_CCB0_MSBY 0x15 |
#define | EFP01_CCB2_LSBY 0x18 |
#define | EFP01_CCB2_MSBY 0x17 |
#define | EFP01_CCC_LSBY 0x1A |
#define | EFP01_CCC_MSBY 0x19 |
#define | EFP01_CMD 0x10 |
#define | EFP01_DEVREV_ID 0x05 |
#define | EFP01_EM_CRSREG_CTRL 0x43 |
#define | EFP01_EM_CRSREG_CTRL_EM_STSEL_EM0 (_EFP01_EM_CRSREG_CTRL_EM_STSEL_EM0 << 1) |
#define | EFP01_EM_CRSREG_CTRL_EM_STSEL_EM2 (_EFP01_EM_CRSREG_CTRL_EM_STSEL_EM2 << 1) |
#define | EFP01_EM_CRSREG_CTRL_EM_STSEL_EM4 (_EFP01_EM_CRSREG_CTRL_EM_STSEL_EM4 << 1) |
#define | EFP01_EM_CRSREG_CTRL_EM_STSEL_RESERVED (_EFP01_EM_CRSREG_CTRL_EM_STSEL_RESERVED << 1) |
#define | EFP01_I2C_CTRL 0x40 |
#define | EFP01_LDOB_CTRL 0x53 |
#define | EFP01_LDOC_BB_CTRL 0x55 |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_1190NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_1190NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_1470NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_1470NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_1750NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_1750NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_2030NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_2030NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_350NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_350NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_630NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_630NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_910NS (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_910NS << 4) |
#define | EFP01_LDOC_BB_CTRL_BB_TON_MAX_NOLIMIT (_EFP01_LDOC_BB_CTRL_BB_TON_MAX_NOLIMIT << 4) |
#define | EFP01_LDOC_CTRL 0x54 |
#define | EFP01_OTP_ADC_CC_CTRL 0x1C |
#define | EFP01_OTP_ADC_LIMITS 0x1D |
#define | EFP01_OTP_ADDR 0x0B |
#define | EFP01_OTP_BB_CTRL3 0x10 |
#define | EFP01_OTP_BB_CTRL5 0x11 |
#define | EFP01_OTP_BB_CTRL6 0x12 |
#define | EFP01_OTP_BB_IPK 0x0F |
#define | EFP01_OTP_BBK_CTRL 0x1A |
#define | EFP01_OTP_BIAS_SW 0x0E |
#define | EFP01_OTP_BK_CTRL0 0x16 |
#define | EFP01_OTP_BK_CTRL1 0x17 |
#define | EFP01_OTP_BK_CTRL2 0x19 |
#define | EFP01_OTP_BK_IPK 0x18 |
#define | EFP01_OTP_CC_CTRL 0x01 |
#define | EFP01_OTP_CCCAL_HIGH 0x34 |
#define | EFP01_OTP_CCCAL_LOW 0x33 |
#define | EFP01_OTP_EM_CRSREG_CTRL 0x03 |
#define | EFP01_OTP_I2C_CTRL 0x00 |
#define | EFP01_OTP_LDOB_CTRL 0x13 |
#define | EFP01_OTP_LDOC_BB_CTRL 0x15 |
#define | EFP01_OTP_LDOC_CTRL 0x14 |
#define | EFP01_OTP_OPN_NUM 0x30 |
#define | EFP01_OTP_OPN_REV 0x31 |
#define | EFP01_OTP_RDATA 0x0C |
#define | EFP01_OTP_STATCTRL 0x0E |
#define | EFP01_OTP_TEMP_CODE 0x2F |
#define | EFP01_OTP_UID_HIGH 0x21 |
#define | EFP01_OTP_UID_LOW 0x20 |
#define | EFP01_OTP_VOA_V 0x09 |
#define | EFP01_OTP_VOB_EM0_V 0x0C |
#define | EFP01_OTP_VOB_EM2_V 0x0D |
#define | EFP01_OTP_VOC_V 0x0B |
#define | EFP01_STATUS_G 0x00 |
#define | EFP01_STATUS_GM 0x02 |
#define | EFP01_STATUS_LIVE 0x04 |
#define | EFP01_STATUS_V 0x01 |
#define | EFP01_STATUS_VM 0x03 |
#define | EFP01_VDD_AVG_LSBY 0x1C |
#define | EFP01_VDD_AVG_MSN 0x1B |
#define | EFP01_VDD_MAX_LSBY 0x20 |
#define | EFP01_VDD_MAX_MSN 0x1F |
#define | EFP01_VDD_MIN_LSBY 0x1E |
#define | EFP01_VDD_MIN_MSN 0x1D |
#define | EFP01_VOA_SW_STAT 0x23 |
#define | EFP01_VOA_V 0x49 |
#define | EFP01_VOB_EM0_V 0x4C |
#define | EFP01_VOB_EM2_V 0x4D |
#define | EFP01_VOC_V 0x4B |
#define | SL_EFPDRV_I2C_ERROR 1 |
I2C transfer error.
|
|
#define | SL_EFPDRV_NOT_SUPPORTED 2 |
Operation not supported.
|
|
#define | SL_EFPDRV_OK 0 |
Success.
|
|
Enumerations |
|
enum |
sl_efpdrv_voa_mode_t
{
efp_voa_mode_disabled = _EFP01_BB_CTRL3_BB_MODE_DISABLED, efp_voa_mode_wired_buck = _EFP01_BB_CTRL3_BB_MODE_WIREDBUCK, efp_voa_mode_wired_boost = _EFP01_BB_CTRL3_BB_MODE_WIREDBOOST, efp_voa_mode_wired_buck_ldo = _EFP01_BB_CTRL3_BB_MODE_WIREDBUCKLDO, efp_voa_mode_buck_boost_autonomous = _EFP01_BB_CTRL3_BB_MODE_AUTONOMOUS, efp_voa_mode_buck_boost_forced_buck = _EFP01_BB_CTRL3_BB_MODE_FORCEBUCK, efp_voa_mode_buck_boost_forced_ntm = _EFP01_BB_CTRL3_BB_MODE_FORCENTM, efp_voa_mode_buck_boost_forced_boost = _EFP01_BB_CTRL3_BB_MODE_FORCEBOOST } |
VOA regulator modes.
|
|
enum |
sl_efpdrv_voa_sw_mode_t
{
efp_voa_sw_mode_off = _EFP01_BIAS_SW_VOA_SW_CON_OFF, efp_voa_sw_mode_on = _EFP01_BIAS_SW_VOA_SW_CON_ON, efp_voa_sw_mode_on_in_em0 = _EFP01_BIAS_SW_VOA_SW_CON_ONINEM0, efp_voa_sw_mode_on_in_em02 = _EFP01_BIAS_SW_VOA_SW_CON_ONINEM02 } |
VOA SW (switched output) modes.
|
|
enum |
sl_efpdrv_vob_mode_t
{
efp_vob_mode_disabled = _EFP01_BK_CTRL1_BK_MODE_DISABLED, efp_vob_mode_buck = _EFP01_BK_CTRL1_BK_MODE_BUCKONLY, efp_vob_mode_ldo = _EFP01_BK_CTRL1_BK_MODE_LDOONLY, efp_vob_mode_buck_ldo = _EFP01_BK_CTRL1_BK_MODE_BUCKLDO } |
VOB regulator modes.
|
|
Functions |
|
int | sl_efpdrv_enable_direct_mode (void) |
Configure I2C GPIO pins for "direct mode" EM transfer mode.
|
|
int | sl_efpdrv_enter_em0 (void) |
Set EFP in EM0 energy mode.
|
|
int | sl_efpdrv_enter_em2 (void) |
Set EFP in EM2 energy mode.
|
|
int | sl_efpdrv_get_vdd_avg (uint16_t *voltage_mv) |
Measure average VDD.
|
|
int | sl_efpdrv_get_vdd_max (uint16_t *voltage_mv) |
Measure maximum VDD.
|
|
int | sl_efpdrv_get_vdd_min (uint16_t *voltage_mv) |
Measure minimum VDD.
|
|
int | sl_efpdrv_init (const sl_efpdrv_init_data *init) |
Initialize EFP driver and configure underlying EFP hardware.
|
|
int | sl_efpdrv_read_otp (uint8_t addr, uint8_t *data) |
Read EFP OTP register.
|
|
int | sl_efpdrv_read_register (uint8_t addr, uint8_t *data) |
Read EFP control register.
|
|
int | sl_efpdrv_read_register_field (uint8_t addr, uint8_t *data, uint8_t mask, uint8_t pos) |
Read EFP control register field.
|
|
int | sl_efpdrv_set_voa_em01_peak_current (unsigned int current_ma, unsigned int vddb_mv, unsigned int voa_mv, unsigned int inductor_nh) |
Set regulator VOA EM01 peak output current.
|
|
int | sl_efpdrv_set_voa_em23_peak_current (unsigned int current_ma, unsigned int vddb_mv, unsigned int voa_mv, unsigned int inductor_nh) |
Set regulator VOA EM23 peak output current.
|
|
int | sl_efpdrv_set_voa_mode ( sl_efpdrv_voa_mode_t mode) |
Set regulator VOA mode.
|
|
int | sl_efpdrv_set_voa_sw_mode ( sl_efpdrv_voa_sw_mode_t mode) |
Set VOA SW (switched output) mode.
|
|
int | sl_efpdrv_set_voa_voltage (unsigned int voltage_mv) |
Set regulator VOA output voltage.
|
|
int | sl_efpdrv_set_vob_em01_peak_current (unsigned int current_ma, unsigned int vddb_mv, unsigned int vob_mv, unsigned int inductor_nh) |
Set regulator VOB EM01 peak output current.
|
|
int | sl_efpdrv_set_vob_em01_voltage (unsigned int voltage_mv) |
Set regulator VOB EM01 output voltage.
|
|
int | sl_efpdrv_set_vob_em23_peak_current (unsigned int current_ma, unsigned int vddb_mv, unsigned int vob_mv, unsigned int inductor_nh) |
Set regulator VOB EM23 peak output current.
|
|
int | sl_efpdrv_set_vob_em23_voltage (unsigned int voltage_mv) |
Set regulator VOB EM23 output voltage.
|
|
int | sl_efpdrv_set_vob_mode ( sl_efpdrv_vob_mode_t mode) |
Set regulator VOB mode.
|
|
int | sl_efpdrv_set_voc_voltage (unsigned int voltage_mv) |
Set regulator VOC output voltage.
|
|
int | sl_efpdrv_shutdown_emu_ldo (void) |
Turn off the internal EMU LDO that supplies DECOUPLE pin.
|
|
int | sl_efpdrv_write_register (uint8_t addr, uint8_t data) |
Write EFP control register.
|
|
int | sl_efpdrv_write_register_field (uint8_t addr, uint8_t data, uint8_t mask, uint8_t pos) |
Write EFP control register field.
|
|
Macro Definition Documentation
#define _EFP01_ADC_CC_CTRL_ADDRESS 0x5C |
Bit fields for EFP01_ADC_CC_CTRL
Definition at line
723
of file
sl_efp01.h
.
#define _EFP01_ADC_LIMITS_ADDRESS 0x5D |
Bit fields for EFP01_ADC_LIMITS
Definition at line
731
of file
sl_efp01.h
.
#define _EFP01_BB_CTRL3_ADDRESS 0x50 |
Bit fields for EFP01_BB_CTRL3
Definition at line
541
of file
sl_efp01.h
.
#define _EFP01_BB_CTRL5_ADDRESS 0x51 |
Bit fields for EFP01_BB_CTRL5
Definition at line
575
of file
sl_efp01.h
.
#define _EFP01_BB_CTRL6_ADDRESS 0x52 |
Bit fields for EFP01_BB_CTRL6
Definition at line
583
of file
sl_efp01.h
.
#define _EFP01_BB_IPK_ADDRESS 0x4F |
Bit fields for EFP01_BB_IPK
Definition at line
533
of file
sl_efp01.h
.
#define _EFP01_BBK_CTRL_ADDRESS 0x5A |
Bit fields for EFP01_BBK_CTRL
Definition at line
713
of file
sl_efp01.h
.
#define _EFP01_BIAS_SW_ADDRESS 0x4E |
Bit fields for EFP01_BIAS_SW
Definition at line
483
of file
sl_efp01.h
.
#define _EFP01_BK_CTRL0_ADDRESS 0x56 |
Bit fields for EFP01_BK_CTRL0
Definition at line
653
of file
sl_efp01.h
.
#define _EFP01_BK_CTRL1_ADDRESS 0x57 |
Bit fields for EFP01_BK_CTRL1
Definition at line
661
of file
sl_efp01.h
.
#define _EFP01_BK_CTRL2_ADDRESS 0x59 |
Bit fields for EFP01_BK_CTRL2
Definition at line
703
of file
sl_efp01.h
.
#define _EFP01_BK_IPK_ADDRESS 0x58 |
Bit fields for EFP01_BK_IPK
Definition at line
695
of file
sl_efp01.h
.
#define _EFP01_CC_CAL_ADDRESS 0x0A |
Bit fields for EFP01_CC_CAL
Definition at line
209
of file
sl_efp01.h
.
#define _EFP01_CC_CTRL_ADDRESS 0x41 |
Bit fields for EFP01_CC_CTRL
Definition at line
413
of file
sl_efp01.h
.
#define _EFP01_CC_MODE_ADDRESS 0x12 |
Bit fields for EFP01_CC_MODE
Definition at line
289
of file
sl_efp01.h
.
#define _EFP01_CCA_LSBY_ADDRESS 0x14 |
Bit fields for EFP01_CCA_LSBY
Definition at line
317
of file
sl_efp01.h
.
#define _EFP01_CCA_MSBY_ADDRESS 0x13 |
Bit fields for EFP01_CCA_MSBY
Definition at line
311
of file
sl_efp01.h
.
#define _EFP01_CCB0_LSBY_ADDRESS 0x16 |
Bit fields for EFP01_CCB0_LSBY
Definition at line
329
of file
sl_efp01.h
.
#define _EFP01_CCB0_MSBY_ADDRESS 0x15 |
Bit fields for EFP01_CCB0_MSBY
Definition at line
323
of file
sl_efp01.h
.
#define _EFP01_CCB2_LSBY_ADDRESS 0x18 |
Bit fields for EFP01_CCB2_LSBY
Definition at line
341
of file
sl_efp01.h
.
#define _EFP01_CCB2_MSBY_ADDRESS 0x17 |
Bit fields for EFP01_CCB2_MSBY
Definition at line
335
of file
sl_efp01.h
.
#define _EFP01_CCC_LSBY_ADDRESS 0x1A |
Bit fields for EFP01_CCC_LSBY
Definition at line
353
of file
sl_efp01.h
.
#define _EFP01_CCC_MSBY_ADDRESS 0x19 |
Bit fields for EFP01_CCC_MSBY
Definition at line
347
of file
sl_efp01.h
.
#define _EFP01_CMD_ADDRESS 0x10 |
Bit fields for EFP01_CMD
Definition at line
271
of file
sl_efp01.h
.
#define _EFP01_DEVREV_ID_ADDRESS 0x05 |
Bit fields for EFP01_DEVREV_ID
Definition at line
201
of file
sl_efp01.h
.
#define _EFP01_EM_CRSREG_CTRL_ADDRESS 0x43 |
Bit fields for EFP01_EM_CRSREG_CTRL
Definition at line
431
of file
sl_efp01.h
.
#define _EFP01_I2C_CTRL_ADDRESS 0x40 |
Bit fields for EFP01_I2C_CTRL
Definition at line
401
of file
sl_efp01.h
.
#define _EFP01_LDOB_CTRL_ADDRESS 0x53 |
Bit fields for EFP01_LDOB_CTRL
Definition at line
603
of file
sl_efp01.h
.
#define _EFP01_LDOC_BB_CTRL_ADDRESS 0x55 |
Bit fields for EFP01_LDOC_BB_CTRL
Definition at line
627
of file
sl_efp01.h
.
#define _EFP01_LDOC_CTRL_ADDRESS 0x54 |
Bit fields for EFP01_LDOC_CTRL
Definition at line
615
of file
sl_efp01.h
.
#define _EFP01_OTP_ADDR_ADDRESS 0x0B |
Bit fields for EFP01_OTP_ADDR
Definition at line
243
of file
sl_efp01.h
.
#define _EFP01_OTP_RDATA_ADDRESS 0x0C |
Bit fields for EFP01_OTP_RDATA
Definition at line
249
of file
sl_efp01.h
.
#define _EFP01_OTP_STATCTRL_ADDRESS 0x0E |
Bit fields for EFP01_OTP_STATCTRL
Definition at line
255
of file
sl_efp01.h
.
#define _EFP01_STATUS_G_ADDRESS 0x00 |
Bit fields for EFP01_STATUS_G
Definition at line
113
of file
sl_efp01.h
.
#define _EFP01_STATUS_GM_ADDRESS 0x02 |
Bit fields for EFP01_STATUS_GM
Definition at line
149
of file
sl_efp01.h
.
#define _EFP01_STATUS_LIVE_ADDRESS 0x04 |
Bit fields for EFP01_STATUS_LIVE
Definition at line
185
of file
sl_efp01.h
.
#define _EFP01_STATUS_V_ADDRESS 0x01 |
Bit fields for EFP01_STATUS_V
Definition at line
133
of file
sl_efp01.h
.
#define _EFP01_STATUS_VM_ADDRESS 0x03 |
Bit fields for EFP01_STATUS_VM
Definition at line
169
of file
sl_efp01.h
.
#define _EFP01_VDD_AVG_LSBY_ADDRESS 0x1C |
Bit fields for EFP01_VDD_AVG_LSBY
Definition at line
365
of file
sl_efp01.h
.
#define _EFP01_VDD_AVG_MSN_ADDRESS 0x1B |
Bit fields for EFP01_VDD_AVG_MSN
Definition at line
359
of file
sl_efp01.h
.
#define _EFP01_VDD_MAX_LSBY_ADDRESS 0x20 |
Bit fields for EFP01_VDD_MAX_LSBY
Definition at line
389
of file
sl_efp01.h
.
#define _EFP01_VDD_MAX_MSN_ADDRESS 0x1F |
Bit fields for EFP01_VDD_MAX_MSN
Definition at line
383
of file
sl_efp01.h
.
#define _EFP01_VDD_MIN_LSBY_ADDRESS 0x1E |
Bit fields for EFP01_VDD_MIN_LSBY
Definition at line
377
of file
sl_efp01.h
.
#define _EFP01_VDD_MIN_MSN_ADDRESS 0x1D |
Bit fields for EFP01_VDD_MIN_MSN
Definition at line
371
of file
sl_efp01.h
.
#define _EFP01_VOA_SW_STAT_ADDRESS 0x23 |
Bit fields for EFP01_VOA_SW_STAT
Definition at line
395
of file
sl_efp01.h
.
#define _EFP01_VOA_V_ADDRESS 0x49 |
Bit fields for EFP01_VOA_V
Definition at line
457
of file
sl_efp01.h
.
#define _EFP01_VOB_EM0_V_ADDRESS 0x4C |
Bit fields for EFP01_VOB_EM0_V
Definition at line
469
of file
sl_efp01.h
.
#define _EFP01_VOB_EM2_V_ADDRESS 0x4D |
Bit fields for EFP01_VOB_EM2_V
Definition at line
477
of file
sl_efp01.h
.
#define _EFP01_VOC_V_ADDRESS 0x4B |
Bit fields for EFP01_VOC_V
Definition at line
463
of file
sl_efp01.h
.
#define EFP01_OTP_I2C_CTRL 0x00 |
EFP01 OTP Register definitions.
Definition at line
31
of file
sl_efp01.h
.
#define EFP01_STATUS_G 0x00 |
EFP01 Register definitions.
Definition at line
62
of file
sl_efp01.h
.
Referenced by sl_efpdrv_init() .
Enumeration Type Documentation
enum sl_efpdrv_voa_mode_t |
VOA regulator modes.
Definition at line
48
of file
sl_efpdrv.h
.
enum sl_efpdrv_vob_mode_t |
Function Documentation
int sl_efpdrv_enable_direct_mode | ( | void |
|
) |
Configure I2C GPIO pins for "direct mode" EM transfer mode.
- Note
- This must be the last EFP driver function called prior to entering EM2/3 via EMU_EnterEMx() calls. Any EFP API call that involves an I2C transfer will leave the I2C GPIO pins in I2C mode.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
226
of file
sl_efpdrv.c
.
References sl_efpdrv_enter_em0() .
Referenced by sl_efpdrv_init() .
int sl_efpdrv_enter_em0 | ( | void |
|
) |
Set EFP in EM0 energy mode.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
238
of file
sl_efpdrv.c
.
References GPIO_PinOutSet() , sl_efpdrv_init_data::i2c_scl_pin , sl_efpdrv_init_data::i2c_scl_port , SL_EFPDRV_OK , and sl_efpdrv_write_register_field() .
Referenced by sl_efpdrv_enable_direct_mode() .
int sl_efpdrv_enter_em2 | ( | void |
|
) |
Set EFP in EM2 energy mode.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
267
of file
sl_efpdrv.c
.
References GPIO_PinOutClear() , sl_efpdrv_init_data::i2c_scl_pin , sl_efpdrv_init_data::i2c_scl_port , SL_EFPDRV_OK , and sl_efpdrv_write_register_field() .
int sl_efpdrv_get_vdd_avg | ( | uint16_t * |
voltage_mv
|
) |
Measure average VDD.
- Note
- This function will measure VDDA or VDDB depending of the voltage on the VDDA pin after power on. If VDDA is powered this function returns a VDDA reading, otherwise a VDDB reading is returned.
- Parameters
-
[out] voltage_mv
Average VDD voltage expressed in miilivolts.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
304
of file
sl_efpdrv.c
.
int sl_efpdrv_get_vdd_max | ( | uint16_t * |
voltage_mv
|
) |
Measure maximum VDD.
- Note
- This function will measure VDDA or VDDB depending of the voltage on the VDDA pin after power on. If VDDA is powered this function returns a VDDA reading, otherwise a VDDB reading is returned.
- Parameters
-
[out] voltage_mv
Maximum VDD voltage expressed in miilivolts.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
324
of file
sl_efpdrv.c
.
int sl_efpdrv_get_vdd_min | ( | uint16_t * |
voltage_mv
|
) |
Measure minimum VDD.
- Note
- This function will measure VDDA or VDDB depending of the voltage on the VDDA pin after power on. If VDDA is powered this function returns a VDDA reading, otherwise a VDDB reading is returned.
- Parameters
-
[out] voltage_mv
Minimum VDD voltage expressed in miilivolts.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
344
of file
sl_efpdrv.c
.
int sl_efpdrv_init | ( | const sl_efpdrv_init_data * |
init
|
) |
Initialize EFP driver and configure underlying EFP hardware.
- Parameters
-
[in] init
Initialization data structure.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
359
of file
sl_efpdrv.c
.
References sl_efpdrv_init_data::config_data , sl_efpdrv_init_data::config_size , EFP01_STATUS_G , sl_efpdrv_init_data::enable_irq_pin , GPIO_PinModeSet() , gpioModeInputPull , I2C_FREQ_FASTPLUS_MAX , sl_efpdrv_init_data::i2c_instance , sl_efpdrv_init_data::i2c_scl_pin , sl_efpdrv_init_data::i2c_scl_port , sl_efpdrv_init_data::i2c_sda_pin , sl_efpdrv_init_data::i2c_sda_port , i2cClockHLRStandard , I2CSPM_Init() , sl_efpdrv_init_data::irq_pin , sl_efpdrv_init_data::irq_port , I2CSPM_Init_TypeDef::port , sl_efpdrv_enable_direct_mode() , SL_EFPDRV_OK , sl_efpdrv_read_register() , and sl_efpdrv_write_register() .
int sl_efpdrv_read_otp | ( | uint8_t |
addr,
|
uint8_t * |
data
|
||
) |
Read EFP OTP register.
- Parameters
-
[in] addr
Register address. [out] data
The value read from the OTP register.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
466
of file
sl_efpdrv.c
.
References SL_EFPDRV_OK , sl_efpdrv_read_register() , sl_efpdrv_write_register() , and sl_efpdrv_write_register_field() .
int sl_efpdrv_read_register | ( | uint8_t |
addr,
|
uint8_t * |
data
|
||
) |
Read EFP control register.
- Parameters
-
[in] addr
Register address. [out] data
The value read from the register.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
517
of file
sl_efpdrv.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_FLAG_WRITE_READ , sl_efpdrv_init_data::i2c_instance , I2CSPM_Transfer() , i2cTransferDone , SL_EFPDRV_I2C_ERROR , and SL_EFPDRV_OK .
Referenced by sl_efpdrv_init() , sl_efpdrv_read_otp() , sl_efpdrv_read_register_field() , and sl_efpdrv_write_register_field() .
int sl_efpdrv_read_register_field | ( | uint8_t |
addr,
|
uint8_t * |
data,
|
||
uint8_t |
mask,
|
||
uint8_t |
pos
|
||
) |
Read EFP control register field.
- Parameters
-
[in] addr
Register address. [out] data
The value read from the register field. [in] mask
Bit mask corresponding to target bit field. [in] pos
Bit number of least significant bit of target bit field.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
559
of file
sl_efpdrv.c
.
References SL_EFPDRV_OK , and sl_efpdrv_read_register() .
int sl_efpdrv_set_voa_em01_peak_current | ( | unsigned int |
current_ma,
|
unsigned int |
vddb_mv,
|
||
unsigned int |
voa_mv,
|
||
unsigned int |
inductor_nh
|
||
) |
Set regulator VOA EM01 peak output current.
- Parameters
-
[in] current_ma
Target peak current expressed in milliamperes. [in] vddb_mv
VDDB expressed in millivolt. [in] voa_mv
VOA expressed in millivolt. [in] inductor_nh
Inductor size expressed in nanohenry.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
593
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() , SL_MAX , and SL_MIN .
int sl_efpdrv_set_voa_em23_peak_current | ( | unsigned int |
current_ma,
|
unsigned int |
vddb_mv,
|
||
unsigned int |
voa_mv,
|
||
unsigned int |
inductor_nh
|
||
) |
Set regulator VOA EM23 peak output current.
- Parameters
-
[in] current_ma
Target peak current expressed in milliamperes. [in] vddb_mv
VDDB expressed in millivolt. [in] voa_mv
VOA expressed in millivolt. [in] inductor_nh
Inductor size expressed in nanohenry.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
630
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() , SL_MAX , and SL_MIN .
int sl_efpdrv_set_voa_mode | ( | sl_efpdrv_voa_mode_t |
mode
|
) |
Set regulator VOA mode.
- Parameters
-
[in] mode
Regulator mode.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
658
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() .
int sl_efpdrv_set_voa_sw_mode | ( | sl_efpdrv_voa_sw_mode_t |
mode
|
) |
Set VOA SW (switched output) mode.
- Parameters
-
[in] mode
VOA SW mode.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
693
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() .
int sl_efpdrv_set_voa_voltage | ( | unsigned int |
voltage_mv
|
) |
Set regulator VOA output voltage.
- Parameters
-
[in] voltage_mv
Voltage in millivolt.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
676
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register() .
int sl_efpdrv_set_vob_em01_peak_current | ( | unsigned int |
current_ma,
|
unsigned int |
vddb_mv,
|
||
unsigned int |
vob_mv,
|
||
unsigned int |
inductor_nh
|
||
) |
Set regulator VOB EM01 peak output current.
- Parameters
-
[in] current_ma
Target peak current expressed in milliamperes. [in] vddb_mv
VDDB expressed in millivolt. [in] vob_mv
VOB expressed in millivolt. [in] inductor_nh
Inductor size expressed in nanohenry.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
720
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() , SL_MAX , and SL_MIN .
int sl_efpdrv_set_vob_em01_voltage | ( | unsigned int |
voltage_mv
|
) |
Set regulator VOB EM01 output voltage.
- Parameters
-
[in] voltage_mv
Voltage in millivolt.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
748
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() .
int sl_efpdrv_set_vob_em23_peak_current | ( | unsigned int |
current_ma,
|
unsigned int |
vddb_mv,
|
||
unsigned int |
vob_mv,
|
||
unsigned int |
inductor_nh
|
||
) |
Set regulator VOB EM23 peak output current.
- Parameters
-
[in] current_ma
Target peak current expressed in milliamperes. [in] vddb_mv
VDDB expressed in millivolt. [in] vob_mv
VOB expressed in millivolt. [in] inductor_nh
Inductor size expressed in nanohenry.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
775
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() , SL_MAX , and SL_MIN .
int sl_efpdrv_set_vob_em23_voltage | ( | unsigned int |
voltage_mv
|
) |
Set regulator VOB EM23 output voltage.
- Parameters
-
[in] voltage_mv
Voltage in millivolt.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
803
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register() .
int sl_efpdrv_set_vob_mode | ( | sl_efpdrv_vob_mode_t |
mode
|
) |
Set regulator VOB mode.
- Parameters
-
[in] mode
Regulator mode.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
820
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register_field() .
int sl_efpdrv_set_voc_voltage | ( | unsigned int |
voltage_mv
|
) |
Set regulator VOC output voltage.
- Parameters
-
[in] voltage_mv
Voltage in millivolt.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
838
of file
sl_efpdrv.c
.
References sl_efpdrv_write_register() .
int sl_efpdrv_shutdown_emu_ldo | ( | void |
|
) |
Turn off the internal EMU LDO that supplies DECOUPLE pin.
- Note
- Make sure that an external source supply the DECOUPLE pin before calling this function.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_NOT_SUPPORTED.
Definition at line
856
of file
sl_efpdrv.c
.
References SL_EFPDRV_NOT_SUPPORTED , and SL_EFPDRV_OK .
int sl_efpdrv_write_register | ( | uint8_t |
addr,
|
uint8_t |
data
|
||
) |
Write EFP control register.
- Parameters
-
[in] addr
Register address. [in] data
The value to write to the register.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
882
of file
sl_efpdrv.c
.
References I2C_TransferSeq_TypeDef::addr , I2C_FLAG_WRITE_WRITE , sl_efpdrv_init_data::i2c_instance , I2CSPM_Transfer() , i2cTransferDone , SL_EFPDRV_I2C_ERROR , and SL_EFPDRV_OK .
Referenced by sl_efpdrv_init() , sl_efpdrv_read_otp() , sl_efpdrv_set_voa_voltage() , sl_efpdrv_set_vob_em23_voltage() , sl_efpdrv_set_voc_voltage() , and sl_efpdrv_write_register_field() .
int sl_efpdrv_write_register_field | ( | uint8_t |
addr,
|
uint8_t |
data,
|
||
uint8_t |
mask,
|
||
uint8_t |
pos
|
||
) |
Write EFP control register field.
- Note
- This function performs a read-modify-write of a EFP register.
- Parameters
-
[in] addr
Register address. [in] data
The value to write to the register field. [in] mask
Bit mask corresponding to target bit field. [in] pos
Bit number of least significant bit of target bit field.
- Returns
- SL_EFPDRV_OK or SL_EFPDRV_I2C_ERROR on I2C transfer errors.
Definition at line
924
of file
sl_efpdrv.c
.
References SL_EFPDRV_OK , sl_efpdrv_read_register() , and sl_efpdrv_write_register() .
Referenced by sl_efpdrv_enter_em0() , sl_efpdrv_enter_em2() , sl_efpdrv_read_otp() , sl_efpdrv_set_voa_em01_peak_current() , sl_efpdrv_set_voa_em23_peak_current() , sl_efpdrv_set_voa_mode() , sl_efpdrv_set_voa_sw_mode() , sl_efpdrv_set_vob_em01_peak_current() , sl_efpdrv_set_vob_em01_voltage() , sl_efpdrv_set_vob_em23_peak_current() , and sl_efpdrv_set_vob_mode() .