SPIDRV_Init Struct ReferenceEMDRV > SPIDRV
An SPI driver instance initialization structure. Contains a number of SPIDRV configuration options. This structure is passed to SPIDRV_Init() when initializing a SPIDRV instance. Some common initialization data sets are predefined in SPIDRV_MASTER_USART0 and friends.
Definition at line 120
of file spidrv.h
.
#include <
spidrv.h
>
Data Fields | |
SPIDRV_BitOrder_t | bitOrder |
A bit order on the SPI bus, MSB or LSB first. | |
uint32_t | bitRate |
An SPI bitrate. | |
SPIDRV_ClockMode_t | clockMode |
SPI mode, CLKPOL/CLKPHASE setting. | |
SPIDRV_CsControl_t | csControl |
A select master mode chip select (CS) control scheme. | |
uint32_t | dummyTxValue |
The value to transmit when using SPI receive API functions. | |
uint32_t | frameLength |
An SPI framelength, valid numbers are 4..16. | |
uint8_t | pinClk |
Clock pin. | |
uint8_t | pinCs |
Chip select pin. | |
uint8_t | pinRx |
Rx pin. | |
uint8_t | pinTx |
Tx pin. | |
USART_TypeDef * | port |
The USART used for SPI. | |
GPIO_Port_TypeDef | portClk |
Clock port. | |
GPIO_Port_TypeDef | portCs |
Chip select port. | |
GPIO_Port_TypeDef | portRx |
Rx port. | |
GPIO_Port_TypeDef | portTx |
Tx port. | |
SPIDRV_SlaveStart_t | slaveStartMode |
A slave mode transfer start scheme. | |
SPIDRV_Type_t | type |
An SPI type, master or slave. | |
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emdrv/spidrv/inc/
spidrv.h