WDOG_Init_TypeDef Struct ReferenceEMLIB > WDOG
Watchdog initialization structure.
Definition at line 131
of file em_wdog.h
.
#include <
em_wdog.h
>
Data Fields | |
bool | debugRun |
bool | em2Run |
bool | em3Run |
bool | em4Block |
bool | enable |
bool | lock |
WDOG_PeriodSel_TypeDef | perSel |
bool | resetDisable |
WDOG_WarnSel_TypeDef | warnSel |
WDOG_WinSel_TypeDef | winSel |
Field Documentation
bool WDOG_Init_TypeDef::debugRun |
Counter keeps running during debug halt.
Definition at line 136
of file em_wdog.h
.
Referenced by WDOGn_Init().
bool WDOG_Init_TypeDef::em2Run |
Counter keeps running when in EM2.
Definition at line 139
of file em_wdog.h
.
Referenced by WDOGn_Init().
bool WDOG_Init_TypeDef::em3Run |
Counter keeps running when in EM3.
Definition at line 142
of file em_wdog.h
.
Referenced by WDOGn_Init().
bool WDOG_Init_TypeDef::em4Block |
bool WDOG_Init_TypeDef::enable |
Enable watchdog when initialization completed.
Definition at line 133
of file em_wdog.h
.
Referenced by WDOGn_Init().
bool WDOG_Init_TypeDef::lock |
Block SW from disabling LFRCO/LFXO oscillators. Block SW from modifying the configuration (a reset is needed to reconfigure).
Definition at line 153
of file em_wdog.h
.
Referenced by WDOGn_Init().
WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel |
Clock source to use for watchdog. Watchdog timeout period.
Definition at line 161
of file em_wdog.h
.
Referenced by WDOGn_Init().
bool WDOG_Init_TypeDef::resetDisable |
Disable watchdog reset output if true
Definition at line 178
of file em_wdog.h
.
Referenced by WDOGn_Init().
WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel |
Select warning time as % of the watchdog timeout
Definition at line 166
of file em_wdog.h
.
Referenced by WDOGn_Init().
WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel |
Select illegal window time as % of the watchdog timeout
Definition at line 172
of file em_wdog.h
.
Referenced by WDOGn_Init().
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_wdog.h