TIMER_InitCC_TypeDef Struct ReferenceEMLIB > TIMER
TIMER compare/capture initialization structure.
Definition at line
357
of file
em_timer.h
.
#include <
em_timer.h
>
Data Fields |
|
TIMER_OutputAction_TypeDef | cmoa |
TIMER_OutputAction_TypeDef | cofoa |
bool | coist |
TIMER_OutputAction_TypeDef | cufoa |
TIMER_Edge_TypeDef | edge |
TIMER_Event_TypeDef | eventCtrl |
bool | filter |
TIMER_CCMode_TypeDef | mode |
bool | outInvert |
bool | prsInput |
TIMER_PrsInput_TypeDef | prsInputType |
TIMER_PrsOutput_t | prsOutput |
TIMER_PRSSEL_TypeDef | prsSel |
Field Documentation
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cmoa |
Counter match output action.
Definition at line
377
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cofoa |
Counter overflow output action.
Definition at line
374
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
bool TIMER_InitCC_TypeDef::coist |
Compare output initial state. Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.
Definition at line
395
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cufoa |
Counter underflow output action.
Definition at line
371
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_Edge_TypeDef TIMER_InitCC_TypeDef::edge |
Input capture edge select.
Definition at line
362
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_Event_TypeDef TIMER_InitCC_TypeDef::eventCtrl |
Input capture event control.
Definition at line
359
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
bool TIMER_InitCC_TypeDef::filter |
TIMER_CCMode_TypeDef TIMER_InitCC_TypeDef::mode |
Compare/capture channel mode.
Definition at line
380
of file
em_timer.h
.
Referenced by BOARD_init() , TIMER_InitCC() , and USTIMER_Init() .
bool TIMER_InitCC_TypeDef::outInvert |
Invert output from compare/capture channel.
Definition at line
398
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
bool TIMER_InitCC_TypeDef::prsInput |
Select TIMERnCCx (false) or PRS input (true).
Definition at line
386
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_PrsOutput_t TIMER_InitCC_TypeDef::prsOutput |
PRS output configuration. PRS output from a timer can either be a pulse output or a level output that follows the CC out value.
Definition at line
404
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_PRSSEL_TypeDef TIMER_InitCC_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsInput
is enabled.
Definition at line
368
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_timer.h