retargetserial.c File Reference
Provide stdio retargeting to USART/UART or LEUART.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
Definition in file retargetserial.c
.
#include <stdio.h>
#include "em_device.h"
#include "em_cmu.h
"
#include "em_core.h
"
#include "em_gpio.h
"
#include "retargetserial.h
"
#include "retargetserialconfig.h"
Macros | |
#define | _GENERIC_UART_STATUS_IDLE LEUART_STATUS_TXC |
#define | RXBUFSIZE 8 |
Functions | |
static void | disableRxInterrupt () |
Disable RX interrupt. | |
static void | enableRxInterrupt () |
Enable RX interrupt. | |
void | RETARGET_IRQ_NAME (void) |
UART/LEUART IRQ Handler. | |
int | RETARGET_ReadChar (void) |
Receive a byte from USART/LEUART and put into global buffer. | |
void | RETARGET_SerialCrLf (int on) |
UART/LEUART toggle LF to CRLF conversion. | |
bool | RETARGET_SerialEnableFlowControl (void) |
Enable hardware flow control. (RTS + CTS) | |
void | RETARGET_SerialFlush (void) |
Flush UART/LEUART. | |
void | RETARGET_SerialInit (void) |
Intializes UART/LEUART. | |
int | RETARGET_WriteChar (char c) |
Transmit single byte to USART/LEUART. | |
Variables | |
static bool | initialized = false |
static uint8_t | LFtoCRLF = 0 |
static volatile uint8_t | rxBuffer [RXBUFSIZE] |
static volatile int | rxCount = 0 |
static volatile int | rxReadIndex = 0 |
static volatile int | rxWriteIndex = 0 |