DMA_CfgDescrSGAlt_TypeDef Struct ReferenceEMLIB > DMA
Configuration structure for alternate scatter-gather descriptor.
Definition at line
257
of file
em_dma.h
.
#include <
em_dma.h
>
Data Fields |
|
DMA_ArbiterConfig_TypeDef | arbRate |
void * | dst |
DMA_DataInc_TypeDef | dstInc |
uint8_t | hprot |
uint16_t | nMinus1 |
bool | peripheral |
DMA_DataSize_TypeDef | size |
void * | src |
DMA_DataInc_TypeDef | srcInc |
Field Documentation
DMA_ArbiterConfig_TypeDef DMA_CfgDescrSGAlt_TypeDef::arbRate |
Arbitration rate, i.e., number of DMA transfers done before re-arbitration takes place.
Definition at line
277
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
void* DMA_CfgDescrSGAlt_TypeDef::dst |
Pointer to location to transfer data to.
Definition at line
262
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
DMA_DataInc_TypeDef DMA_CfgDescrSGAlt_TypeDef::dstInc |
Destination increment size for each DMA transfer.
Definition at line
265
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
uint8_t DMA_CfgDescrSGAlt_TypeDef::hprot |
HPROT signal state, refer to reference manual, DMA chapter for further details. Normally set to 0 if protection is not an issue. The following bits are available:
- bit 0 - HPROT[1] control for source read accesses, privileged/non-privileged access.
- bit 3 - HPROT[1] control for destination write accesses, privileged/non-privileged access.
Definition at line
291
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
uint16_t DMA_CfgDescrSGAlt_TypeDef::nMinus1 |
Number of DMA transfers minus 1 to do. Must be <= 1023.
Definition at line
280
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
bool DMA_CfgDescrSGAlt_TypeDef::peripheral |
Specify if a memory or peripheral scatter-gather DMA cycle. Notice that this parameter should be the same for all alternate descriptors.
- true - this is a peripheral scatter-gather cycle.
- false - this is a memory scatter-gather cycle.
Definition at line
299
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
DMA_DataSize_TypeDef DMA_CfgDescrSGAlt_TypeDef::size |
DMA transfer unit size.
Definition at line
271
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
void* DMA_CfgDescrSGAlt_TypeDef::src |
Pointer to location to transfer data from.
Definition at line
259
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
DMA_DataInc_TypeDef DMA_CfgDescrSGAlt_TypeDef::srcInc |
Source increment size for each DMA transfer.
Definition at line
268
of file
em_dma.h
.
Referenced by DMA_CfgDescrScatterGather() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_dma.h