USART_InitSync_TypeDef Struct ReferenceEMLIB > USART
Synchronous mode initialization structure.
Definition at line
418
of file
em_usart.h
.
#include <
em_usart.h
>
Data Fields |
|
| bool | autoCsEnable |
| bool | autoTx |
| uint32_t | baudrate |
| USART_ClockMode_TypeDef | clockMode |
| USART_Databits_TypeDef | databits |
| USART_Enable_TypeDef | enable |
| bool | master |
| bool | msbf |
| USART_PRS_Channel_t | prsRxCh |
| bool | prsRxEnable |
| uint32_t | refFreq |
Field Documentation
| bool USART_InitSync_TypeDef::autoCsEnable |
| bool USART_InitSync_TypeDef::autoTx |
Enable AUTOTX mode. Transmits as long as RX is not full. Generates underflows if TX is empty.
Definition at line
454
of file
em_usart.h
.
Referenced by MIC_init() , and USART_InitSync() .
| uint32_t USART_InitSync_TypeDef::baudrate |
Desired baud rate.
Definition at line
429
of file
em_usart.h
.
Referenced by MIC_init() , MICROSD_Init() , SPIDRV_Init() , and USART_InitSync() .
| USART_ClockMode_TypeDef USART_InitSync_TypeDef::clockMode |
Clock polarity/phase mode.
Definition at line
441
of file
em_usart.h
.
Referenced by SPIDRV_Init() , and USART_InitSync() .
| USART_Databits_TypeDef USART_InitSync_TypeDef::databits |
Number of data bits in frame.
Definition at line
432
of file
em_usart.h
.
Referenced by SPIDRV_Init() , and USART_InitSync() .
| USART_Enable_TypeDef USART_InitSync_TypeDef::enable |
Specifies whether TX and/or RX shall be enabled when initialization is completed.
Definition at line
420
of file
em_usart.h
.
Referenced by MIC_init() , USART_InitI2s() , and USART_InitSync() .
| bool USART_InitSync_TypeDef::master |
Select if to operate in master or slave mode.
Definition at line
435
of file
em_usart.h
.
Referenced by SPIDRV_Init() , and USART_InitSync() .
| bool USART_InitSync_TypeDef::msbf |
Select if to send most or least significant bit first.
Definition at line
438
of file
em_usart.h
.
Referenced by MICROSD_Init() , SPIDRV_Init() , and USART_InitSync() .
| USART_PRS_Channel_t USART_InitSync_TypeDef::prsRxCh |
Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).
Definition at line
448
of file
em_usart.h
.
Referenced by USART_InitSync() .
| bool USART_InitSync_TypeDef::prsRxEnable |
Enable USART Rx via PRS.
Definition at line
445
of file
em_usart.h
.
Referenced by USART_InitSync() .
| uint32_t USART_InitSync_TypeDef::refFreq |
USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.
Definition at line
426
of file
em_usart.h
.
Referenced by USART_InitSync() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_usart.h