UARTDRV_InitUart_t Struct ReferenceEMDRV > UARTDRV
A UART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required for driver instance initialization. This structure is passed to UARTDRV_Init() when initializing a UARTDRV instance.
Definition at line 179
of file uartdrv.h
.
#include <
uartdrv.h
>
Data Fields | |
uint32_t | baudRate |
UART baud rate. | |
uint8_t | ctsPin |
A CTS pin number. | |
GPIO_Port_TypeDef | ctsPort |
A CTS pin port number. | |
UARTDRV_FlowControlType_t | fcType |
Flow control mode. | |
bool | mvdis |
Majority Vote Disable for 16x, 8x and 6x oversampling modes. | |
USART_OVS_TypeDef | oversampling |
Oversampling mode. | |
USART_Parity_TypeDef | parity |
Parity configuration. | |
USART_TypeDef * | port |
The peripheral used for UART. | |
uint8_t | portLocation |
A location number for UART pins. | |
uint8_t | rtsPin |
An RTS pin number. | |
GPIO_Port_TypeDef | rtsPort |
An RTS pin port number. | |
UARTDRV_Buffer_FifoQueue_t * | rxQueue |
A receive operation queue. | |
USART_Stopbits_TypeDef | stopBits |
A number of stop bits. | |
UARTDRV_Buffer_FifoQueue_t * | txQueue |
T transmit operation queue. | |
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emdrv/uartdrv/inc/
uartdrv.h