TIMER_InitCC_TypeDef Struct ReferenceEMLIB > TIMER
TIMER compare/capture initialization structure.
Definition at line 357
of file em_timer.h
.
#include <
em_timer.h
>
Field Documentation
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cmoa |
Counter match output action.
Definition at line 377
of file em_timer.h
.
Referenced by TIMER_InitCC().
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cofoa |
Counter overflow output action.
Definition at line 374
of file em_timer.h
.
Referenced by TIMER_InitCC().
bool TIMER_InitCC_TypeDef::coist |
Compare output initial state. Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.
Definition at line 395
of file em_timer.h
.
Referenced by TIMER_InitCC().
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cufoa |
Counter underflow output action.
Definition at line 371
of file em_timer.h
.
Referenced by TIMER_InitCC().
TIMER_Edge_TypeDef TIMER_InitCC_TypeDef::edge |
TIMER_Event_TypeDef TIMER_InitCC_TypeDef::eventCtrl |
Input capture event control.
Definition at line 359
of file em_timer.h
.
Referenced by TIMER_InitCC().
bool TIMER_InitCC_TypeDef::filter |
TIMER_CCMode_TypeDef TIMER_InitCC_TypeDef::mode |
Compare/capture channel mode.
Definition at line 380
of file em_timer.h
.
Referenced by BOARD_init(), TIMER_InitCC(), USBTIMER_Init(), and USTIMER_Init().
bool TIMER_InitCC_TypeDef::outInvert |
Invert output from compare/capture channel.
Definition at line 398
of file em_timer.h
.
Referenced by TIMER_InitCC().
bool TIMER_InitCC_TypeDef::prsInput |
Select TIMERnCCx (false) or PRS input (true).
Definition at line 386
of file em_timer.h
.
Referenced by TIMER_InitCC().
TIMER_PrsOutput_t TIMER_InitCC_TypeDef::prsOutput |
PRS output configuration. PRS output from a timer can either be a pulse output or a level output that follows the CC out value.
Definition at line 404
of file em_timer.h
.
Referenced by TIMER_InitCC().
TIMER_PRSSEL_TypeDef TIMER_InitCC_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if prsInput
is enabled.
Definition at line 368
of file em_timer.h
.
Referenced by TIMER_InitCC().
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_timer.h