EUSART_UartInit_TypeDef Struct Reference
Initialization structure.
Definition at line
224
of file
em_eusart.h
.
#include <
em_eusart.h
>
Data Fields |
|
EUSART_AdvancedInit_TypeDef * | advancedSettings |
Advanced initialization structure pointer. It can be NULL.
|
|
uint32_t | baudrate |
EUSART_Databits_TypeDef
|
databits |
Number of data bits in frame.
|
|
EUSART_Enable_TypeDef
|
enable |
Specifies whether TX and/or RX will be enabled when initialization completes.
|
|
EUSART_LoopbackEnable_TypeDef
|
loopbackEnable |
Enable Loop Back configuration.
|
|
EUSART_MajorityVote_TypeDef
|
majorityVote |
Majority Vote can be disabled for 16x, 8x and 6x oversampling modes.
|
|
EUSART_OVS_TypeDef
|
oversampling |
Oversampling used.
|
|
EUSART_Parity_TypeDef
|
parity |
Parity mode to use.
|
|
uint32_t | refFreq |
EUSART_Stopbits_TypeDef
|
stopbits |
Number of stop bits to use.
|
|
Field Documentation
uint32_t EUSART_UartInit_TypeDef::baudrate |
Desired baud rate. If set to 0, Auto Baud feature is enabled and the EUSART will wait for (0x55) frame to detect the Baudrate.
Definition at line
234
of file
em_eusart.h
.
Referenced by EUSART_IrDAInit() , EUSART_UartInitLf() , and UARTDRV_InitEuart() .
uint32_t EUSART_UartInit_TypeDef::refFreq |
EUSART reference clock assumed when configuring baud rate setup. Set to 0 if using currently configured reference clock.
Definition at line
230
of file
em_eusart.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super/platform/emlib/inc/
em_eusart.h