Represents DNS/SRP server address information parsed from a Network Data service entry.
The mType field specifies the entry type. Some fields are only applicable to specific types.
The
mPortfield is only applicable forOT_HISTORY_TRACKER_DNS_SRP_ADDR_TYPE_UNICAST_*types.The
mSequenceNumberfield is only applicable for theOT_HISTORY_TRACKER_DNS_SRP_ADDR_TYPE_ANYCASTtype.Other fields are common and used for all address types.
Public Attributes#
The server address.
uint16_t
The RLOC16 of the Border Router adding/removing the entry.
uint16_t
Port number.
uint8_t
Anycast sequence number.
uint8_t
Version number.
Address type.
Indicates the event (added/removed).