You are viewing documentation for version:
PDFRepresent a unicast IPv6 address info.
Public Attributes#
The unicast IPv6 address.
uint8_t
The Prefix length (in bits).
uint8_t
The address origin (OT_ADDRESS_ORIGIN_* constants).
Indicates the event (address is added/removed).
bool
If the address is preferred.
bool
If the address is an RLOC.
Public Attribute Documentation#
mAddress#
otIp6Address otHistoryTrackerUnicastAddressInfo::mAddress
The unicast IPv6 address.
mPrefixLength#
uint8_t otHistoryTrackerUnicastAddressInfo::mPrefixLength
The Prefix length (in bits).
mAddressOrigin#
uint8_t otHistoryTrackerUnicastAddressInfo::mAddressOrigin
The address origin (OT_ADDRESS_ORIGIN_* constants).
mEvent#
otHistoryTrackerAddressEvent otHistoryTrackerUnicastAddressInfo::mEvent
Indicates the event (address is added/removed).
mScope#
uint8_t otHistoryTrackerUnicastAddressInfo::mScope
The IPv6 scope.
mPreferred#
bool otHistoryTrackerUnicastAddressInfo::mPreferred
If the address is preferred.
mValid#
bool otHistoryTrackerUnicastAddressInfo::mValid
If the address is valid.
mRloc#
bool otHistoryTrackerUnicastAddressInfo::mRloc
If the address is an RLOC.