Represents a favored OMR prefix tracked by a device acting as a Border Router (BR).
The mIsLocal field indicates whether the favored OMR prefix is the same as the local one maintained by this BR. The local OMR prefix can be either based on (random) ULA or a prefix delegated via DHCPv6-PD.
Public Attributes#
The OMR prefix.
signed int
The 2-bit signed preference (OT_ROUTE_PREFERENCE_* values).
bool
true if the prefix is the local OMR prefix; false otherwise.