Struct containing specifics of PA configuration.
PA descriptor as used in the PA conversion functions.
Public Attributes#
Algorithm used to map dBm to power levels for this PA.
uint8_t
The number of piecewise segments provided to the PA in a piecewise linear curve fit.
Min power level for this PA.
Max power level for this PA.
Union containing a pointer to algorithm-specific conversion data.
Public Attribute Documentation#
algorithm#
RAIL_PaConversionAlgorithm_t RAIL_PaDescriptor_t::algorithm
Algorithm used to map dBm to power levels for this PA.
Definition at line
224
of file plugin/pa-conversions/pa_curve_types_efr32.h
segments#
uint8_t RAIL_PaDescriptor_t::segments
The number of piecewise segments provided to the PA in a piecewise linear curve fit.
The default is 8. Should be set to 0 when not using the piecewise linear algorithm.
Definition at line
230
of file plugin/pa-conversions/pa_curve_types_efr32.h
min#
RAIL_TxPowerLevel_t RAIL_PaDescriptor_t::min
Min power level for this PA.
Definition at line
232
of file plugin/pa-conversions/pa_curve_types_efr32.h
max#
RAIL_TxPowerLevel_t RAIL_PaDescriptor_t::max
Max power level for this PA.
Definition at line
234
of file plugin/pa-conversions/pa_curve_types_efr32.h
conversion#
RAIL_PowerConversion_t RAIL_PaDescriptor_t::conversion
Union containing a pointer to algorithm-specific conversion data.
Definition at line
248
of file plugin/pa-conversions/pa_curve_types_efr32.h