More generic structure containing information about piecewise linear curves and mapping tables, instead of specific PA's.
Public Attributes#
The curves for each PA.
uint32_t
Signature used for validation of the curves configuruation.
uint16_t
PA VDD voltage, in millivolts.
Public Attribute Documentation#
curves#
RAIL_PaDescriptor_t RAIL_TxPowerCurvesConfigAlt_t::curves[RAIL_NUM_PA]
The curves for each PA.
Definition at line
259
of file plugin/pa-conversions/pa_curve_types_efr32.h
signature#
uint32_t RAIL_TxPowerCurvesConfigAlt_t::signature
Signature used for validation of the curves configuruation.
Definition at line
261
of file plugin/pa-conversions/pa_curve_types_efr32.h
paVoltage#
uint16_t RAIL_TxPowerCurvesConfigAlt_t::paVoltage
PA VDD voltage, in millivolts.
Definition at line
263
of file plugin/pa-conversions/pa_curve_types_efr32.h